Booting C6X Linux
                        =================

Booting c6x Linux requires a boot loader or debugger support. The boot loader
and debugger are expected to minimally initialize hardware, call the Linux
kernel, and pass information to the kernel.

Essentially, the boot loader should:

   1) Initialize system RAM
   2) Setup other hardware as needed
   3) Setup information to pass to kernel
   4) Jump to the kernel entry point


Tagged List
-----------

The boot loader may create and initialize a kernel tagged list which is used
to pass information from boot loader to kernel. Each entry in the tagged list
has the following strucuture:

         +------------+
Word 0   | Tag Type   |  |
         +------------+  |
Word 1   | Tag Size   |  v increasing addresses
         +------------+
Word 2   : Tag Data 1 :
         +    ...     +
         : Tag Data N :
         +------------+
Word 2+N | Tag Type   |
         +   ...      +

Where:
  Tag Type is a unique value for each tag
  Tag Size is size of tag data in bytes
  Tag Data is data appropriate for tag type

NB: Tag size is in bytes, but actual space used by tag data is an integral
    number of 32-bit words to maintain alignment for the following tag.

A tagged list must begin with a TAG_SOL tag and end with a TAG_EOL tag. Lists
may contain any number of tags. The tagged list must be placed in a region of
memory where neither the kernel decompressor nor RAM-based filesystem images
will overwrite it. Before jumping to the kernel entry point, a boot loader
using a tagged list must put a "magic" number (0x54694265) in register A4 and
a pointer to the list in register B4.

Definitions and code used to access the tagged list can be found in
arch/c6x/kernel/tags.[ch]


Passing a command line to kernel
--------------------------------
A bootloader may pass a command line to the kernel by using a tagged list and
TAG_CMDLINE. Alternatively, a boot loader may copy a NULL terminated command
line to offset 0x1000 of the kernel image. Maximum length of this command line
is 1024 bytes including terminating NULL.