#! /bin/bash

PAD_SIZE=0
ROUND_SIZE=0
FSIMAGE_START=""
FSIMAGE_SIZE=""
ABS_BASE=0

need-args() {
    found=$1; shift
    echo "$CMD expected $# arguments and found $found"
    i=1
    for name in "$@" ; do
        printf "\t%s\t%s\n" "arg$i" "$name"
        i=$((i+1))
    done
    exit 2
}
    
assert-readable() {
    for file in "$@" ; do
	if [ ! -r $file ] ; then
	    echo "Can not read file $file"
	    exit 2
	fi
    done
}
    
save-cmdline() {
    if [ $# -ne 2 ]; then need-args $# "bootblob or kernel image"  "cmdline save file"; fi
    IMAGE=$1
    CMDLINE_FILE=$2
    assert-readable $IMAGE
    # get 0x400 bytes at offset 0x1000
    dd if=$IMAGE of=$CMDLINE_FILE skip=4 bs=1024 count=1
}

get-cmdline() {
    if [ $# -ne 1 ]; then need-args $# "bootblob or kernel image"; fi
    IMAGE=$1
    assert-readable $IMAGE
    # get 0x400 bytes at offset 0x1000 and isolate the stuff before the first NUL character
    dd if=$IMAGE skip=4 bs=1024 count=1 2>/dev/null | xargs -0 -n 1 2>/dev/null | head -n 1
}

set-cmdline() {
    if [ $# -ne 2 ]; then need-args $# "bootblob or kernel image"  "quoted command line text"; fi

    IMAGE=$1
    CMDLINE=$2
    assert-readable $IMAGE
    dd if=/dev/zero of=$IMAGE seek=4 bs=1024 count=1 conv=notrunc 2>/dev/null
    echo -n "$2" | dd  of=$IMAGE seek=4 bs=1024 count=1 conv=notrunc 2>/dev/null
}

expand-vars() {
    FSIMAGE_START_ABS=$(($ABS_BASE + $FSIMAGE_START))
    KERNEL_START_ABS=$(($ABS_BASE + 0))

    val=$1
    val=${val//\%fsimage-start-off%/$(printf "%d" $FSIMAGE_START)}
    val=${val//\%fsimage-start-off-x%/$(printf "%x" $FSIMAGE_START)}
    val=${val//\%fsimage-start-abs%/$(printf "%d" $FSIMAGE_START_ABS)}
    val=${val//\%fsimage-start-abs-x%/$(printf "%x" $FSIMAGE_START_ABS)}
    val=${val//\%fsimage-size%/$(printf "%d" $FSIMAGE_SIZE)}
    val=${val//\%fsimage-size-x%/$(printf "%x" $FSIMAGE_SIZE)}
    echo "$val"
}

my-dd() {
    COUNT=$1
    SEEK=$2
    SKIP=$3
    shift 3

    if [ -z "$COUNT" ] ; then COUNT=0x40000000 ; fi

    for BLOCKSIZE in 1048576 4096 1024 16 4 1 ; do
        if [ $(( ($COUNT % $BLOCKSIZE) + ($SEEK % $BLOCKSIZE) + ($SKIP % $BLOCKSIZE) )) -eq 0 ]; then
            break;
        fi
    done
    echo "using blocksize of $BLOCKSIZE"
    COUNT=$(($COUNT / $BLOCKSIZE ))
    SEEK=$(($SEEK / $BLOCKSIZE ))
    SKIP=$(($SKIP / $BLOCKSIZE ))

    dd bs=$BLOCKSIZE seek=$SEEK skip=$SKIP count=$COUNT "$@"
}

make-image() {
    if [ $# -ne 4 ]; then need-args $# "bootblob to create"  "kernel binary image" "filesystem/initramfs image" "quoted command line text"; fi
    IMAGE=$1
    KERNEL=$2
    FSIMAGE=$3
    CMDLINE=$4

    assert-readable $KERNEL $FSIMAGE
    KERNEL_REAL_SIZE=$(stat -c"%s" $KERNEL)
    FS_REAL_SIZE=$(stat -c"%s" $FSIMAGE)

    if [ $ROUND_SIZE -gt 0 ] ; then
        KERNEL_ROUND_SIZE=$(( (($KERNEL_REAL_SIZE + $ROUND_SIZE - 1) / $ROUND_SIZE) * $ROUND_SIZE ))
        FS_ROUND_SIZE=$((     (($FS_REAL_SIZE     + $ROUND_SIZE - 1) / $ROUND_SIZE) * $ROUND_SIZE ))
    else
        KERNEL_ROUND_SIZE=$KERNEL_REAL_SIZE
        FS_ROUND_SIZE=$FS_REAL_SIZE
    fi

    if [ -z "$FSIMAGE_START" ] ; then FSIMAGE_START=$KERNEL_ROUND_SIZE; fi
    if [ -z "$FSIMAGE_SIZE"  ] ; then FSIMAGE_SIZE=$FS_ROUND_SIZE; fi
    TOTAL_SIZE=$(( $FSIMAGE_START + $FSIMAGE_SIZE ))
    if [ $TOTAL_SIZE -lt $KERNEL_ROUND_SIZE  ] ; then TOTAL_SIZE=$KERNEL_ROUND_SIZE; fi

   CMDLINE=$(expand-vars "$CMDLINE")

    printf "kernel   %8.8X  for %10d bytes end at %8.8X\n"  0  $KERNEL_REAL_SIZE $((0+$KERNEL_ROUND_SIZE-1))
    printf "fsimage  %8.8X  for %10d bytes end at %8.8X\n"  $FSIMAGE_START  $FS_REAL_SIZE  $(($FSIMAGE_START + $FSIMAGE_SIZE-1))
    printf "total    %8.8X  for %10d bytes end at %8.8X\n"  0 $TOTAL_SIZE $(($TOTAL_SIZE-1))
    printf "cmdline  %s\n"  "$CMDLINE"

#    dd if=/dev/zero   of=$IMAGE bs=1 count=$TOTAL_SIZE
#    dd if=$KERNEL     of=$IMAGE conv=notrunc
#    dd if=$FSIMAGE    of=$IMAGE bs=1 seek=$FSIMAGE_START conv=notrunc
    my-dd $TOTAL_SIZE 0                 0       if=/dev/zero   of=$IMAGE 
    my-dd ""          0                 0       if=$KERNEL     of=$IMAGE conv=notrunc
    my-dd ""          $FSIMAGE_START    0       if=$FSIMAGE    of=$IMAGE conv=notrunc
    set-cmdline $IMAGE "$CMDLINE"
}

do_help() {
    echo "bootblob [options] <cmd> [options] <args>"
    echo "where cmd is one of: (run just the command to see the argument description)"
    echo "    make-image              create a new bootblob image"
    echo "    set-cmdline             set command line of a blob image or kernel binary image"
    echo "    get-cmdline             print the current command line of a blob image or kernel binary image"
    echo "    save-cmdline            save the raw cmdline data to a file"
    echo ""
    echo "and where options is zero or more of: (use decimal or 0x prefix for hex)"
    echo "    --fsimage-start=        specify the starting offset of the file system image"
    echo "    --fsimage-size=         specify the size of the file system image"
    echo "    --round=                round starting and ending addresses to a multiple of this value"
    echo "    --abs-base=             specify the absolute address where image will reside (used for var expansion)"
    echo ""
    echo "the command line value of make-image (only) can have variable expansion.  The following values are supported"
    echo "    %fsimage-start-off%     starting offset of the filesystem image (decimal)"
    echo "    %fsimage-start-off-x%   starting offset of the filesystem image (hex)"
    echo "    %fsimage-start-abs%     starting absolute address of the filesystem image (decimal)"
    echo "    %fsimage-start-abs-x%   starting absolute address of the filesystem image (hex)"
    echo "    %fsimage-size%          size of filesystem image (decimal)"
    echo "    %fsimage-size-x%        size of filesystem image (hex)"
    echo ""
    echo "example:"
    echo "    ./bootblob make-image --abs-base=0x80000000 --round=0x100000 test.blob vmlinux-xxx.bin min-root-c6x.cpio.gz \\"
    echo "        console=cio initrd=0x%fsimage-start-abs-x%,0x%fsimage-size-x% ip=dhcp"
}

handle-one-option() {
    opt=$1
    case $opt in
        -d|--debug)
            set -x
            ;;
        -h|--help)
            do_help
            exit 0
            ;;
        --fsimage-start=*)
            FSIMAGE_START=${1#--fsimage-start=}
            ;;
        --fsimage-size=*)
            FSIMAGE_SIZE=${1#--fsimage-size=}
            ;;
        --round=*)
            ROUND_SIZE=$(( ${1#--round=} + 0 ))
            ;;
        --abs-base=*)
            ABS_BASE=$(( ${1#--abs-base=} + 0 ))
            ;;
        --)
            return 2
            ;;
        -*)
            echo "unknow option use '$0 help' for info"
            exit 2
            ;;
        *)
            return 1
            ;;
    esac
    return 0
}

BINDIR=$(dirname $0)

# handle options before the CMD
while handle-one-option $1 ; do
    shift
done
if [ "$1" == "--" ]; then shift; fi

# get command
CMD=$1
shift

# handle options after the CMD
while handle-one-option $1 ; do
    shift
done
if [ "$1" == "--" ]; then shift; fi

case $CMD in
    help)
        do_help
        exit 0
        ;;
    make-image|set-cmdline|get-cmdline|save-cmdline)
        $CMD "$@"
        ;;
    "")
        echo "must specifiy a command, try:"
        echo "    bootblob help"
        exit 1
        ;;
    *)
        echo "unknown command $CMD"
        exit 1
        ;;
esac