#!/bin/bash

# This is either the prj script or a bootstrap script created from it

### INSTANCE MARK
### INSTANCE VARS BEGIN
# configurations for this instance of prj
PROJECT="linux-c6x"
BASEURL="git://linux-c6x.org/git/"
BOMPRJ=linux-c6x-project
BOMEXT=.git
REF="master"
REMOTE="origin"

BASE_PRJ="linux-c6x busybox"
WRAP_PRJ=""
EXTRA_PRJ="projects/mtd-utils projects/rio-utils projects/packages projects/ltp projects/c6x-linux-mcsdk-demo projects/syslink"

CONFIG_CMD=scripts/setup

TOP=..
REST_PRJ="$BASE_PRJ $WRAP_PRJ $EXTRA_PRJ"
ALL_PRJ="$BOMPRJ $REST_PRJ"
### INSTANCE VARS END

do-help-bootstrap() {
    echo "bootstrap a project development setup for $PROJECT"
    echo "bootstrap [options] [version]"
    echo ""
    echo "supported options:"
    echo "    --help  -h              print this help message and exit"
    echo "    --debug -d              do debug tracing"
    echo "    --url=                  specify a base URL"
    echo "    --bom=                  specify the master / Bill Of Materials project"
    echo "    --print-vars            print the default vars from this instance of bootstrap and exit"
    echo "    --safer                 don't run stage 2, allow user to verify it & run it manually"
    echo ""
    echo "version is a branch or tag name in the master project"
    echo ""
    echo "This instance of bootstrap has:"
    echo "  Default URL              $BASEURL"
    echo "  Default BOM Project      $BOMPRJ"
    echo "  Default Version          $REF"
    echo ""
    if [ -n "$OTHER_REF_SUGGESTIONS" ] ; then
        echo "It also suggests the following other versions:"
        printf "%b\n" "$OTHER_REF_SUGGESTIONS"
    fi
}

do-help-prj() {
    do-include-local

    echo "operations across multi-components of $PROJECT"
    echo "prj [options] cmd <args>"
    echo ""
    echo "supported options:"
    echo "    --help  -h              print this help message and exit"
    echo "    --debug -d              do debug tracing"
    echo ""
    echo "version is a branch or tag name in the master project"
    echo ""
    echo "This instance of prj has:"
    echo "  Base URL                  $BASEURL"
    echo "  BOM Project               $BOMPRJ"
    echo "  Version                   $REF"
    echo ""
}


do-print-vars-bootstrap() {
    printf 'PROJECT="%s"\n' "$PROJECT"
    echo "BASEURL=\"$BASEURL\""
    echo "BOMPRJ=\"$BOMPRJ\""
    echo "BOMEXT=\"$BOMEXT\""
    echo "REF=\"$REF\""
    echo "OTHER_REF_SUGGESTIONS=\"$OTHER_REF_SUGGESTIONS\""
}

handle-one-option-bootstrap() {
    opt=$1
    case $opt in
        -d|--debug)
            set -x
            STAGE2_OPTIONS="$STAGE2_OPTIONS --debug"
            ;;
        -h|--help)
            do-help-bootstrap
            exit 0
            ;;
        --url=*)
            BASEURL=${1#--url=}
            ;;
        --bom=*)
            BOMPRJ=${1#--bom=}
            ;;
        --avail)
            do-print-avail
            exit 0
            ;;
        --print-vars)
            do-print-vars-bootstrap
            exit 0
            ;;
        --safer)
            SAFER_MODE=true
            ;;
        --)
            return 2
            ;;
        -*)
            echo "unknow option use '$0 help' for info"
            exit 2
            ;;
        *)
            return 1
            ;;
    esac
    return 0
}

handle-one-option-prj() {
    opt=$1
    case $opt in
        -d|--debug)
            set -x
            ;;
        -h|--help)
            do-help-prj
            exit 0
            ;;
        --)
            return 2
            ;;
        -*)
            echo "unknow option use '$0 help' for info"
            exit 2
            ;;
        *)
            return 1
            ;;
    esac
    return 0
}

check-git() {
    if $GIT_CHECKED; then
	return
    fi

    GIT_CHECKED=true
    if ! which git ; then 
	echo "you don't have git in your PATH"
	exit 2
    fi

    if git --version | grep -q [01]\.[0-6]\. ; then
	echo "***Warning***: you are using $(git --version) and prj recomends at least 1.7"
	FF_ONLY_OPTION=""
    fi
}

do-bootstrap-stage1() {
    # handle options
    while handle-one-option-bootstrap $1 ; do
        shift
    done
    if [ "$1" == "--" ]; then shift; fi

    if [ -n "$1" ] ; then REF=$1 ; fi

    # assure we have at least the tools we need to get the bom project
    check-git

    # get the BOM project
    TOP="."
    (do-clone-ref $BOMPRJ $REF)

    # hack for development of bootstrap and ./prj
    if [ -n "$BOOTSTRAP_DEV_HACK" ] ; then 
        (cd $STARTPWD; cp -p $MYDIR/prj $BOMPRJ/ )
    fi

    # save info on what we did
    cd $BOMPRJ
    do-print-vars-bootstrap >.prj.local

    # execute the bootstrap 2nd stage which is part of the bom project itself
    # since this executes stuff just downloaded, allow a mode that tells user
    # how to manually do it.
    if $SAFER_MODE ; then
        echo "you should:"
        echo "  cd $PWD"
        echo "  less ./prj"
        echo "        (inspect the prj script and assure yourself it is OK)"
        echo "  ./prj bootstrap-stage2"
        exit 0
    else
        # see if the bom project has a ./prj script and it supports bootstrap
        if [ ! -x ./prj -o "$(./prj parle-vu-bootstrap)" != "parle-vu-i-do" ] ; then 
            echo "The $REF version is not bootstrap enabled"
            exit 2
        fi
        ./prj $STAGE2_OPTIONS bootstrap-stage2 
        echo "Done.  you should:"
        echo "  cd $PWD"
    fi
}

do-clone-ref() {
    PRJ=$1
    PRJ_REF=$2

    STARTDIR=$(pwd)
    BASEDIR=$(dirname $TOP/$PRJ)

    check-git

    # get the project, unless it exists already
    if [ -d $TOP/$PRJ/.git ] ; then
        echo "$TOP/$PRJ/.git already exists, skipping clone"
    else
        mkdir -p $BASEDIR
        cd $BASEDIR
        git clone $BASEURL$PRJ$BOMEXT
	cd $STARTDIR
    fi
    cd $TOP/$PRJ

    # pull down more info & resolve ref
    git fetch --tags origin
    FULL_REF=$(git show-ref $REF | head -n 1 | cut -f2 -d" ")
    if [ -z "$FULL_REF" ]; then 
        echo "can't find ref $REF in $PRJ"; 
        return 2 
    fi

    case $FULL_REF in
    refs/heads/*)
        # already a local branch of the same name, see if we can switch to it and update it
        git checkout ${FULL_REF#refs/heads/}
        if ! git pull $FF_ONLY_OPTION $REMOTE $REF ; then
            git checkout $FULL_REF
        fi
        ;;
    refs/remotes/*)
        # remote branch w/ no local one, 
        git checkout -b $REF ${FULL_REF#refs/remotes/}
        ;;
    refs/tags/*)
        # tag, leave the HEAD disconnected, the user can create a branch if she wishes
        git checkout $FULL_REF
        ;;
    *)
        # unexpected pattern, try it
        echo "unexpected reference format $FULL_REF"
        git checkout $FULL_REF
        ;;
    esac
}

do-include-local() {
    if [ -r $TOP/$BOMPRJ/.prj.local ] ; then
        source $TOP/$BOMPRJ/.prj.local
    fi
}

#local vars
SAFER_MODE=false
STAGE2_OPTIONS=""
export prj=none

ME=$0
MYDIR=$(dirname $0)
STARTPWD=$PWD
IS_BOOTSTRAP=false
GIT_CHECKED=false
FF_ONLY_OPTION="--ff-only"

case "$(basename $0)" in
*bootstrap) 
    IS_BOOTSTRAP=1

    if [ y"$1" == y"parle-vu-bootstrap" ] ; then
        echo "no, I just do stage1"
        exit 2
    fi
    
    do-bootstrap-stage1 "$@"
    exit $?
;;
esac

# if here we are a real prj script
while handle-one-option-prj $1 ; do
    shift
done
if [ "$1" == "--" ]; then shift; fi

do-include-local

case $1 in
parle-vu-bootstrap)
    # protocol version 0 ignores any args and answers back like so
    echo "parle-vu-i-do"
    # future enhancements in bootstrap can supply a requested level 
    # the response would include the level granted (unless the grant is level 0 as above)
;;
bootstrap-stage1)
    do-bootstrap-stage1 "$@"
;;
bootstrap-stage2)
    for prj in $ALL_PRJ ; do
        echo "****** $prj"
        (do-clone-ref $prj $REF)
    done
;;
make-bootstrap)
    OUTFILE=$2
    if [ -z "$OUTFILE" ] ; then 
        echo "need path/filename to which to write"
        exit 2
    fi
    TMPFILE=$(mktemp)
    printf "### INSTANCE VARS BEGIN\n"  >$TMPFILE
    printf "# variables for this instance of bootstrap\n" >>$TMPFILE
    do-print-vars-bootstrap             >>$TMPFILE
    printf "### INSTANCE VARS END\n"    >>$TMPFILE
    sed -e '/^### INSTANCE VARS BEGIN/,/^### INSTANCE VARS END/ d' \
        -e '/^### INSTANCE MARK/ r'"$TMPFILE" <$ME >$OUTFILE
    rm $TMPFILE
;;
clone)
    for prj in $ALL_PRJ ; do
        echo "****** $prj"
        (do-clone-ref $prj $REF)
    done
;;
status)
    for prj in $ALL_PRJ ; do
        echo "****** $prj"
        (cd $TOP/$prj; git status)
    done
;;
config)
    shift
    $CONFIG_CMD "$@"
;;
git)
    shift
    for prj in $ALL_PRJ ; do
        echo "****** $prj"
        (cd $TOP/$prj; eval "git" "$@")
    done
;;
for-each)
    shift
    for prj in $ALL_PRJ ; do
        echo "****** $prj"
        (cd $TOP/$prj; eval "$@")
    done
;;
*)
    echo "Don't know command $1"
    false
;;
esac