xWRL6432 MMWAVE-L-SDK  05.05.00.00
Release Notes 05.02.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless noted otherwise, the SW modules would work in both FreeRTOS and NORTOS environment.
Unless noted otherwise, the SW modules would work on any of the CPU present on the SOC.
Unless noted otherwise, the SW modules would work on all supported EVMs

New in this Release

Feature Module
MPD Proc DPU Datapath
Presence Detection feature OOB Demo
Gtrack library Datapath
Tracker integration to Motion and Presence Detection OOB Demo OOB Demo
1Tx-1Rx, 2Tx-2Rx configuration support Motion and Presence Detection OOB Demo OOB Demo
Antenna geometry configuration support Motion and Presence Detection OOB Demo OOB Demo
INA228 based power measurement in Motion and Presence Detection OOB Dem OOB Demo
Classifier feature extraction libraries Datapath
Added Idle state (Power Mode) in OOB OOB Demo
Added Thresholds for LPDS and Idle low Power Modes POWER
Syconfig support and flash driver redesign to enable new flash configuration BOARD library and QSPI
Configure inter-chirp power saving based on inter-chirp time mmwave Control lib
LIN driver and example support LIN
Update Pin Parking configuration in LPDS low Power Mode POWER
Finite frames support with Low Power Mode enabled in Motion and Presence Detection OOB Demo OOB Demo
DMA support for MCAN driver with Loopback example MCAN
MCAN external read and write example MCAN
Support of triggering Soft and warm reset in SOC driver SOC
Angular JS Visualizer Visualizer
ANA #52 Slicer LDO Test LOAD (TLOAD) not disabled after startup fix in sysconfig SoC

Device and Validation Information

SOC Supported CPUs EVM Host PC
xWRL6432 M4F xWRL6432 EVM (referred to as xwrL64xx-evm in code) Windows 10 64b or Ubuntu 18.04 64b

Tools, Compiler and Other Open Source SW Module Information

Tools / SW module Supported CPUs Version
Code Composer Studio M4F 12.4.0
SysConfig M4F 1.17.0
TI ARM CLANG M4F 2.1.3.LTS
FreeRTOS Kernel M4F 10.4.3
mmwave DFP M4F 3_0_8_6
UNIFLASH M4F 8.3.0

Key Features

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel M4F NA Task, Task notification, interrupts, semaphores, mutexs, timers, event groups. ROV views in CCS IDE, Task load measurement using FreeRTOS run time statistics APIs. -
FreeRTOS POSIX M4F NA pthread, mqueue, semaphore, clock -
NO RTOS M4F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Clock M4F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CycleCounter M4F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug M4F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap M4F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi M4F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore -
MPU M4F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore M4F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task M4F NA FreeRTOS Create, delete tasks -
Timer M4F YES FreeRTOS, NORTOS Configure arbitrary timers -
Event M4F YES FreeRTOS Setting, getting, clearing, and waiting of Event bits -

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
EDMA M4F YES Basic memory copy, DMA/QDMA channels, Interrupt/Polled, Manual/Event trigger, Chaining -
ESM M4F YES Group and Error number selection, Tested ESM notifier with watchdog module -
GPIO M4F YES Basic input/output, GPIO as interrupt -
HWA M4F YES FFT, CFAR and compression/decompression, Interrupt/Polled, Manual/DMA trigger -
I2C M4F YES Controller mode, basic read/write, polling and interrupt mode Target mode not supported.
MCAN M4F YES RX, TX, interrupt and polling mode -
MCSPI M4F YES Controller/Target mode, basic read/write, polling, interrupt and DMA mode -
Pinmux M4F YES Tested with multiple peripheral pinmuxes -
QSPI M4F YES Read direct, Write indirect, Read/Write commands -
SOC M4F YES Lock/unlock MMRs, get CPU clock, CPU name, clock enable, set frequency -
UART M4F YES Basic read/write, polling, interrupt mode, CPU/DMA mode -
WATCHDOG M4F YES Window size and Expiry time selections, Reset mode, Digital windowed -
POWER M4F YES Device LPDS Entry and Exit using sleep counter/SYNCIN IO. Device Idle3 entry and exist using frame timer -
LIN M4F YES LIN Internal loopback, LIN external DIG/ANA loopback -

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
Flash M4F YES QSPI based flash (Macronix part MX25V1635F) All vendor flash types not tested

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MMWLPSDK-238 Unable to connect visualizer to debug versions of CCS builds OOB Demo 5.1.0 onwards xWRL6432 Linker file is modified to use RBL data ram only for heap and stack
MMWLPSDK-243 SDK OOB Demo does not support all configurations OOB Demo 5.1.0 onwards xWRL6432 Enabled Support for 1tx-1rx and 2tx-2rx configurations
MMWLPSDK-272 McSPI driver and GPIO driver Drivers 5.1.0 onwards xWRL6432 Corrected the McSPI driver to configure Data line 0 and 1.
Modified GPIO driver to correctly configure the interrupts.
MMWLPSDK-164 Debugging in CCS throws garbage to UART on startup OOB Demo 5.1.0 onwards xWRL6432 This issue is specific to Tera term tool, resetting or reconnecting terminal will fix this issue
MMWLPSDK-281 Finite frames config support with Low Power mode OOB Demo 5.1.0 onwards xWRL6432 None
MMWLPSDK-229 Re-architecting of the OOB for condition other than Low power operation OOB Demo 5.1.0 onwards xWRL6432 Added idle mode support in OOB for power saving with inter frame idle time less than threshold time for LPDS.
If there is no enough time for Idle mode Demo application would through error to user.
MMWLPSDK-173 Memory Usage fault due to unaligned memory access with Demo and RPMF examples SDK applications 5.1.0 onwards xWRL6432 Added a compiler option -mno-unaligned-access to not generate unaligned access.
MMWLPSDK-174 Timer configuration (APSS_RTI) configuration does not enable source clock. OOB Demo 5.1.0 onwards xWRL6432 Enabled in CSL_APP_RCM_IPCFGCLKGATE0 register and corrected interrupt number

Known Issues

ID Head Line Module Applicable Releases Applicable Devices Workaround
MMWLPSDK-244 HWA decompression output minor deviations HWA driver 5.01.00.03 xWRL6432 None

Limitations

Head Line Module Reported in Release Applicable Devices Workaround
All the TLV's cannot be enabled at same time due to limitation of UART baudrate Motion and Presence detection OOB demo 5.01.00.03 xWRL6432 Enable only required TLV's
On-board INA sensor(INA 226) cannot be used for power measurement. When device with INA226 sensor is used, the Power will not be plotted in visualizer. Motion and Presence detection OOB demo 5.01.00.03 xWRL6432 None
SensorStop not supported in low Power configuration. Motion and Presence detection OOB demo 5.01.00.03 xWRL6432 None.
Debug image of Motion and Presence detection OOB demo does not run with latest visualizer. There are issues when configurations are sent. Motion and Presence detection OOB demo 5.02.00.02 xWRL6432 Use serial terminals like Tera Term etc. to send configurations when working with debug image of OOB demo.
Interframe processing time and transmit output time of Stats TLV show 0 in low Power mode. Motion and Presence detection OOB demo 5.01.00.03 xWRL6432 While measuring interframe processing time and transmit output time, have low Power configuration disabled. These timings should not change with low Power configuration.
Using 32KB RAM memory (Range: 0x00458000 to 0x0045ffff) in application can cause issues. This block is being used by RBL. General 5.01.00.03 xWRL6432 Use this block of memory for sections like Stack, Heap, BSS (if allocated contiguously).
Posix Demo example is failing. Kernel Examples 5.01.00.03 xWRL6432 None.
QSPI Flash (qspi_flash_diag) nortos example is failing. Driver Examples 5.02.00.02 xWRL6432 None.

Upgrade and Compatibility Information

Attention
When migrating from Processor/Older SDK RTOS, see Migration Guides for more details

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

Compiler Options

Module Affected API Change Additional Remarks
Release Build - The release build with ti-arm-clang compiler has been done with Os optimization level. It is recommended that user rebuilds the existing libraries and applications with 'Os' option. This can be done by updating CFLAGS_release in library/example makefiles.