This example uses the WDT module in reset mode to trigger SOC warm reset. Servicing the WDT for few iterations before triggering the warm reset. It will reset the device once it reaches the expiry time set by user.
Make sure to confirm the following configuration in syscfg.
WDT Reset Mode: trigger warm reset
In this example we are trying to show two different flows:
Parameter | Value |
---|---|
CPU + OS | m4fss0-0 freertos |
Toolchain | ti-arm-clang |
Boards | xWRL6432-evm |
Example folder | examples/drivers/watchdog/watchdog_reset/ |
A GUI tool SysConfig is used to configure different modules and peripherals of the example. Using this tool, users can select and customize different modules and peripherals. The SysConfig tool will generate the code for initializing and configuring these modules. This configuration is saved to a file called example.syscfg for every example. To know more about how to use SDK with SysConfig, Visit this page
The user can perform the following sequence if they want to reload complete image from flash during a watchdog reset. After exiting watchdog reset RBL is made to reload from flash by issuing a controlled warm reset with boot vector set to 0. Also when frontend is being used by the application, we have to ensure that frontend PD is ON to enable the RBL to load the frontend firmware.
If the user does not want to reload image from flash and when frontend is not being used we can maintain a backup of the data section so as to restore after watchdog reset. If the user reloads an image from Flash, we do not need to maintain a backup of the data section. The user can update the linker to have the data section only at the run address.
Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console.
CCS Console:
UART Console: