xWRL6432 devices support booting over SPI interface in the absence of serial flash memory (where application usually resides). This example demonstrates the booting of xWRL6432 device with no serial flash memory using another xWRL6432 device. The device that is running this example sends the user application to another device without flash via SPI interface.
ROM bootloader (or RBL) is a software that resides in a on-chip read-only memory (ROM) of application subsystem (APPSS) to assist the customer in transferring and executing their application code. It will do the Reset cause check and Device initialization. After that It will check the SOP lines and SFLASH connection to proceed with either the flashing or execution mode. In Flashing Mode, ROM bootloader (or RBL) performs the serial flash programming over UART interface. In functional mode, the bootloading of an image from the Flash memory is the first bootmode attempted by the bootloader. When not using a serial flash device to store the application image, the bootloader will look for an image to be loaded via SPI or UART interface, if the first ping/command is initiated through SPI interface then RBL switch to SPI mode of image download. This image can be loaded in from a host PC or processor using the protocol documented below. A simplified diagram for command response flow is shown below.
| Parameter | Value |
|---|---|
| CPU + OS | m4fss0-0 freertos |
| Toolchain | ti-arm-clang |
| Board | xWRL6432-evm |
| Example folder | examples/drivers/boot/spibooting |
A GUI tool SysConfig is used to configure different modules and peripherals of the example. Using this tool, users can select and customize different modules and peripherals. The SysConfig tool will generate the code for initializing and configuring these modules. This configuration is saved to a file called example.syscfg for every example. To know more about how to use SDK with SysConfig, Visit this page
| SPI Controller | xWRL6432 where this example is running |
| SPI Peripheral | xWRL6432 without Flash |
This example implements the standard SPI protocol as detailed in Multichannel Serial Port Interface (McSPI) with settings as below
| Setting | Value |
|---|---|
| SPI Mode | 0 (Polarity 0, Phase 0) |
| SPI Clock Frequency | 22 MHz |
| S1.1 | S1.2 | S1.3 | S1.4 | S1.5 | S1.6 |
|---|---|---|---|---|---|
| ON | OFF | X | X | X | ON |
Note Before running the example, reset the device without flash (peripheral) using the "Reset_SWT" on EVM.
After the controller successfully transmits the user application image, output log will be
We can see the output on peripheral side by using Tera Term. It will appear as shown below. For example, When power example is transferred.