xWRL6432 MMWAVE-L-SDK  05.05.00.00
QSPI Flash Transfer

Introduction

This example demonstrates the data transfer from flash connected to QSPI interface

Supported Combinations

Parameter Value
CPU + OS m4fss0-0 freertos
m4fss0-0 nortos
Toolchain ti-arm-clang
Boards xWRL6432-evm
Example folder examples/drivers/qspi/qspi_flash_transfer

Using SDK with SysConfig

A GUI tool SysConfig is used to configure different modules and peripherals of the example. Using this tool, users can select and customize different modules and peripherals. The SysConfig tool will generate the code for initializing and configuring these modules. This configuration is saved to a file called example.syscfg for every example. To know more about how to use SDK with SysConfig, Visit this page

Using SDK with SysConfig

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

[QSPI Flash Transfer Test] Starting ...
[QSPI Flash Transfer Test] Executing Flash Erase on first block...
[QSPI Flash Transfer Test] Performing Write-Read Test...
[QSPI Flash Transfer Test] Write-Done...
[QSPI Flash Transfer Test] Read-Done...
All tests have passed!!