xWRL6432 MMWAVE-L-SDK  05.05.00.00
I2C Temperature Read

Introduction

This example demonstrates probing of sensor via I2C and read data from it. The application reads data from the temperature sensor in the EVM. Application reads 20 samples from the sensor and exits.

Supported Combinations

Parameter Value
CPU + OS m4fss0-0 freertos
m4fss0-0 nortos
Toolchain ti-arm-clang
Board xWRL6432-evm
Example folder examples/drivers/i2c/i2c_temperature

Using SDK with SysConfig

A GUI tool SysConfig is used to configure different modules and peripherals of the example. Using this tool, users can select and customize different modules and peripherals. The SysConfig tool will generate the code for initializing and configuring these modules. This configuration is saved to a file called example.syscfg for every example. To know more about how to use SDK with SysConfig, Visit this page

Using SDK with SysConfig

Steps to Run the Example

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,

[I2C] Temperature sensor found at device address 0x4b
[I2C] Sample 0: 30.250000 (celcius)
[I2C] Sample 1: 30.250000 (celcius)
[I2C] Sample 2: 30.250000 (celcius)
[I2C] Sample 3: 30.250000 (celcius)
[I2C] Sample 4: 30.250000 (celcius)
[I2C] Sample 5: 30.250000 (celcius)
[I2C] Sample 6: 30.250000 (celcius)
[I2C] Sample 7: 30.250000 (celcius)
[I2C] Sample 8: 30.250000 (celcius)
[I2C] Sample 9: 30.250000 (celcius)
[I2C] Sample 10: 30.250000 (celcius)
[I2C] Sample 11: 30.250000 (celcius)
[I2C] Sample 12: 30.250000 (celcius)
[I2C] Sample 13: 30.250000 (celcius)
[I2C] Sample 14: 30.250000 (celcius)
[I2C] Sample 15: 30.250000 (celcius)
[I2C] Sample 16: 30.250000 (celcius)
[I2C] Sample 17: 30.250000 (celcius)
[I2C] Sample 18: 30.250000 (celcius)
[I2C] Sample 19: 30.250000 (celcius)
All tests have passed!!