This example is a application which demonstrates the LIN message communication. Instance LIN1 is set to Transmit as well as Receive.
The LIN1 instance initiates the transmission by sending LINID followed by message. It receives the same message.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos | |
Toolchain | ti-arm-clang |
Boards | xWRL6432-evm |
Example folder | examples/drivers/lin/lin_loopback_interrupt |
A GUI tool SysConfig is used to configure different modules and peripherals of the example. Using this tool, users can select and customize different modules and peripherals. The SysConfig tool will generate the code for initializing and configuring these modules. This configuration is saved to a file called example.syscfg for every example. To know more about how to use SDK with SysConfig, Visit this page
Shown below is a sample output when the application is run,