This example performs HWA based FFT operation on real input data.
The input to the FFT is a sinusoidal real data. This is converted to 16-bit signed fixed point data which the HWA will operate on. The HWA PaRAM sets are initialized with proper configuration for FFT. The HWA is triggered to perform the FFT operation and the frequency domain complex output is converted back to 16-bit signed data.
Parameter | Value |
---|---|
CPU + OS | m4fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | xWRL6432-evm |
Example folder | examples/drivers/hwa/hwa_real_fft |
A GUI tool SysConfig is used to configure different modules and peripherals of the example. Using this tool, users can select and customize different modules and peripherals. The SysConfig tool will generate the code for initializing and configuring these modules. This configuration is saved to a file called example.syscfg for every example. To know more about how to use SDK with SysConfig, Visit this page
Shown below is a sample output when the application is run,