This example is a application which demonstrates the SCI message communication. Instance LIN1 is set to Transmit as well as Receive.
The LIN1 instance initiates the transmission by sending SCI bytes. It receives the same message.
Parameter | Value |
---|---|
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos | |
Toolchain | ti-arm-clang |
Boards | xWRL1432-evm |
Example folder | examples/drivers/lin/lin_sci_loopback |
Shown below is a sample output when the application is run,