Introduction
This example demonstrates the data transfer from flash connected to QSPI interface
Supported Combinations
Parameter | Value |
CPU + OS | m4fss0-0 freertos |
m4fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | xWRL1432-evm |
Example folder | examples/drivers/qspi/qspi_flash_transfer |
Steps to Run the Example
Sample Output
Shown below is a sample output when the application is run,
[QSPI Flash Transfer Test] Starting ...
[QSPI Flash Transfer Test] Executing Flash Erase on first block...
[QSPI Flash Transfer Test] Performing Write-Read Test...
[QSPI Flash Transfer Test] Write-Done...
[QSPI Flash Transfer Test] Read-Done...
All tests have passed!!