Introduction
This example is a application which demonstrates the LIN message communication to external PC via PLIN-USB (from PEAK Systems -> IPEH-004052) Instance LIN1 is set as a Commander in Transmit Mode.
The LIN1 instance initiates the transmission by sending LINID followed by message. The size of the message is also increased with increasing id.
Supported Combinations
Parameter | Value |
CPU + OS | r5fss0-0 freertos |
r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Boards | xWRL1432-evm |
Example folder | examples/drivers/lin/lin_external |
Steps to Run the Example
- Board Configuration, change the switch 3 on S4 to OFF mode
LIN switch 3 on S4 set to OFF
- Hardware Connectivity, connect the PLIN-USB module to PC from USB and Serial Port to be connected as mentioned in the image below.
LIN Hardware Connectivity with PLIN USB.
- Software Setup, Download and Install the PLIN-View Pro from https://www.peak-system.com/PLIN-USB.485.0.html?&L=1
- Click on LIN in the menu bar and connect to PLIN-USB. Make sure the LINMode for PLIN is Responder with Baud Rate of 19200.
LIN Hardware Connectivity with PLIN USB.
- After successful connection with PLIN-USB, the status of connection is shown as the bottom of the screen.
PLIN Connectivity status.
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
See Also
LIN
Sample Output
Shown below is a sample output when the application is run,
[LIN] LIN mode external, application started ...
[LIN] : New Data Sent = 12
[LIN] : New Data Sent = 34
[LIN] : New Data Sent = 56
[LIN] : New Data Sent = 78
[LIN] : New Data Sent = 9a
[LIN] : New Data Sent = ab
[LIN] : New Data Sent = cd
[LIN] : New Data Sent = ef
All tests have passed!!
Shown below is a sample output on PLIN-View Pro
Output on PLIN-View Pro