This example performs HWA based FFT operation on real input data.
The input to the FFT is a sinusoidal real data. This is converted to 16-bit signed fixed point data which the HWA will operate on. The HWA PaRAM sets are initialized with proper configuration for FFT. The HWA is triggered to perform the FFT operation and the frequency domain complex output is converted back to 16-bit signed data.
Parameter | Value |
---|---|
CPU + OS | m4fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | xWRL1432-evm |
Example folder | examples/drivers/hwa/hwa_real_fft |
Shown below is a sample output when the application is run,