![]() |
![]() |
This is the Monitoring report which RadarSS sends to the host, containing the measured RX noise figure values corresponding to the full IF band of a profile. RadarSS sends this to host at the programmed periodicity or when failure occurs, as programmed by the configuration API SB. Event: RL_RF_AE_MON_RX_NOISE_FIG_REPORT. More...
#include <control/mmwavelink/mmwavelink.h>
Data Fields | |
rlUInt16_t | statusFlags |
Status flags indicating pass fail results corresponding to various threshold checks under this monitor. Bit STATUS_FLAG for monitor [0] STATUS_RX_NOISE_FIGURE [15:1]RESERVED 0 - FAIL or check wasn't done, 1 - PASS . | |
rlUInt16_t | errorCode |
Indicates any error reported during monitoring Value of 0 indicates no error. | |
rlUInt8_t | profIndex |
Profile Index for which this monitoring report applies. | |
rlUInt8_t | reserved0 |
Reserved for future use. | |
rlUInt16_t | reserved1 |
Reserved for future use. | |
rlUInt16_t | rxNoiseFigVal [12U] |
TThe measured RX input referred for each enabled channel, at each enabled RF frequency is reported here. Byte numbers corresponding to different RX and RF, in this field are here: RF1 RF2 RF3 RX0 1:0 9:8 17:16 RX1 3:2 11:10 19:18 RX2 5:4 13:12 21:20 RX3 7:6 15:14 23:22 1 LSB = 0.1 dB Only the entries of enabled RF Frequencies and enabled RX channels are valid. . | |
rlUInt32_t | reserved2 |
Reserved for future use. | |
rlUInt32_t | reserved3 |
Reserved for future use. | |
rlUInt32_t | reserved4 |
Reserved for future use. | |
rlUInt32_t | timeStamp |
This field indicates when the last monitoring in the enabled set was performed. 1 LSB = 1 millisecond (the stamp rolls over upon exceeding allotted bit width) . | |
This is the Monitoring report which RadarSS sends to the host, containing the measured RX noise figure values corresponding to the full IF band of a profile. RadarSS sends this to host at the programmed periodicity or when failure occurs, as programmed by the configuration API SB. Event: RL_RF_AE_MON_RX_NOISE_FIG_REPORT.
Definition at line 3250 of file mmwavelink.h.