Readme for ARM Code Generation Tools v20.2.0.LTS
Table of Contents
ARM C/C++ CODE GENERATION TOOLS 20.2.0.LTS Release Notes
The TMS470 CGT v20.2.0.LTS release is a long term support (LTS) release. This release will be supported for roughly 2 years with periodic bug fix updates.
Compiler Documentation and Information
Documentation for the “TI ARM Optimizing Compiler User’s Guide” and the “TI ARM Assembly Language User’s Guide” is available online at:
https://www.ti.com/tool/ARM-CGT
TI E2E Community
Questions concerning TI Code Generation Tools can be posted to the TI E2E Community forums. The “Development Tools” forum can be found at:
http://e2e.ti.com/support/tools
Defect Tracking Database
Compiler defect reports can be tracked at the Development Tools bug database at:
New Features:
Hex utility --cmac option added support for --boot tables
The hex conversion utility’s Cipher-based Message Authentication Protocol (CMAC) feature now supports boot tables with CMAC tags.
To enable, use --cmac=key_file with --boot along with other required boot table options. The CMAC algorithm assumes a fill value of 1’s for gaps between boot table regions which requires setting --fill.
Hex utility --binary option
The hex convertion utility now supports output option --binary.
Hex utility --cmac option (cipher-based message authentication protocol)
The hex conversion utility supports the secure flash boot capability provided by TMS320F2838x devices, which have both C28 and ARM cores. The secure flash boot applies the Cipher-based Message Authentication Protocol (CMAC) algorithm to verify CMAC tags for regions of allocated memory.
In order to apply the CMAC algorithm to the appropriate regions in allocated memory, use the hex conversion utility as follows: --cmac=file where file contains a 128-bit hex CMAC key
NOTE: above additionally requires --image or --load_image options.
CMAC tag locations need to be defined in the user’s C code using below symbols along with LOCATION and RETAIN pragmas: secure boot regions: cmac_sb_1 cmac_sb_2 cmac_sb_3 or cmac_sb_4 user-specified region: cmac_all
The hex utility will then apply the CMAC algorithm to all the CMAC tags defined in the user’s C code.
See ARM Assembly Language Tools User Guide for details.
Default file extension for compiler generated object files
The default file extensions for object files created by the compiler have changed in order to prevent conflicts when C and C++ files have the same names. Object files generated from C source files have the .c.obj extension. Object files generated from C++ source files have the .cpp.obj extension.
Resolved defects
Resolved defects in v20.2.0.LTS:
ID | Summary |
---|---|
CODEGEN-7011 | Compiler intermittently fails with INTERNAL ERROR: opt2000 experienced a segmentation fault |
CODEGEN-6914 | Enum type with no enumerators fails to emit DW_AT_byte_size, crashes CCS |
CODEGEN-6810 | Parser failure with nested lambdas |
CODEGEN-6757 | Use of C++ lambda causes Dwarf debug information to be incorrect, and prevents debugging the code |
CODEGEN-6710 | MOVT/MOVW without # on constant causes assembler crash INTERNAL ERROR!: failed to locate symbol for relocation entry at offset |
CODEGEN-6682 | Combination of many include paths and .cdecls causes assembler to segmentation fault |
CODEGEN-6655 | Linker incorrectly issues the diagnostic: Use of variable-length arrays is not thread-safe |
CODEGEN-6603 | Compiler fails with Internal Error: Constant Table Error |
CODEGEN-6581 | Optimizer fails with segmentation fault |
CODEGEN-6474 | Compiler fails with diagnostic >>>> Optimizer terminated abnormally |
CODEGEN-6362 | Compiler may reassociate mixed-width addition and lose implicit wider-than-int conversion |
CODEGEN-6289 | Pointer to VLA 2D array computation in IF condition is double-adjusted and garbled |
CODEGEN-6270 | Compiler manual incorrectly lists callgraph as option for –analyze |
CODEGEN-6244 | Wrong version of __generic used under –c11 |
CODEGEN-6132 | pdd tool fails when program includes unused file |
CODEGEN-6130 | deque push_back of structure larger than 64-bytes tries to write to invalid memory location |
CODEGEN-6046 | Header file arm_acle.h is missing the matching brace for extern “C” { |
CODEGEN-6031 | Expressions/Variable view is not properly resolving some C++ symbols properly |
CODEGEN-5986 | Compiler may crash when auto as return type of uninstantiated member function in template class resolves to template parameter |
CODEGEN-5943 | Compiler may lose volatile qualifier in A->B->C when B and C are both volatile |
CODEGEN-5924 | ARM compiler error with 64-bit constant decomposed into 2 16-bit constants |
CODEGEN-5843 | Use of –check_misra=14.10 causes non-MISRA related warning to be emitted |
CODEGEN-5791 | C++ enum class with explicit type has some problems |
CODEGEN-5773 | –emit_references:file causes an internal error on Mac |
CODEGEN-5674 | Under -o4, compiler may assume a global variable is constant, if it's only set in files containing inline asm() |
CODEGEN-5574 | Loop controlled by unsigned char counter iterates more than 255 times |
CODEGEN-5563 | Checking for MISRA rule 20.1 causes macro redefinition to be ignored |
CODEGEN-5533 | Loop with Cortex-R, -mf3, and DWARF debug leads to assembler error “defined differently in each pass” |
CODEGEN-5486 | Global constexpr class errors out when assigning to member data |
CODEGEN-5333 | Emit error message when referenced placeholder routine not selected during specialization |
CODEGEN-5119 | Using #pragma RETAIN does not keep a static file level variable |
CODEGEN-4931 | Applying attribute((used)) to static variable does not work |
CODEGEN-1154 | ltoa definition conflicts with quasi-standard ltoa |
Known defects
Known defects in v20.2.0.LTS:
ID | Summary |
---|---|
CODEGEN-6509 | Compiler error: no instance of function template matches the argument list |
CODEGEN-6070 | Erroneous “redeclared with incompatible type” involving two tagless structs with same form |
CODEGEN-5179 | When a symbol is remapped, DW_TAG_TI_branch/DW_AT_name is not updated |
CODEGEN-5078 | Simple syntax error causes assembler to fail with INTERNAL ERROR |
CODEGEN-4985 | Typo on ULP Advisor message |
CODEGEN-4943 | MISRA 12.2 is incorrectly issued when one variable is used multiple times as an array index in the same expression |
CODEGEN-4934 | Incorrect issue MISRA diagnostic 10.5: If the bitwise operators ~ and << are applied |
CODEGEN-4789 | Compiler incorrectly issues MISRA diagnostic 12.7 Bitwise operators shall not be applied to operands whose underlying type is signed |
CODEGEN-4712 | No MISRA 10.1 and 10.6 diagnostics issued on initializations |
CODEGEN-4346 | MISRA 19.4 error fails to identify itself as MISRA diagnostic when problem is on the command line |
CODEGEN-4304 | C++ feature causes runtime failure on unaligned access on ARM9 |
CODEGEN-4298 | Internal error when passing a temporary array of objects |
CODEGEN-4297 | Cannot take the address of std::ctype<char>::table_size |
CODEGEN-4296 | Undefined symbol isblank with -g or -ooff |
CODEGEN-4290 | wstring runtime failure - likely bug in swprintf |
CODEGEN-4281 | Unexpected type returned by bitset [] operator |
CODEGEN-4276 | std::multimap::clear is not noexcept |
CODEGEN-4275 | std::num_get does not parse floating-point strings correctly |
CODEGEN-4259 | noexcept(typeid(d)) runtime fail on polymorphic class type |
CODEGEN-4258 | deeply nested lambda functions hang the codegen |
CODEGEN-4250 | regex_constants::ECMAScript not expected to be 0 |
CODEGEN-4248 | armcl allows non-default arguments to be specified after default arguments |
CODEGEN-4247 | Internal error when assigning default arguments to a parameter pack |
CODEGEN-4246 | armcl allows illegal attribute in friend declarations |
CODEGEN-4245 | Multiple non-variables may be declared using auto or decltype(auto) |
CODEGEN-4244 | armcl errors on legal constexpr constructor call |
CODEGEN-4234 | No error generated for lambda-expression in default argument cannot capture any entity. |
CODEGEN-4228 | armcl fails to flag an inconsistent use of alignas between a declaration and definition of an object |
CODEGEN-4203 | Parser errors on empty enum declaration |
CODEGEN-4158 | TI compiler does not emit clang error: constexpr function never produces a constant expression |
CODEGEN-4157 | error with using constexpr for return from end() with empty std::initializer_list |
CODEGEN-4132 | cannot find matching “==” operator definition |
CODEGEN-4124 | Failure to defer access control checks |
CODEGEN-4122 | decltype cannot be used as a destructor name |
CODEGEN-4119 | user-supplied allocator function is not called |
CODEGEN-4105 | cannot find definition of “>=” operator |
CODEGEN-4099 | Composing operations for valarray may fail to compile |
CODEGEN-4091 | Incomplete class type when using various members of <iterator> |
CODEGEN-4090 | Unimplemented core issue 475: std::uncaught_exception is not true when constructing the thrown object |
CODEGEN-4084 | assembler errors with bogus .iendfunc asm directive when using –c_src_interlist |
CODEGEN-4076 | Exception propagating out of noexcept function does not call std::terminate |
CODEGEN-4072 | Unimplemented core issue 1769: Catching a thrown derived class by reference to base clas |
CODEGEN-4071 | <regex> never throws error_ctype |
CODEGEN-4069 | std::linear_congruential_engine doesn't support 8-bit results |
CODEGEN-4058 | std::function<T>::target_type() should return typeid(void) if target is empty |
CODEGEN-4050 | shared_ptr::get_deleter() should return the original deleter class without copying |
CODEGEN-4044 | libcxx istreambuf_iterator points to end of string instead of character past match |
CODEGEN-4035 | Compiler allows constant subtraction between pointers to different objects |
CODEGEN-4032 | wofstream << operator unexpected termination |
CODEGEN-4026 | Non-standard partial ordering of variadic template partial specialization |
CODEGEN-4015 | Access of const static member through pointer is not a constant expression. |
CODEGEN-4002 | Undefined behavior on lambda capturing constexpr by reference |
CODEGEN-4001 | Unimplemented core issue 588: Unqualified name lookup examines dependent base class |
CODEGEN-4000 | Core 1601: Overload resolution for enum with fixed type |
CODEGEN-3999 | Unimplemented core issue 1374: Conversion sequence ranks qualification before reference binding |
CODEGEN-3998 | Unimplemented core issue 1951: cv-qualified void and scalar types are not literal types |
CODEGEN-3993 | Constant initialiation may take place before dynamic initialization |
CODEGEN-3991 | We do not issue diagnostics if an allocation function throws a non bad_alloc exception |
CODEGEN-3966 | slice_array assignment failures |
CODEGEN-3965 | Invalid conversion on static_cast from T1 to rvalue reference of T2 |
CODEGEN-3964 | Unimplemented core issue 1467: Overloads and initializations with single-element initializer_list |
CODEGEN-3963 | Unimplemented core issue 591: Name lookup in dependent base class that is also the current instantiation |
CODEGEN-3962 | Core Issue 1804 unimplemented: friend declaration does not apply to class template specializations |
CODEGEN-3961 | Pack expansion in template parameter list fails |
CODEGEN-3959 | std::reference_wrapper doesn't define argument_type for classes containing a typedef member named argument_type |
CODEGEN-3954 | Problem with std::swap and <tuple> |
CODEGEN-3953 | scoped_allocator_adaptor can't be explicitly instantiated with two arguments |
CODEGEN-3951 | Spurious error on bypassing initialization of trivially constructible objects |
CODEGEN-3948 | Spurious syntax error on alignas in alias declaration |
CODEGEN-3947 | Spurious error on unevaluated use of undefined constexpr function |
CODEGEN-3946 | Spurious error on global qualifier of struct template |
CODEGEN-3944 | Raw string d-char-sequence isn't supported |
CODEGEN-3941 | operator<<(std::basic_ostream<K,T>&, const std::error_code&) is not defined in system_error |
CODEGEN-3938 | std::rethrow_if_nested does not have standard signature |
CODEGEN-3937 | nested_exception::rethrow_nested() not supported |
CODEGEN-3916 | C++ header file cuchar is not provided in libc++ |
CODEGEN-1678 | Document #pragma once |
CODEGEN-1499 | #pragma LOCATION and palign do not work together |
CODEGEN-1498 | Automatic library build fails when an exact library name is used |
CODEGEN-1495 | Compiler and assembler disagree on format for IT instruction |
CODEGEN-1484 | The armhex command does not handle spaces in the name of the output binary |
CODEGEN-1458 | Consider splitting up unified_locale.cpp to save code space |
CODEGEN-1445 | Compiler inserts unnecessary register copy |
CODEGEN-1101 | When the imaginary part of z is INFINITY, cprojf(z) is NOT equivalent to INFINITY + I * copysign(0.0, cimagf(z)) |
CODEGEN-1059 | Compiler does not respect partial overrides in C99 designated initializers |
CODEGEN-1026 | Disable diagnostic 1558 (–float_operations_allowed diagnostic) in standard header files |
CODEGEN-989 | Should accept “LDRD R8,[R1]” in Thumb-2 mode |
CODEGEN-975 | Missing half-precision float conversion functions |
CODEGEN-974 | Missing __aeabi_read_tp |
CODEGEN-972 | Missing AEABI_COMPATIBILITY_MODE link-time constants |
CODEGEN-967 | Assembler accepts but mistranslates BLLT in v7 thumb mode |
CODEGEN-966 | Should allow “ADD R0, R1, #0xfff” for v6m0 |
CODEGEN-962 | Should accept 2-operand SUB SP in Thumb1/UAL mode |
CODEGEN-927 | Should accept 2-operand add in ARM mode |
CODEGEN-890 | The .label assembler directive should not be accepted when assembling for ELF. |
CODEGEN-830 | __aeabi_dcmpun returns 1 for Inf and -Inf |
CODEGEN-793 | Ill advised enum scalar usage gets MISRA diagnostic, but similar usage of enum array does not |
CODEGEN-792 | Array that is correctly initialized erroneously gets a MISRA diagnostic about size not being specified |
CODEGEN-753 | Warning generated when using __curpc intrinsic on Thumb 2 |
CODEGEN-662 | Double constant incorrectly converted to float changes result slightly |
CODEGEN-578 | MISRA 12.8 and MISRA 10.5 false positives |
CODEGEN-573 | Cortex-M0 library lacks uread4, etc. |
CODEGEN-322 | Structure is not initialized correctly when using -o2 or -o3 optimization |
CODEGEN-316 | The _ssat16 intrinsic allows literals in the range of 0-31, but the SSAT16 instruction only accepts values from 1-16 |
CODEGEN-315 | _ssatl intrinsic allows 3rd argument to be 0 resulting in an assembler error. |
CODEGEN-299 | ARM assembler does not issue a warning for PC-relative loads when –embedded_constants=off |
CODEGEN-237 | Linker outputting wrong build attribute name for EABI TAG_VFP_arch on ARM targets |
CODEGEN-235 | Section relative ELF symbol values in partially linking object files should hold the section offset for the symbol |
CODEGEN-104 | Linker gives misleading warning when dot expressions used in SECTION directive for .stack section |
CODEGEN-63 | DWARF does not correctly represent variables stored in register pairs |
CODEGEN-56 | Forward reference in .space generates an internal error |
CODEGEN-30 | Compilers on PC will not work without TMP set |