2.3. Release Notes - 07_00_00

2.3.1. Introduction

This release notes provides important information that will assist you in using the PDK software package. This document provides the product information and known issues that are specific to the PDK software package.

2.3.2. What’s New

ID Description Module
PDK-4940 SBL shall program the Thermal shutdown (TSHUT) values during boot SBL
PDK-5246 Boot time Security support on RTOS SDK for AM65xx and J721E Platforms SBL
PDK-6298 SciClient: Update the Sciclient_rmIrqSet and Sciclient_rmIrqRelease APIs to perform interrupt routing Sciclient
PDK-5264 Support Thumb2 mode on R5F BUILD
PDK-5372 Board: DDR software shall use EMIF/LPDDR chip support library BOARD
PDK-5367 DDR software shall support runtime refresh rate modification based on temperature feedback BOARD
PDK-5866 VTM: SW shall enable configuration of Temperature Warning CSL VTM
PDK-5366 CSL-FL: FSS Support CSL FSS
PDK-5149 Support DSS, VHWA, CSI-RX, CSI-TX on mcu2_0 instead of mcu2_1 Video Drivers
PDK-5252 AM65xx PG2: CAL Configuration option to route traffic through real time or non real time path CAL
PDK-5204 Fusion 2 board Support CSIRX
PDK-5255 CSIRX: YUV422 dataformat Support CSIRX
PDK-5253 CSI2 TX : Support for multiple virtual channel CSITX
PDK-4988 AM65xx PG2: DSS Driver update required to support yuv2rgb DSS
PDK-6486 VPAC LDC driver shall support config updates after create time VPAC
PDK-5811 PMIC: Driver shall support TPS6594x (Leo) PMIC
PDK-4966 SA2UL Driver shall be supported SA2UL
ETHFW-1201 CPSW Checksum offload support CPSW
ETHFW-1163 Directed packet support CPSW
ETHFW-1139 Tx packet control: Timestamp Enable, Domain, msg_type, sequence_id CPSW

2.3.2.1. SBL

  • Adds J721E-HS secure boot support for RTOS SDK
  • Programs thermal limits for J721E to force the SoC into reset if the max temp is reached
  • SBL “cust” build by default now only initializes MCU DOMAIN clocks & resources for a faster boot option for MCU R5 apps (J721E/J721E-HS only)
  • Added an optional set of build flags for the SBL “cust” build specifically for testing Early CAN response
  • Added a small-footprint SBL boot performance test app that works with the SBL “cust” build (MCU DOMAIN only usage)
  • Optional SBL build flag added to allow subsequent software (e.g., HLOS) to take control of the OSPI flash
  • Updated the default GTC clock rate to 200 MHz. Matches the value expected by ARM Trusted Firmware build for the Cortex-A cores.
  • SBL update added to fix occasional instability seen when the R5 reads from the OSPI flash

2.3.2.2. SYSFW

  • Security Features:
    • Official support for silicon tested J721e HS images.
    • HS Devices: Support for configuring derived KEK (DKEK) in SA2UL and enabled host access to SA2UL
    • Removed support of HSM-related features (TRNG, Asymmetric key services, and keystore)
    • Global soft lock for extended OTP
  • PM Features:
    • HW PTSTAT silicon errata workaround
  • RM Features:
    • RM board configuration now allows up to two assignments of a resource per host.
    • Added the TISCI_MSG_RM_UDMAP_FLOW_DELEGATE message to pass configuration control of common flows to other hosts.
  • Boot Time Optimizations
    • SYSFW Boot notification + Board Configuration = 6.39 ms (Within Budget of 5 ms (+/- 2 ms))
    • ROM MCU Only Boot mode support.

2.3.3. Upgrade and Compatibility

2.3.3.1. Build and Packaging

  • The PDK Jacinto package is now a combined package for both AM65xx and J721E platforms. Hence the pdk folder name in SDK reflect the family name rather than the SOC name like am65xx or j721e. Due to this the PDK_SOC variable derived from the pdk folder while sourcing pdksetupenv.sh/.bat will default to one of the SOC in the family i.e. in this case am65xx

    • This means user need to set PDK_SOC variable to the required SOC while calling pdk makefile from PDK_INSTALL_DIR/packages
  • Only the files applicable to a particular platform is packaged. This is to done to reduce the overall package size, remove unwanted files for users for better file/folder navigation and also to ensure that a file which is not applicable for a platform is not wrongly included by application

    • Due to this some of the application interface files may be missing from the package compared to last release. Users are advised to remove the inclusion of these files in their application for the respective platform builds
  • API guide for PDK is now generated for the entire PDK package instead of individual module API guides. The generated API guide is now present in PDK_INSTALL_DIR/docs/api_guide folder. This gives flexibility to give cross references across modules in PDK as well generate SOC specific documentation. Due to this API_Documentation.html present in PDK_INSTALL_DIR/packages is removed

2.3.3.2. CPSW

  • Hardware push instance number in CPTS events is now an enumeration of type CpswCpts_HwPush, not an 8-bit integer.

  • CPSW DMA TX channel params (CpswDma_UdmaChTxPrms) added boolean flags to filter out extended and protocol specific info words.

  • Exposed below UDMA ring and channel config params
    • Added Ring mode config option in CpswDma_UdmaRingPrms
    • CpswDma_UdmaFlowPrms - added boolean flags to indicate if extended or protocol specific info words.
  • CpswDma_PktInfo now has fields for packet timestamp information (CpswDma_PktTsInfo) and directed port numbers.

2.3.3.3. SBL

  • In case of AM65xx-HS build, the HS SBL image is generated under PDK_INSTALL_DIR/packages/ti/boot/sbl/binary/am65xx_evm_hs folder instead of PDK_INSTALL_DIR/packages/ti/boot/sbl/binary/am65xx_evm folder. This is done in order to support HS and GP builds in the same package.
  • In case of HS build, BUILD_HS flag need not be passed while calling make. Both the HS and GP SBL binaries gets generated by the default build procedures

2.3.3.4. Sciclient

  • Due to a System Firmware ABI change, applications using the Sciclient_rmGetResourceRange API to retrieve host processor IRQ ranges need to update the processor through which processor IRQ ranges are discovered.

    System Firmware no longer directly manages host processor input IRQs as a resource. All resources of subtype TISCI_RESASG_SUBTYPE_<destination processor IRQ interface>_IRQ_GROUPr*_FROM_<source interrupt router> have been removed.

    System Firmware now manages all interrupt router (IR) outputs directly with SoC IR output ranges managed under the resource subtype TISCI_RESASG_SUBTYPE_IR_OUTPUT

    Applications that query System Firmware for the host processor input IRQ range via the Sciclient_rmGetResourceRange() must update the types and subtypes used in the query. The processor IRQ subtypes have been removed. The query via Sciclient_rmGetResourceRange() now needs to use SoC IR types and the IR output resource subtype. Note, this requires knowledge of which IR is directly connected to the processor IRQ input range desired for configuration. The linked tables below show the resource type migration that an application using the Sciclient_rmGetResourceRange() API should make when switching from the old IRQ input resource types to the new IR output resource types.

    To facilitate backwards compatibility between the new IR output resource and the Sciclient_rmIrqSet and Sciclient_rmIrqRelease APIs which take a destination host IRQ (dst_host_irq parameter) as input the Sciclient_rmIrqTranslateIrOutput() API has been added.

    The Sciclient_rmIrqTranslateIrOutput API translates an IR output to the destination processor input IRQ value. The returned value can be provided directly to the dst_host_irq parameter of the Sciclient_rmIrqSet and Sciclient_rmIrqRelease APIs.

  • New Sciclient_rmIrqSetRaw and Sciclient_rmIrqReleaseRaw APIs have been added. These APIs allow direct programming of SoC interrupt aggregators (IA) and interrupt routers (IR) in accordance to new System Firmware interrupt management functionality.

    The existing Sciclient_rmIrqSet and Sciclient_rmIrqRelease APIs continue to function as they did before.

2.3.3.5. SYSFW

  • Interrupt management Simplification and Memory Optimization. (ABI 3.0)
  • Board configuration updates for New Security features - DKEK, SA2UL sharing. (ABI 3.0)
  • AM65x SR 1.0 RM resource assignment types are now aligned with AM65x SR 2.0 resource assignment types
  • The TISCI_MSG_RM_GET_RESOURCE_RANGE has been updated to return an additional resource range - Backward compatible.

2.3.3.6. Executing sysbios applications via CCS (no-boot mode)

  • An additional step of copying interrupt vector to ATCM is necessary
  • Refer FAQ Copy Vecs to ATCM for details

2.3.3.7. BOARD Diagnostics

  • In case of AM65xx, the board diagnostics builds are now supported from PDK top level makefile present in pdk/packages/makefile or from pdk/packages/ti/build folders
  • Board diagnostic application image location is changed from ‘pdk/packages/ti/board/bin’ to ‘pdk/packages/binary’. Refer to Board Diagnostics Documentation for more details.

2.3.3.7.1. AM65X Sciclient Interrupt Resource Type Migration Table

Old Resource Type Old Resource Subtype New Resource Type New Resource Subtype
RESASG_TYPE_GIC_IRQ RESASG_SUBTYPE_GIC_IRQ_MAIN_NAV_SET0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_GIC_IRQ_MAIN_GPIO TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_GIC_IRQ_MAIN_NAV_SET1 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_GIC_IRQ_COMP_EVT TISCI_DEV_CMPEVENT_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_GIC_IRQ_WKUP_GPIO TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
RESASG_TYPE_PULSAR_C0_IRQ RESASG_SUBTYPE_PULSAR_C0_IRQ_MCU_NAV TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_PULSAR_C0_IRQ_WKUP_GPIO TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_PULSAR_C0_IRQ_MAIN2MCU_LVL TISCI_DEV_MAIN2MCU_LVL_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_PULSAR_C0_IRQ_MAIN2MCU_PLS TISCI_DEV_MAIN2MCU_PLS_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
RESASG_TYPE_PULSAR_C1_IRQ RESASG_SUBTYPE_PULSAR_C1_IRQ_MCU_NAV TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_PULSAR_C1_IRQ_WKUP_GPIO TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_PULSAR_C1_IRQ_MAIN2MCU_LVL TISCI_DEV_MAIN2MCU_LVL_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_PULSAR_C1_IRQ_MAIN2MCU_PLS TISCI_DEV_MAIN2MCU_PLS_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
RESASG_TYPE_ICSSG0_IRQ RESASG_SUBTYPE_ICSSG0_IRQ_MAIN_NAV TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_ICSSG0_IRQ_MAIN_GPIO TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
RESASG_TYPE_ICSSG1_IRQ RESASG_SUBTYPE_ICSSG1_IRQ_MAIN_NAV TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_ICSSG1_IRQ_MAIN_GPIO TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
RESASG_TYPE_ICSSG2_IRQ RESASG_SUBTYPE_ICSSG1_IRQ_MAIN_NAV TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  RESASG_SUBTYPE_ICSSG1_IRQ_MAIN_GPIO TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT

2.3.3.7.2. AM65X SR2 Sciclient Interrupt Resource Type Migration Table

Old Resource Type Old Resource Subtype New Resource Type New Resource Subtype
AM6_DEV_MCU_CPSW0 TISCI_RESASG_SUBTYPE_MCU_CPSW0_CPTS_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_CPSW0_CPTS_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_WKUP_DMSC0_CORTEX_M3_0 TISCI_RESASG_SUBTYPE_WKUP_DMSC0_CORTEX_M3_0_NVIC_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_ESM0 TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT0_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT1_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT2_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_WKUP_ESM0 TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT0_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT1_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT2_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_GIC0 TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP1_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 TISCI_DEV_CMPEVENT_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_GIC0_SPI_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_PRU_ICSSG0 TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_SLV_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_PRU_ICSSG1 TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_SLV_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_PRU_ICSSG2 TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG2_PR1_SLV_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_NAVSS0 TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW1_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW5_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW6_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW7_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_CPTS0_HW8_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_PCIE0 TISCI_RESASG_SUBTYPE_PCIE0_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_PCIE1 TISCI_RESASG_SUBTYPE_PCIE1_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_PDMA1 TISCI_RESASG_SUBTYPE_PDMA1_LEVENT_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PDMA1_LEVENT_IN_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 TISCI_DEV_CMPEVENT_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_MCU_ARMSS0_CPU0 TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU0_INTR_IRQ_GROUP0_FROM_MCU_NAVSS0_INTR_ROUTER_0 TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU0_INTR_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU0_INTR_IRQ_GROUP0_FROM_MAIN2MCU_LVL_INTRTR0 TISCI_DEV_MAIN2MCU_LVL_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU0_INTR_IRQ_GROUP0_FROM_MAIN2MCU_PLS_INTRTR0 TISCI_DEV_MAIN2MCU_PLS_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
AM6_DEV_MCU_ARMSS0_CPU1 TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU1_INTR_IRQ_GROUP0_FROM_MCU_NAVSS0_INTR_ROUTER_0 TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU1_INTR_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU1_INTR_IRQ_GROUP0_FROM_MAIN2MCU_LVL_INTRTR0 TISCI_DEV_MAIN2MCU_LVL_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_ARMSS0_CPU1_INTR_IRQ_GROUP0_FROM_MAIN2MCU_PLS_INTRTR0 TISCI_DEV_MAIN2MCU_PLS_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT

2.3.3.7.3. J721E Sciclient Interrupt Resource Type Migration Table

Old Resource Type Old Resource Subtype New Resource Type New Resource Subtype
TISCI_DEV_COMPUTE_CLUSTER0_CLEC TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP1_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 TISCI_DEV_CMPEVENT_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP2_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_CLEC_SOC_EVENTS_IN_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_COMPUTE_CLUSTER0_GIC500SS TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP1_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 TISCI_DEV_CMPEVENT_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP2_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_COMPUTE_CLUSTER0_GIC500SS_SPI_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_MCU_CPSW0 TISCI_RESASG_SUBTYPE_MCU_CPSW0_CPTS_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_CPSW0_CPTS_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_CPSW0 TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW1_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW5_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW6_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW7_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_CPSW0_CPTS_HW8_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_ESM0 TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT0_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT1_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_ESM0_ESM_PLS_EVENT2_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_WKUP_ESM0 TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT0_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT1_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_WKUP_ESM0_ESM_PLS_EVENT2_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_PRU_ICSSG0 TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG0_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_PRU_ICSSG1 TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC0_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC0_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC1_LATCH0_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_EDC1_LATCH1_IN_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_IEP0_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_IEP1_CAP_INTR_REQ_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_PRU_ICSSG1_PR1_SLV_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_C66SS0_CORE0 TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP0_FROM_C66SS0_INTROUTER0 TISCI_DEV_C66SS0_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP1_FROM_C66SS0_INTROUTER0 TISCI_DEV_C66SS0_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP2_FROM_C66SS0_INTROUTER0 TISCI_DEV_C66SS0_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP3_FROM_C66SS0_INTROUTER0 TISCI_DEV_C66SS0_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_C66SS0_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP4_FROM_C66SS0_INTROUTER0 TISCI_DEV_C66SS0_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_C66SS1_CORE0 TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP0_FROM_C66SS1_INTROUTER0 TISCI_DEV_C66SS1_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP1_FROM_C66SS1_INTROUTER0 TISCI_DEV_C66SS1_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP2_FROM_C66SS1_INTROUTER0 TISCI_DEV_C66SS1_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP3_FROM_C66SS1_INTROUTER0 TISCI_DEV_C66SS1_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_C66SS1_CORE0_C66_EVENT_IN_SYNC_IRQ_GROUP4_FROM_C66SS1_INTROUTER0 TISCI_DEV_C66SS1_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_NAVSS512L_MAIN_0 TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW1_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW3_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW4_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW5_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW6_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW7_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS512L_MAIN_0_CPTS0_HW8_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_NAVSS0_UDMASS_INTAGGR_0 TISCI_RESASG_SUBTYPE_NAVSS0_UDMASS_INTAGGR_0_INTAGGR_LEVI_PEND_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_UDMASS_INTAGGR_0_INTAGGR_LEVI_PEND_IRQ_GROUP0_FROM_CMPEVENT_INTRTR0 TISCI_DEV_CMPEVENT_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_NAVSS0_UDMASS_INTAGGR_0_INTAGGR_LEVI_PEND_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_MCU_NAVSS0_INTAGGR_0 TISCI_RESASG_SUBTYPE_MCU_NAVSS0_INTAGGR_0_INTAGGR_LEVI_PEND_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_PCIE0 TISCI_RESASG_SUBTYPE_PCIE0_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_PCIE1 TISCI_RESASG_SUBTYPE_PCIE1_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_PCIE2 TISCI_RESASG_SUBTYPE_PCIE2_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_PCIE3 TISCI_RESASG_SUBTYPE_PCIE3_PCIE_CPTS_HW2_PUSH_IRQ_GROUP0_FROM_TIMESYNC_INTRTR0 TISCI_DEV_TIMESYNC_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_R5FSS0_CORE0 TISCI_RESASG_SUBTYPE_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_R5FSS0_INTROUTER0 TISCI_DEV_R5FSS0_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_R5FSS0_CORE1 TISCI_RESASG_SUBTYPE_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_R5FSS0_INTROUTER0 TISCI_DEV_R5FSS0_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_R5FSS1_CORE0 TISCI_RESASG_SUBTYPE_R5FSS1_CORE0_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_R5FSS1_CORE0_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_R5FSS1_CORE0_INTR_IRQ_GROUP0_FROM_R5FSS1_INTROUTER0 TISCI_DEV_R5FSS1_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_R5FSS1_CORE1 TISCI_RESASG_SUBTYPE_R5FSS1_CORE1_INTR_IRQ_GROUP0_FROM_GPIOMUX_INTRTR0 TISCI_DEV_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_R5FSS1_CORE1_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_R5FSS1_CORE1_INTR_IRQ_GROUP0_FROM_R5FSS1_INTROUTER0 TISCI_DEV_R5FSS1_INTROUTER0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_MCU_R5FSS0_CORE0 TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_MCU_NAVSS0_INTR_ROUTER_0 TISCI_DEV_MAIN2MCU_LVL_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_MAIN2MCU_LVL_INTRTR0 TISCI_DEV_MAIN2MCU_LVL_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_MAIN2MCU_PLS_INTRTR0 TISCI_DEV_MAIN2MCU_PLS_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE0_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
TISCI_DEV_MCU_R5FSS0_CORE1 TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_MCU_NAVSS0_INTR_ROUTER_0 TISCI_DEV_MCU_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_WKUP_GPIOMUX_INTRTR0 TISCI_DEV_WKUP_GPIOMUX_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_MAIN2MCU_LVL_INTRTR0 TISCI_DEV_MAIN2MCU_LVL_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_MAIN2MCU_PLS_INTRTR0 TISCI_DEV_MAIN2MCU_PLS_INTRTR0 TISCI_RESASG_SUBTYPE_IR_OUTPUT
  TISCI_RESASG_SUBTYPE_MCU_R5FSS0_CORE1_INTR_IRQ_GROUP0_FROM_NAVSS0_INTR_ROUTER_0 TISCI_DEV_NAVSS0_INTR_ROUTER_0 TISCI_RESASG_SUBTYPE_IR_OUTPUT

2.3.4. Device Support

  • AM65xx EVM, AM65xx IDK, AM65xx-HS EVM (BOARD=am65xx_evm, am65xx_idk)
  • J721E EVM, J721E-HS EVM (BOARD=j721e_evm)

2.3.5. Validation Information

This release is validated on above devices for the applicable components. For details on the validated examples refer to the platform specific test report present in PDK_INSTALL_DIR/docs/test_report folder.

2.3.6. Tool Chain Information

Refer to SDK level documentation for Tool Chain and dependent component version used to validate this release.

2.3.7. Fixed Issues

ID Head Line Module Affected Versions Affected Platforms
PDK-5764 R5F MPU configuration for ATCM and BTCM is wrong in r5_mpu.xs for J721E and J7200 BUILD 06.02.00 j721e-evm
PDK-5759 Incorrect status for memory attributes in r5_mpu.xs for j721e and j7200 for DDR BUILD 06.02.00 j721e-evm
PRSDK-7244 CSL Serdes configuration for PCIE Gen2 is unreliable CSL 06.01.00 am654x-evm, am654x-idk
PRSDK-7754 LPDDR CSL-FL: Missing API to read and write thermal monitor CSL 06.02.00 j721e-evm
PDK-4959 [Boot App]Compilation Error During Boot App Build CSL 06.02.00 j721e-evm
PDK-5070 Latest Uniflash documentation is not included in the release COMMON 06.02.00 j721e-evm
PDK-6378 [DSS]DSS sample application crashes with DMSC flow DSS 06.02.00 am654x-evm
PRSDK-7735 am65xx: Need to optimize time it takes to polll for packets from udma rings on R5 EMAC 06.02.00 am654x-idk
PRSDK-8081 GPIO instance is hardcoded in GPIO driver GPIO 06.02.00 j721e-evm
PRSDK-7933 Mailbox irq does not work on mcu1_1 using dynamic allocation IPC 06.01.00 j721e-evm
PRSDK-8481 OSAL: Timer API wrongly uses HWIP clear and disable interrupts, instead of OSAL clear and disable APIs OSAL 06.03.00 am654x-evm, am654x-hsevm, am654x-idk, j721e-evm
PDK-5588 OSAL API TimerP_Params_init() initializes the Timer with wrong default clock (25MHz) OSAL 06.02.00 j721e-evm
PRSDK-8426 OSAL: SemaphoreP_postfromISR() API does not work for baremetal OSAL 06.02.00 j721e-evm
PDK-6685 Timer osal - noos - Uninitialized variable OSAL 06.02.00 j721e-evm
PRSDK-5415 RTOS: K3: fix issue in OSPI INDAC mode with interrupt enabled for J7 OSPI 05.02.00 j721e-evm
PRSDK-8301 OSPI configured in SDR mode is not stable for SBL image copies OSPI 06.02.00 j721e-evm
PDK-5600 OSPI FLash timing optimization OSPI 06.02.00 j721e-evm
PDK-6294 SA: AM65x: Unit test aborts due to memory allocation failure SA2UL 06.02.00 am654x-evm
PRSDK-8302 Board config for SBL is not setting proper value for GTC clock in MAIN domain SBL 06.02.00 j721e-evm
PDK-5733 [Boot] Certificate Parsing for X509 SBL is not fool proof SBL 06.02.00 j721e-evm
PDK-5645 SBL configures MCU DMTimer0 for 250MHz while BIOS Timer.xs expects it to be at 19.2MHz SBL 06.02.00 j721e-evm
PDK-5574 ipc: messages coming twice unexpectedly IPC 06.02.00 j721e-evm
PDK-5573 ipc: heapAlloc is not returning NULL when allocation fails IPC 06.02.00 j721e-evm
PDK-5572 ipc: echo tests: Linux vrings not properly configured for non-cached for some cores IPC 06.02.00 am654x-evm, j721e-evm
PDK-5146 IPC: tests: Board_init with pinmux config is conflicting with other test firmware IPC 06.02.00 j721e-evm
PDK-5261 [SCICLIENT] Sciclient PM functions send NULL request payloads SCICLIENT 06.02.00 am654x-evm
PDK-5033 [SCICLIENT] Alignment mismatches in C66x causes the response to not be captured correctly SCICLIENT 06.02.00 j721e-evm
PDK-4963 {SCICLIENT] Build fails intermittendly SCICLIENT 06.02.00 j721e-evm
PDK-4948 Launch.js file fails when running OSPI boot mode SCICLIENT 06.02.00 j721e-evm
PDK-4994 [UDMA] Proxy access fails when using CPSW LLD from QNX UDMA 06.02.00 am654x-evm, j721e-evm
PDK-6522 udma - Ring occupancy becoming negative UDMA 06.02.00 j721e-evm
PDK-5221 Spurious Interrupts observed for MSC & other modules in VPAC VHWA 06.01.00 j721e-evm
PDK-5804 VPAC VISS H3A driver does not check for invalid parameters VHWA 06.02.00 j721e-evm
PDK-6701 [VISS]:Edge Enhancer does not work for YUV422 output VHWA 06.02.00 j721e-evm
PRSDK-7492 Uniflash requires extra Serial-Cable Unplug/Re-plug step during operation UNIFLASH 06.01.00 am654x-evm, am654x-hsevm, am654x-idk
PDK-5262 [BOARD LIB]UB960 pattern generation API programs UB960 in case of error BOARD 06.02.00 j721e-evm
PDK-5147 [Board Lib]Board lib does not support more the 1 active I2C instances BOARD 06.02.00 j721e-evm
PDK-5016 [j721e board] Serdes config function uses serdesInstance value for phyInstance BOARD 06.02.00 j721e-evm
PRSDK-7908 R5 Board Diagnostics Apploader crashes BOARD DIAG 06.02.00 am654x-evm, am654x-hsevm, am654x-idk, j721e-evm
PRSDK-7889 Audio DC diagnostic test failure BOARD DIAG 06.01.00 j721e-evm
PRSDK-7176 AM65x R5 diagnostic tests are hanging while running from diag framework BOARD DIAG 06.01.00 am654x-evm, am654x-idk
PRSDK-4661 AM65x: Board diagnostics LCD touchscreen test reports incorrect number of touch events BOARD DIAG 05.01.00 am654x-evm, am654x-hsevm, am654x-idk
ETHFW-1570 CPSW DMA - Ring monitor not allocated even though enabled by an application CPSW 06.02.00 j721e-evm
ETHFW-1564 ETHFW-1564 - Examples - Sciclient_rmIrqSet fails for mcu2_1 examples due IR conflict CPSW 06.02.00 j721e-evm
ETHFW-1496 CPSW PHY: dp83867: Robust auto-mdix is disabled for non-loopback mode CPSW 06.02.00 j721e-evm
ETHFW-1497 CPSW - MAC reset is not released in SGMII 100/10 Mbps mode CPSW 06.02.00 j721e-evm

2.3.8. Known Issues

ID Head Line Module Reported in Release Affected Platforms Impact Workaround in this release
PDK-6549 MCU2 core diagnostic tests not running through sbl BOARD 07.00.00 j721e_evm None Use CCS/JTAG to run the tests
PDK-6548 Display port (eDP) diagnostic test failure BOARD 07.00.00 j721e_evm None Use display sample application
PDK-6707 PCIe diagnostic test failure BOARD 07.00.00 am65xx_evm, am65xx_idk None Use PCIe driver sample application
PRSDK-7891 CPSW RGMII diagnostic test failure BOARD 06.01.00 j721e-evm None None
PRSDK-8607 Board_init(SBL_PLL_INIT) is configuring PLL directly without going through SYSFW. BOARD 06.03.00 am654x-idk, am64x-evm None Comment below lines of code from Board_PLLInitAll() (pdk/packages/ti/board/src/evmKeystone3) Board_PLLConfig(&pllcConfigs[CSL_PER0_PLL]); Board_PLLConfig(&pllcConfigs[CSL_MCU_PLL]); Board_PLLConfig(&pllcConfigs[CSL_CPSW_PLL]);
PDK-6762 CSL: UART test fails for MCU 1_0 CSL 07.00.00 am65xx_evm, j721e_evm Low. There are other CSL examples that output to UART without any issue. Additionally, this test works fine for MPU1_0. Suspect this is a CSL example application. Use UART driver in baremetal mode
PDK-6800 AM65: Watchdog timer diagnostic test fails DIAG 07.00.00 am65xx_evm The watchdog timer has been tested successfully on AM65 using CSL test. Suspect the diagnostics test may have a timing issue None
PDK-5224 Active DP -> HDMI adapter doesn’t work DSS 00.09.01 j721e_evm DP to HDMI adapter for display cannot be used. None
PDK-5040 Display stops working if two pipelines are started back to back DSS 06.02.00 j721e_evm None, if the workaround is in place. Wait for a frame to go out from a pipeline before starting the next one
PDK-6734 am65xx: emac: Driver updates to support wire clock feature in TX CFG EMAC 07.00.00 am65xx_idk There will be jitter in the inter arrival packet gap when transmitting packets at a high data rate None
PRSDK-5022 am65xx: Running emac unit test on R5 core from ddrless SBL at times does not complete execution EMAC 05.02.00 am654x-evm, am654x-idk Running emac unit test which does not access DDR from SBL does not finish execution, this unit test only added to run on R5 core None
PDK-6791 i2c eeprom smp testapp load fails I2C 07.00.00 am65xx_evm The issue is most likely a application configuration or test setup issue as other SMP applications are working fine None. Use non-SMP mode
PDK-6742 McASP regression test app some tests are failing McASP 07.00.00 am65xx_evm The issue is most likely a application configuration None
PDK-6743 McASP SMP tests fails McASP 07.00.00 am65xx_evm, j721e_evm The issue is most likely a application configuration or test setup issue as other SMP applications are working fine None. Use non-SMP mode
PRSDK-5074 McASP driver hangs with small buffer size McASP 05.01.00 am654x-evm, j721e-evm None Use packet size 32 samples or greater
PDK-6649 Timer osal - noos - Timer delete doesn’t “free” timer OSAL 06.02.00 j721e_evm Resource leak if create/delete called in a loop. But typically this is not done for Timer. Use the same timer in the application without create/deleting multiple times
PDK-6534 Timer osal - noos - Timer should be reset first before registering interrupts OSAL 06.02.00 j721e_evm None if the workaround is in place Reset the timer before using
PDK-6758 pcie qos examples fails for 2 lane configuration PCIE 07.00.00 am65xx_idk None None
PRSDK-8036 PCIE-0: Intermittent failures during Gen 3 mode on AM65x PG2.0 PCIE 06.02.00 am654x-evm, am654x-idk None None
PDK-6415 PMIC: Need to support asynchronous interrupts PMIC 07.00.00 j721e_evm Asynchronous Interrupt feature is not supported None
PDK-6440 PMIC: SBL test for GPIO Interrupts on Pins 3 and 4 are causing Hang on J721 EVM PMIC 07.00.00 j721e_evm GPIO Pin 3 and 4 is not supported while testing with SBL GPIO Pin 3 and 4 functionalities can be tested using CCS
PDK-6439 PMIC: GPIO Interrupt tests on Pin 7, 9 and 11 are failing PMIC 07.00.00 j721e_evm GPIO Interrupt feature for Pin 7, 9 11 is not supported GPIO Interrupt feature for other Pins except 7, 9 11 is supported
PDK-6757 PMIC: SBL test for RTC unit tests results in hang for mcu1_1 core PMIC 07.00.00 j721e_evm PMIC RTC Test application fails while testing with SBL PMIC RTC Test application is supported on muc1_1 core using CCS
PRSDK-6382 SBL: R5F: Core 1 boot is not working with unsigned binary with ipc images SBL 06.01.00 am654x-evm None None
PRSDK-5448 SBL boot from MMCSD fails intermittently SBL 05.02.00 am654x-evm, am654x-idk None

The workaround involves configuring the MMCSD driver in DS mode instead of the default HS mode. This can be done by making the below change in SBL’s mmcsd config file pdk/packages/ti/boot/sbl/src/mmcsd/sbl_mmcsd.c#n232

Before calling the function MMCSD_socSetInitCfg(), insert the below line hwAttrsConfig.supportedModes = MMCSD_SUPPORT_SD_DS; Rebuild the MMCSD SBL image (sbl_mmcsd_img) cd pdk_<ver>/packages/ti/build make sbl_mmcsd_img_clean BOARD=<board> CORE=mcu1_0 make sbl_mmcsd_img BOARD=<board> CORE=mcu1_0

Use the sbl_mmcsd_img built above

PRSDK-5626 OSPI Read using UDMA fails on AM65x HS devices. SBL 05.03.00 am654x-hsevm None Non-DMA mode could be used for the read operation
PDK-6789 MCU/Main NAVSS UDMA memcpy from L2SRAM fails UDMA 07.00.00 j721e_evm Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location Use ring memory from non-L2SRAM location
PRSDK-5989 USB Host MSC test hangs in SMP mode on AM65xx IDK board USB 06.00.00 am654x-idk None None. Use non-SMP mode
PDK-5228 Output mismatch when each region requiring 3 TRs VHWA 01.00.00 j721e_evm In multi-region mode with more then 3 TR per region can’t be used In multi-region mode for each region less than 3 TR should be used
PDK-5226 DOF generated wrong output with SOF if pixel in all row are not enabled VHWA 01.00.00, 00.09.01 j721e_evm When using the SOF if the Paxel rows without any pixel enabled is not in consecutive pair with lead to lead to output mismatch This issue is due to shift in flowvector out buffer. While generating the SOF binary map make sure that Paxel rows without any pixel enabled should be in consecutive pair
PDK-5217 VPAC VISS driver doesn’t support several valid mux combinations for outputs VHWA 01.00.00, 00.09.01 j721e_evm VISS output with Chroma only and one of the RGB component enabled may not work Enable YUV420 instead of Chroma only while using RGB component

2.3.9. Limitations

  • Active DP -> HDMI adapter doesn’t work. As a workaround use the display that supports Active DP