7.2. Boot using secondary boot loader (SBL) for AM65XX¶
7.2.1. Building the SBL¶
The secondary boot loader (SBL) prebuilt images are packaged at pdk_<device>_<version>/packages/ti/boot/sbl/binary/am65xx_evm folder. If there is a need to be built from source.
Do below to build SBL
cd pdk_<device>_<version>/packages/ti/build make -s sbl_mmcsd_img make -s sbl_ospi_img make -s sbl_uart_img
The generated pdk binaries will be present at
pdk_<device>_<version>/packages/ti/boot/sbl/binary/am65xx_evm
7.2.2. SD Boot Mode¶
7.2.2.1. Prepare a bootable SD card¶
Important
In Linux GUI tool like gparted (sudo apt install gparted) can be used.
Below instruction are for windows, in Linux, apply same parameters when formating the SD card
7.2.2.1.1. Option 1: Using windows command prompt¶
Ensure empty SD card (at least 256MB, preferably 8GB SDHC) is available.
Ensure SD memory card reader is available.
Create a primary FAT partition on MMC/SD card (FAT32 format with sector size 512) and mark it as Active. A partition manager utility has to be used for the same.
Format SD card from DOS command line as below.
format <drive> /A:512 /FS:FAT32
Make SD card partition as active using tool at this page http://www.pcdisk.com/download.html
7.2.2.1.2. Option 2: Using Diskpart¶
Open windows 7 Command prompt and Run as Administrator mode
Enter command “diskpart.exe”
C:\Windows\system32>diskpart.exe will take you DISKPART prompt Warning: Enter below command carefully w.r.t your computer/laptop SD card disk number. Choosing wrong disk number may delete data present in other drive To list all disk drive present on computer DISKPART> list disk Select the SD card disk number, in my case it is disk 1 DISKPART> select disk 1 Now all next command applicable only to disk 1(SD card) Delete entire partition DISKPART> clean To create Primary partition DISKPART> create partition primary To list partition DISKPART> list partition Select partition DISKPART> select partition 1 To list volume DISKPART> list volume Select volume associated with SD card, In my case its 3 DISKPART> select volume 3 Format SD card, please wait this may take few seconds DISKPART>format quick fs=fat32 unit=512 label=SD_BOOT Make disk active DISKPART> active To exit utility DISKPART> exit
7.2.2.2. Copy files to SD card¶
When the boot switches are set to the SD boot mode, ROM bootloader will look for the bootable images in the SD card. We need to put the bootloader image, system firmware image and the application images in the SD card.
bootloader Image for SD boot is
pdk_<device>_<version>/packages/ti/boot/sbl/binary/am65xx_evm/mmcsd/bin/sbl_mmcsd_img_mcu1_0_release.tiimage
Rename this file to tiboot3.bin
The system firmware image is
pdk_<device>_<version>/packages/ti/sciclient/soc/V0/sysfw.bin
The Application image to boot should be renamed to app
Copy the files ** tiboot3.bin, sysfw.bin and app ** to the SD card root folder to boot from SD card.
7.2.3. OSPI Boot Mode¶
Download and install the latest Uniflash version from https://www.ti.com/tool/UNIFLASH
Follow steps at Uniflash User Guide to flash the binaries.
After successful flashing, configure boot switches to OSPI boot mode and reset the board
Image Type
Offset
Binary name
SBL
0x0
pdk_<device>_<version>/packages/ti/boot/sbl/binary/am65xx_evm/ospi/bin/sbl_ospi_img_mcu1_0_release.tiimage
System Firmware
0x80000
pdk_<device>_<version>/packages/ti/drv/sciclient/soc/V0/sysfw.bin
App Image
0x100000
Application image, eg: udma_memcpy_testapp_mcu1_0_release.appimage
Note
Use MCU UART port for programming.
When using UART boot mode for programming the flash writer make sure you are using “-i 0” in command e.g. “dslite.bat –mode processors -c <COM_Port> -f <Path_to_the_flash_writer_to_be_transfered> -i 0”