2.2. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layertool-setup.sh -f <config>
The following config files are located in the configs/processor-sdk
directory of the oe-layersetup git repo.
| Config File | Description | Supported machines/platforms | |
|---|---|---|---|
| processor-sdk-08.00.00.21-config.txt | Processor SDK 08.00.00.21 Release | am64xx-evm | |