5.3. Developer Notes¶
- 5.1.2. Connect to an EVM via Telnet
- 5.1.3. How to Setup a Samba Server
- 5.1.4. Moving Files to the Target System
- 5.2.1. SDK File System Optimization/Customization
- 5.3.1. How to verify IPC between Linux and MCU R5 in Keystone devices?
- 5.3.2. How to configure K3 MSMC memory for use as SRAM or L3 cache?
- 5.3.3. How to check some device tree information from user-space of Linux?
- 5.3.4. How do I integrate a different version of open source software than what is packaged in Processor SDK?
- 5.1.1. How to Build a Ubuntu Linux host under VMware
- 5.1.5. K3 Resource Partitioning Tool