3.2.2.5. CPSW3g¶
- Introduction
- Driver Configuration
- Device tree bindings
- Multi MAC mode
- Multi port Switch mode
3.2.2.5.1. Introduction¶
The TI AM64x family of devices have multi port Gigabit Ethernet Switch subsystem. SoCs may have more than 2 external port with selectable RGMII and RMII interfaces and an internal Communications Port Programming Interface (CPPI) port (Host port 0). Host Port 0 CPPI Packet Streaming Interface interface supports 8 TX channels and one RX channel DMA channel.
Multi port Gigabit Ethernet Switch subsystem support both independent MAC mode of operation supporting multiple independent Ethernet interfaces with complete isolation (no packet switching between external ports), or can be configured in Switch mode with IEEE 802.1Q HW bridge in managed or learning mode between each of the individual MAC ports.
The driver follows the standard Linux network interface architecture and supports the following features:
- Mulitple indpendent MAC mode
- Switch mode as per IEEE 802.1Q
- Cut Through forwarding in Switch mode
- 10/100/1000 Mbps mode of operation.
- Auto negotiation.
- Linux NAPI support
- VLAN filtering
- Ethertool
- CPTS/PTP as per 802.1AS-2011 (TSN)
- EST/TAS offload as per 802.1Q-2018 (TSN)
- IET/preemption offload as per 802.1Q-2018 (TSN)
- Forwarding and Queuing Enhancements for Time-Sensitive Streams (FQTSS) as per 802.1Q-2018 previously referred to as CBS or 802.1Qav
Note
Default mode of operation is multiple indpendent MAC ports.
3.2.2.5.1.1. Supported platforms¶
| SoC | Number of external ports |
|---|---|
| AM64X | 2 external port (CPSW3g) |
3.2.2.5.2. Driver Configuration¶
Default SDK build will have these configurations enabled. In case of custom builds, please ensure following configs are enabled.
CONFIG_TI_K3_AM65_CPSW_NUSS
CONFIG_TI_K3_AM65_CPSW_SWITCHDEV
CONFIG_TI_K3_AM65_CPTS
CONFIG_TI_DAVINCI_MDIO
CONFIG_TI_CPSW_ALE
CONFIG_TI_AM65_CPSW_TAS
Module Build
Module build for the cpsw driver is supported. To do this, use option ‘m’ for above configs, where applicable.
3.2.2.5.3. Device tree bindings¶
The DT bindings description can be found at:
3.2.2.5.4. Multi MAC mode¶
Note
This section documents Independent MAC mode of operation with CPSW3g.
Bringing Up interface
The network interface can be configured automatically depending on root file system or configured manually. Manual configuration:
ip addr add 192.168.1.1/24 dev eth0
ip link set dev eth0 up
< or >
ifconfig eth0 <ip> netmask <mask> up
Get driver information
The MCU_CPSW0 interface can be identified by using ethtool -i|--driver command.
It also provides some information about supported features.
# ethtool -i <dev>
driver: am65-cpsw-nuss
version: 0.1
firmware-version:
expansion-rom-version:
bus-info: 46000000.ethernet
supports-statistics: yes
supports-test: no
supports-eeprom-access: no
supports-register-dump: yes
supports-priv-flags: yes
ethtool - Display standard information about device/link
# ethtool eth0
Supported ports: [ TP MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Half 1000baseT/Full
Supported pause frame use: Symmetric Receive-only
Supports auto-negotiation: Yes
Supported FEC modes: Not reported
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Half 1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Advertised FEC modes: Not reported
Link partner advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
Link partner advertised pause frame use: Symmetric
Link partner advertised auto-negotiation: Yes
Link partner advertised FEC modes: Not reported
Speed: 100Mb/s
Duplex: Full
Port: MII
PHYAD: 0
Transceiver: internal
Auto-negotiation: on
Supports Wake-on: d
Wake-on: d
Current message level: 0x00000000 (0)
Link detected: yes
RX checksum offload
The Driver enables RX checksum offload by default. It can be disabled/enabled by using ethtool -K command:
# ethtool -k <dev>
....
rx-checksumming: on
ethtool -K <dev> rx-checksum on|off
VLAN Config
VLAN can be added/deleted using ip or vconfig utility.
VLAN Add
ip link add link eth0 name eth0.5 type vlan id 5
< or >
vconfig add eth0 5
VLAN del
ip link del eth0.5
< or >
vconfig rem eth0 5
VLAN IP assigning
IP address can be assigned to the VLAN interface either via udhcpc
when a VLAN aware dhcp server is present or via static ip assigning
using ip or ifconfig.
Once VLAN is added, it will create a new entry in Ethernet interfaces like eth0.5, below is an example how it check the vlan interface
ip addr add 192.168.1.1/24 dev eth0.5
< or >
ifconfig eth0.5
....
eth0.5 Link encap:Ethernet HWaddr 20:CD:39:2B:C7:BE
inet addr:192.168.10.5 Bcast:192.168.10.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
VLAN Packet Send/Receive
To Send or receive packets with the VLAN tag, bind the socket to the proper Ethernet interface shown above and can send/receive via that socket-fd.
Multicast Add/Delete
Multicast MAC address can be added/deleted using ip maddr commands or Linux socket ioctl SIOCADDMULTI/SIOCDELMULTI.
Show muliticast address
# ip maddr show dev <dev>
2: eth0
link 01:00:5e:00:00:01
link 01:80:c2:00:00:00
link 01:80:c2:00:00:03
link 01:80:c2:00:00:0e
link 01:00:5e:00:00:fc
inet 224.0.0.252
inet 224.0.0.1
Add muliticast address
# ip maddr add 01:00:5e:00:00:05 dev eth0
# ip maddr show dev eth0
2: eth0
link 01:00:5e:00:00:01
link 01:80:c2:00:00:00
link 01:80:c2:00:00:03
link 01:80:c2:00:00:0e
link 01:00:5e:00:00:fc
link 01:00:5e:00:00:05 static
inet 224.0.0.252
inet 224.0.0.1
Delete muliticast address
# ip maddr del 01:00:5e:00:00:05 dev eth0
ethtool -P|--show-permaddr DEVNAME Show permanent hardware
address
# ethtool -P eth0
Permanent address: a0:f6:fd:a6:46:6e"
ethtool -s|--change DEVNAME Change generic options
Below commands will be redirected to the phy driver:
# ethtool -s <dev>
[ speed %d ]
[ duplex half|full ]
[ autoneg on|off ]
[ wol p|u|m|b|a|g|s|d... ]
[ sopass %x:%x:%x:%x:%x:%x ]
Note
CPSW driver do not perform any kind of WOL specific actions or configurations.
#ethtool -s eth0 duplex half speed 100
[ 3550.892112] cpsw 48484000.ethernet eth0: Link is Down
[ 3556.088704] cpsw 48484000.ethernet eth0: Link is Up - 100Mbps/Half - flow control off
Sets the driver message type flags by name or number
[ msglvl %d | msglvl type on|off ... ]
# ethtool -s eth0 msglvl drv off
# ethtool -s eth0 msglvl ifdown off
# ethtool -s eth0 msglvl ifup off
# ethtool eth0
Current message level: 0x00000031 (49)
drv ifdown ifup
ethtool -r|--negotiate DEVNAME Restart N-WAY negotiation
# ethtool -r eth0
[ 4338.167685] cpsw 48484000.ethernet eth0: Link is Down
[ 4341.288695] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx"
ethtool -a|--show-pause DEVNAME Show pause options
# ethtool -a eth0
Pause parameters for eth0:
Autonegotiate: off
RX: off
TX: off
ethtool -A|--pause DEVNAME Set pause options
# ethtool -A eth0 rx on tx on
cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
# ethtool -a eth0
Pause parameters for eth0:
Autonegotiate: off
RX: on
TX: on
ethtool -g|--show-ring DEVNAME Query RX/TX ring parameters
# ethtool -g eth0
Ring parameters for eth0:
Pre-set maximums:
RX: 0
RX Mini: 0
RX Jumbo: 0
TX: 0
Current hardware settings:
RX: 500
RX Mini: 0
RX Jumbo: 0
TX: 512
ethtool-l|--show-channels DEVNAME Query Channels
# ethtool -l eth0
Channel parameters for eth0:
Pre-set maximums:
RX: 1
TX: 8
Other: 0
Combined: 0
Current hardware settings:
RX: 1
TX: 8
Other: 0
Combined: 0
ethtool -L\|--set-channels DEVNAME Set Channels.
Allows to control number of TX channels driver is allowed to work with at DMA level. The maximum number of TX channels is 8.
Supported options [ tx N ]:
# ethtool -L eth0 tx 3
ethtool --show-priv-flags/--set-priv-flags DEVNAME Show/Set private flags
Allows to control private flags supported by driver.
| Flag | |
|---|---|
| p0-rx-ptype-rrobin | Controls TX DMA channels processing mode: round-robin or priority mode. In case priority mode is enabled, the high number channel will have higher priority: TX 7 - prio 7 ... TX 0 - prio 0. |
| iet-frame-preemption | Enables support for Interspersed Express Traffic (IET) IEEE 802.3br (frame preemption). |
| iet-mac-verify | Enables Interspersed Express Traffic (IET) MAC verification procedure on link up event. |
# ethtool --show-priv-flags eth0
Private flags for eth0:
p0-rx-ptype-rrobin : on
iet-frame-preemption: off
iet-mac-verify : off
# ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
Note
The network interface have to be down for private flags configuration.
ethtool -S|--statistics DEVNAME Show adapter statistics
“ethtool -S” command displays statistic for both external Port 1 and Host port 0. Host port 0 statistics prefixed with p0_.
# ethtool -S eth0
NIC statistics:
p0_rx_good_frames: 347
p0_rx_broadcast_frames: 4
p0_rx_multicast_frames: 264
p0_rx_crc_errors: 0
p0_rx_oversized_frames: 0
p0_rx_undersized_frames: 0
p0_ale_drop: 0
p0_ale_overrun_drop: 0
p0_rx_octets: 25756
p0_tx_good_frames: 4816
p0_tx_broadcast_frames: 3629
p0_tx_multicast_frames: 1120
p0_tx_octets: 878055
p0_tx_64B_frames: 735
p0_tx_65_to_127B_frames: 1023
...
rx_good_frames: 4816
rx_broadcast_frames: 3629
rx_multicast_frames: 1120
rx_pause_frames: 0
rx_crc_errors: 0
rx_align_code_errors: 0
rx_oversized_frames: 0
rx_jabber_frames: 0
rx_undersized_frames: 0
rx_fragments: 0
ale_drop: 0
ale_overrun_drop: 0
rx_octets: 878055
tx_good_frames: 347
tx_broadcast_frames: 4
tx_multicast_frames: 264
tx_pause_frames: 0
tx_deferred_frames: 0
tx_collision_frames: 0
tx_single_coll_frames: 0
tx_mult_coll_frames: 0
tx_excessive_collisions: 0
tx_late_collisions: 0
...
ethtool -T|--show-time-stamping DEVNAME Show time stamping
capabilities.
Accessible when CPTS is enabled.
# ethtool -T eth0
Time stamping parameters for eth0:
Capabilities:
hardware-transmit (SOF_TIMESTAMPING_TX_HARDWARE)
software-transmit (SOF_TIMESTAMPING_TX_SOFTWARE)
hardware-receive (SOF_TIMESTAMPING_RX_HARDWARE)
software-receive (SOF_TIMESTAMPING_RX_SOFTWARE)
software-system-clock (SOF_TIMESTAMPING_SOFTWARE)
hardware-raw-clock (SOF_TIMESTAMPING_RAW_HARDWARE)
PTP Hardware Clock: 1
Hardware Transmit Timestamp Modes:
off (HWTSTAMP_TX_OFF)
on (HWTSTAMP_TX_ON)
Hardware Receive Filter Modes:
none (HWTSTAMP_FILTER_NONE)
all (HWTSTAMP_FILTER_ALL)
ethtool --show-eee DEVNAME Show EEE settings
#ethtool --show-eee eth0
EEE Settings for eth0:
EEE status: not supported
ethtool --set-eee DEVNAME Set EEE settings.
Note
Full EEE is not supported in driver, but it enables reading and writing of EEE advertising settings in Ethernet PHY. This way one can disable advertising EEE for certain speeds.
ethtool -d|--register-dump DEVNAME Do a register dump
This command dumps all CPSW MMIO regions in the below format. The TI switch-config tool can be used for CPSW NUSS register dump parsing.
| MMIO region header (8 Bytes) | |
|---|---|
| module_id (u32) | MMIO region id NUSS = 1, RGMII_STATUS = 2, MDIO = 3, CPSW = 4, CPSW_P0 = 5, CPSW_P1 = 6, CPSW_CPTS = 7, CPSW_ALE = 8, CPSW_ALE_TBL = 9 |
| len (u32) | MMIO region dump length, including header |
| MMIO region registers dump (num_regs * 8 Bytes) | |
| reg_offset (u32) | register offset from the start of MCU NAVSS MMIO space |
| reg_value (u32) | MMIO region dump length, including header |
Exception: ALE table dumped as raw array of ALE records (3 * u32 per record).
# ethtool -d eth0
Offset Values
------ ------
0x0000: 01 00 00 00 48 00 00 00 00 00 00 00 00 71 a0 6b
0x0010: 04 00 00 00 00 00 00 00 08 00 00 00 00 00 00 00
0x0020: 0c 00 00 00 00 00 00 00 10 00 00 00 01 00 00 00
0x0030: 14 00 00 00 00 00 00 00 18 00 00 00 00 00 00 00
0x0040: 1c 00 00 00 00 00 00 00 02 00 00 00 48 00 00 00
0x0050: 30 00 00 00 0b 00 00 00 34 00 00 00 00 00 00 00
0x0060: 38 00 00 00 00 00 00 00 3c 00 00 00 00 00 00 00
...
3.2.2.5.4.1. Common Platform Time Sync (CPTS) module¶
The Common Platform Time Sync (CPTS) module is used to facilitate host control of time sync operations. It enables compliance with the IEEE 1588-2008 standard for a precision clock synchronization protocol.
The support for CPTS module can be enabled by Kconfig option CONFIG_TI_AM65_CPTS or through menuconfig tool. The PTP packet timestamping can be enabled only for one CPSW port.
When CPTS module is enabled it will exports a kernel interface for specific clock drivers and a PTP clock API user space interface and enable support for SIOCSHWTSTAMP and SIOCGHWTSTAMP socket ioctls. The PTP exposes the PHC as a character device with standardized ioctls which usually can be found at path:
/dev/ptpN
Supported PTP hardware clock functionality:
Basic clock operations
- Set time
- Get time
- Shift the clock by a given offset atomically
- Adjust clock frequency
Ancillary clock features
- Time stamp external events
- Periodic output signals configurable from user space
- Synchronization of the Linux system time via the PPS subsystem
Supported parameters for SIOCSHWTSTAMP and SIOCGHWTSTAMP:
SIOCSHWTSTAMP
hwtstamp_config.flags = 0
hwtstamp_config.tx_type
HWTSTAMP_TX_ON - enables hardware time stamping for outgoing packets
HWTSTAMP_TX_OFF - no outgoing packet will need hardware time stamping
hwtstamp_config.rx_filter
HWTSTAMP_FILTER_NONE - time stamp no incoming packet at all
HWTSTAMP_FILTER_ALL - time stamp any incoming packet
CPTS PTP packet timestamping default configuration when enabled (SIOCSHWTSTAMP):
CPSW_PN_TS_CTL_REG
TS_MSG_TYPE_EN = 0xF (Sync, Delay_Req, Pdelay_Req, and Pdelay_Resp.)
TS_TX_ANNEX_F_EN = 1
TS_TX_ANNEX_E_EN = 1
TS_TX_ANNEX_D_EN = 1
TS_TX_VLAN_LTYPE1_E = 1
CPSW_PN_TS_CTL_LTYPE2_REG
TS_TTL_NONZERO = 1
TS_320 = 1
TS_319 = 1
TS_132 = 1
TS_131 = 1
TS_130 = 1
TS_129 = 1
TS_107 = 1
TS_LTYPE1 = 0x88F7 (ETH_P_1588)
CPSW_PN_TS_SEQ_LTYPE_REG
TS_SEQ_ID_OFFSET = 0x1e
TS_LTYPE1 = 0x88F7 (ETH_P_1588)
CPSW_PN_TS_VLAN_LTYPE_REG
TS_VLAN_LTYPE1 = 0x8100 (ETH_P_8021Q)
For more information about PTP clock API and Network timestamping see Linux kernel documentation
Testing using ptp4l tool from linuxptp project
To check the ptp clock adjustment with PTP protocol, a PTP slave (client) and a PTP master (server) applications are needed to run on separate devices (EVM or PC). Open source application package linuxptp can be used as slave and as well as master. Hence TX timestamp generation can be delayed (especially with low speed links) the ptp4l “tx_timestamp_timeout” parameter need to be set for ptp4l to work.
- create file ptp.cfg with content as below:
[global]
tx_timestamp_timeout 400
- pass configuration file to ptp4l using “-f” option:
ptp4l -E -2 -H -i eth0 -l 6 -m -q -p /dev/ptpN -f ptp.cfg
- Slave Side Examples
The following command can be used to run a ptp-over-L4 client on the evm in slave mode
./ptp4l -E -4 -H -i eth0 -s -l 7 -m -q -p /dev/ptpN
For ptp-over-L2 client, use the command
./ptp4l -E -2 -H -i eth0 -s -l 7 -m -q -p /dev/ptpN
- Master Side Examples
ptp4l can also be run in master mode. For example, the following command starts a ptp4l-over-L2 master on an EVM using hardware timestamping,
./ptp4l -E -2 -H -i eth0 -l 7 -m -q -p /dev/ptpN
On a Linux PC which does not support hardware timestamping, the following command starts a ptp4l-over-L2 master using software timestamping.
./ptp4l -E -2 -S -i eth0 -l 7 -m -q
Testing using testptp tool from Linux kernel
- get the ptp clock time
# testptp -d /dev/ptpN -g
clock time: 1493255613.608918429 or Thu Apr 27 01:13:33 2017
- query the ptp clock’s capabilities
# testptp -d /dev/ptpN -c
capabilities:
10000000 maximum frequency adjustment (ppb)
0 programmable alarms
4 external time stamp channels
2 programmable periodic signals
1 pulse per second
0 programmable pins
0 cross timestamping
- Sanity testing of cpts ref frequency
Time difference between to testptp -g calls should be equal sleep time
# testptp -g -d /dev/ptpN && sleep 5 && testptp -g -d /dev/ptpN
clock time: 1493255884.565859901 or Thu Apr 27 01:18:04 2017
clock time: 1493255889.611065421 or Thu Apr 27 01:18:09 2017
- shift the ptp clock time by ‘val’ seconds
# testptp -g -d /dev/ptpN && testptp -t 100 && testptp -g -d /dev/ptpN
clock time: 1493256107.640649117 or Thu Apr 27 01:21:47 2017
time shift okay
clock time: 1493256207.678819093 or Thu Apr 27 01:23:27 2017
- set the ptp clock time to ‘val’ seconds
# testptp -g -d /dev/ptpN && testptp -T 1000000 && testptp -g -d /dev/ptpN
clock time: 1493256277.568238925 or Thu Apr 27 01:24:37 2017
set time okay
clock time: 100.018944504 or Thu Jan 1 00:01:40 1970
- adjust the ptp clock frequency by ‘val’ ppb
# testptp -g -d /dev/ptpN && testptp -f 1000000 && testptp -g -d /dev/ptpN
clock time: 151.347795184 or Thu Jan 1 00:02:31 1970
frequency adjustment okay
clock time: 151.386187454 or Thu Jan 1 00:02:31 1970
Example of using Time stamp external events
Timestamping of external events can be tested using testptp tool. Before testing the proper CPTS signal routing has to be done by using timesync router in DT.
For example, output of GENF0 can be routed to HW3_TS_PUSH_EN input. It’s required to rebuild kernel with below changes first
#define TS_OFFSET(pa, val) (0x4+(pa)*4) (0x80000000 | val)
×ync_router {
pinctrl-names = "default";
pinctrl-0 = <&mcu_cpts>;
/* Example of the timesync routing */
mcu_cpts: mcu_cpts {
pinctrl-single,pins = <
/* pps [cpts genf0] in12 -> out24 [cpts hw4_push] */
TS_OFFSET(24, 12)
>;
};
};
Then execute:
# testptp -d /dev/ptpN -p 500000000 -i 0
# testptp -d /dev/ptpN -e 100 -i 2
event index 2 at 384.250000025
event index 2 at 384.750000025
event index 2 at 385.250000025
event index 2 at 385.750000025
PPS Pulse Per Second support
The default PPS support for AM64x depends on TI SCI system firmware configuration which may put timesync_router IO space under firewall in which case the Linux can not configure timesync_router. In such case, the timesync_router has to be configured from Core for which timesync_router IO space access is allowed and Linux DT should provide CPTS “ti,pps” property configuration.
The PPS support for AM64x can be enabled by adding below changes to the board DT file to route CPSWxG CPTS GENF1 output to HW3_TS_PUSH_EN input, for example:
k3-am654-base-board.dts
#define TS_OFFSET(pa, val) (0x4+(pa)*4) (0x80000000 | val)
×ync_router {
pinctrl-names = "default";
pinctrl-0 = <&mcu_cpts>;
/* Example of the timesync routing */
mcu_cpts: mcu_cpts {
pinctrl-single,pins = <
/* pps [cpts genf1] in13 -> out25 [cpts hw4_push] */
TS_OFFSET(25, 13)
>;
};
};
&mcu_cpsw {
...
cpts {
ti,pps = <3 1>;
};
};
The PPS support for AM64x is enabled in TI SDK by default.
Once enabled, PPS can be tested using testptp and ppstest tools:
# ./testptp -d /dev/ptp1 -P 1
pps for system time request okay
# ./ppstest /dev/pps0
trying PPS source "/dev/pps0"
found PPS source "/dev/pps0"
ok, found 1 source(s), now start fetching data...
source 0 - assert 198.000000700, sequence: 7 - clear 0.000000000, sequence: 0
source 0 - assert 199.000000700, sequence: 8 - clear 0.000000000, sequence: 0
TI AM65x switch-config tool
The TI Processor SDK includes precompiled correct version of AM64x switch-config tool.
The TI AM64x switch-config tool sources for AM64x SoC can be found at:
git@git.ti.com:switch-config/switch-config.git
branch:
origin/am65x-v1.0
Usage:
# switch-config -h
Switch configuration commands.....
switch-config -I,--ndev <dev> <command>
commands:
switch-config -d,--dump-ale :dump ALE table
switch-config -D,--dump=<0..9> :dump registers (0 - all)
switch-config -v,--version
dump values:
:1 - cpsw-nuss regs
:2 - cpsw-nuss-rgmii-status regs
:3 - cpsw-nuss-mdio regs
:4 - cpsw-nu regs
:5 - cpsw-nu-p0 regs
:6 - cpsw-nu-p1 regs
:7 - cpsw-nu-cpts regs
:8 - cpsw-nu-ale regs
:9 - cpsw-nu-ale-tbl regs
Example, ALE table dump:
# switch-config -d
K3 cpsw dump version (1) len(6328)
ALE table dump ents(64):
0 : type: vlan , vid = 0, untag_force = 0x3, reg_mcast = 0x0, unreg_mcast = 0x0, member_list = 0x3
1 : type: ucast, addr = f4:84:4c:eb:a0:00, ucast_type = persistant, port_num = 0x0, Secure
2 : type: mcast, addr = ff:ff:ff:ff:ff:ff, mcast_state = f, no super, port_mask = 0x3
3 : type: mcast, addr = 01:00:5e:00:00:01, mcast_state = f, no super, port_mask = 0x3
4 : type: mcast, addr = 01:80:c2:00:00:00, mcast_state = f, no super, port_mask = 0x3
5 : type: mcast, addr = 01:80:c2:00:00:03, mcast_state = f, no super, port_mask = 0x3
6 : type: mcast, addr = 01:80:c2:00:00:0e, mcast_state = f, no super, port_mask = 0x3
8 : type: mcast, addr = 01:00:5e:00:00:fc, mcast_state = f, no super, port_mask = 0x3
9 : type: ucast, vid = 0, addr = 9c:b6:d0:89:0d:85, ucast_type = touched , port_num = 0x1
26 : type: ucast, vid = 0, addr = c4:71:54:a9:6e:b4, ucast_type = touched , port_num = 0x1
27 : type: ucast, vid = 0, addr = 00:25:22:a9:4c:b3, ucast_type = touched , port_num = 0x1
Example, CPTS registers dump:
switch-config -D7
K3 cpsw dump version (1) len(6328)
cpsw-nu-cpts regdump: num_regs(38)
0003d000:reg(4E8A2109)
0003d004:reg(00000C21)
0003d008:reg(00000000)
0003d00c:reg(00000000)
0003d010:reg(7EA3BA9B)
0003d014:reg(00000000)
0003d018:reg(00000000)
0003d01c:reg(00000000)
0003d020:reg(00000000)
0003d024:reg(00000000)
0003d028:reg(00000001)
0003d02c:reg(00000000)
0003d030:reg(00000000)
0003d034:reg(C7298A99)
0003d038:reg(03300000)
0003d03c:reg(00000000)
0003d040:reg(0000028E)
0003d044:reg(00000000)
0003d048:reg(00000000)
3.2.2.5.4.2. Enhancements for Scheduled Traffic (EST) Offload¶
IEEE 802.1Qbv/D2.2 Enhancements for Scheduled Traffic (EST), Formerly known as Time Aware Shaper (TAS), is an enhancement to Transmission Selection algorithm defined in 802.1Q standard. It became formally part of 802.1Q-2018 edition of the standard. As per standard, a Bridge or an end station may support enhancements that allow transmission from each queue to be scheduled relative to a known timescale. In order to achieve this, a transmission gate is associated with each queue; the state of the transmission gate determines whether or not queued frames can be selected for transmission. For a given queue, the transmission gate can be in one of two states:
- Open: Queued frames are selected for transmission, in accordance with the definition of the transmission selection algorithm associated with the queue.
- Closed: Queued frames are not selected for transmission.
In Linux, EST/TAS offload to hardware is implemented using taprio offload. Time Aware Priority Shaper (TAPRIO) TAPRIO, is a qdisc that implements a simplified version of the scheduling state machine defined by IEEE 802.1Q-2018 Section 8.6.9, which allows configuration of a sequence of gate states, where each gate state allows outgoing traffic for a subset (potentially empty) of traffic classes. EST is configured using tc command. Please refer the manual page TAPRIO for more details on command syntax and description
CPSW2g h/w supports EST configuration or offload. EST is configured through tc command as described in the above manual page. User indicate “flag 2” in the command which is then parsed by taprio scheduler in net core and indicate that the command is to be offloaded to h/w. taprio then offloads the command to the driver by calling ndo_setup_tc() ndo ops.
Currently driver supports only SetGateStates operation. EST operates on a repeating time interval generated by the CPTS EST function generator. Each Ethernet port has a global EST fetch RAM that can be configured as 2 buffers, each of 64 locations or one large buffer of 128 location. In 2 buffer configuration, a ping pong mechanism is used to hold the active schedule (oper) in one buffer and new (admin) command in the other. Each 22-bit fetch command consists of a 14-bit fetch count (14 MSB’s) and an 8-bit priority fetch allow (8 LSB’s) that will be applied for the fetch count time in wireside clocks. Driver process each of the sched-entry in the offload command and update the fetch RAM. Driver configures duration in sched-entry into the fetch count and Gate mask into the priority fetch bits of the RAM. Then configures the CPTS EST function generator to activate the schedule. Since driver uses 2 buffer configuration for fetch ram, this results in a max cycle time of ~8 msec (64 * 128 usec).
CPSW2g supports a configurable number of priority queues (up to 8) and needs to be switched to this mode from the default round robin mode before EST can be configured. User configures these through ethtool commands:- -L for changing number of queues and –set-priv-flags to disable round robin mode. Driver doesn’t enable EST if pf_p0_rx_ptype_rrobin privat flag is set. The flag is common for all ports, and so can’t be just overridden by taprio configuration w/o user involvement. Command fails if pf_p0_rx_ptype_rrobin is already set in the driver. Also note that –set-priv-flags ethtool can be execute only when the Ethernet interface is down. So execute ifconfig down or equivalent command before execute the ethtool command.
Schedule (commands) configuration depends on interface speed so driver translates the duration to the fetch count based on link speed. Each schedule can be constructed with several command entries in fetch RAM depending on interval. For example if each schedule has timer interval < ~128us on 1G link then each sched consumes one command and have 1:1 mapping. When Ethernet link goes down, driver purge the configuration if link is down for more than 1 second.
example schedule
- An example configuration with 3 schedule entries given below:-
- Uses 3 Queues (Q0-Q2). Each Q has a Gate associated in h/w. Maximum 8 Queues/Gates supported
- 2 higher priority Gates open for 125usec (Q1 and Q2) each about 10 packets
- Q7 is the highest priority Queue and Q0 is the lowest priority
- 1 lower priority (Q0) opens remaining gates for 250 usec
Here are the steps to configure this schedule.
#Setup interface and queue configuration
ip link set dev eth0 down
ethtool -L eth0 tx 3
#disable rrobin
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
#bring up eth0 interface
ip link set dev eth0 up
#Setup EST schedule with 3 Gates (Q0-Q2). For description of Command parameters, see manual page for taprio.
#TC0 <-> Q0, TC1 <-> Q1, and TC2 <-> Q2
tc qdisc replace dev eth0 parent root handle 100 taprio \
num_tc 3 \
map 0 0 1 2 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 1@2 \
base-time 0000 \
sched-entry S 4 125000 \
sched-entry S 2 125000 \
sched-entry S 1 250000 \
flags 2
#Where num_tc is same as number of queues = 3, map, maps 16 priorities to one of 3 TCs, queues specify the
#Queue associated with each TC, TC0 - One queue @0, TC1 - One queue @1 and TC2 - One queue @2
# sched-entry S 4 125000
# S - SetGateStates operation
# 4 - Bit mask showing bit 2 set (Q2/TC2)
# 125000 - 125000 nsecs (125 usecs ) duration of Gate open
# The cycle-time is 500 msec
#enable classifier. Classifier is used to mark the packet based on packet meta data. For example UDP port
#number
tc qdisc add dev eth0 clsact
#Using tc filter command edit the SKB priority based on udp port number. i.e Udp port 5003 -> prio 3 (TC2/Q2), port 5002 -> prio 2 (TC1/Q1), 5001 -> prio 1( TC0/Q0)
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5001 0xffff action skbedit priority 1
#Network core and Driver uses the skb priority to deliver frames to specific h/w queues. In the above case,
#priority 3 SKB (packet) goes to Q2 (4th entry in map in the tc qdisc command), priority 2 SKB goes to Q1
#(3rd entry in map) and priority 1 SKB goes to Q0 (2nd entry in map)
#Run 3 iperf sessions, each with udp port 5001, 5002 and 5003 as
#Remote PC connected to eth0 with IP address 192.168.2.10
iperf3 -s -i30 -p5001&
iperf3 -s -i30 -p5002&
iperf3 -s -i30 -p5003&
#At DUT, start trasmission of stream using iperf3
ip addr add 192.168.2.20/24 dev eth0
ip link set dev eth0 up
iperf3 -c 192.168.2.10 -u -b100M -p 5003 -l1472 -t10 -i5&
iperf3 -c 192.168.2.10 -u -b100M -p 5002 -l1472 -t10 -i5&
iperf3 -c 192.168.2.10 -u -b100M -p 5001 -l1472 -t10 -i5&
#Capture frame using wireshark at the PC to see how EST work. The frames will be on the wire only at
#scheduled time and a periodic burst of frames will be seen every 500 milli seconds.
A sample wireshark capture for the example above is shown below
Packet highlighted are the first packet transmitted during Gate open of Q2/TC2 and are spaced apart by about 500 msec which is the cycle-time of the TAS schedule. Also there are about 9 packets transmitted during the window which is about 12 * 9 = 108 usec within the Gate open interval of 125 usec.
Guard band
CPSW2g EST H/W will transmit the frame during Gate open. If a frame happens to arrive at the h/w queue just before the Gate closes, it gets spilled over to the next schedule window. If this is not desirable, user may add a guard band between schedule window, duration of which should equal to the transmission time of a MTU frame (1518 * 8 = 12144 nsec) + 2336 nsec (TRM describes this as 292 wire clocks = 292 * 8 = 2336). This ensures that frames don’t spill over to the next sched window. For example, for the example schedule described above, to ensure no spill over, guard bands may be introduced as follows:-
tc qdisc replace dev eth0 parent root handle 100 taprio \
num_tc 3 \
map 0 0 1 2 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 1@2 \
base-time 0000 \
sched-entry S 4 110520 \
sched-entry S 0 14480 \
sched-entry S 2 110520 \
sched-entry S 0 14480 \
sched-entry S 1 235520 \
sched-entry S 0 14480 \
flags 2
The above schedule still have a cycle-time of 500 msec, however there are guard bands inserted between Gate Close/Open and uses 0 Gate mask during the period of 12144 usec.
cycle-time
In the example schedule described earlier, there are 3 schedule windows described by sched-entry, first 2 being each of 125 usec and a third of 250 usec. So the schedule has a cycle-time of 500 msec which is the sum of the intervals of individual schedule. tc command also allow user to specify cycle-time as part of the command which can be used to truncate or stretch an entry. For example in the typical schedule, if user specify cycle-time of 600000
tc qdisc replace dev eth0 parent root handle 100 taprio \
num_tc 3 \
map 0 0 1 2 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 1@2 \
base-time 0000 \
sched-entry S 4 110520 \
sched-entry S 0 14480 \
sched-entry S 2 110520 \
sched-entry S 0 14480 \
sched-entry S 1 235520 \
sched-entry S 0 14480 \
cycle-time 600000 \
flags 2
In the above example, the last window gets stretched for a total of 350 usec instead of 250 usec resulting in a cycle-time of 600 usec. Similarly if the cycle-time is less than the sum of individual sched-entry, then schedule would get truncated.
tc qdisc replace dev eth0 parent root handle 100 taprio \
num_tc 3 \
map 0 0 1 2 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 1@2 \
base-time 0000 \
sched-entry S 4 110520 \
sched-entry S 0 14480 \
sched-entry S 2 110520 \
sched-entry S 0 14480 \
sched-entry S 1 235520 \
sched-entry S 0 14480 \
cycle-time 400000 \
flags 2
In the above case, last sched-entry will become truncated to 150 usec resulting in a cycle-time of 400 usec. Also it takes about 16 wireside clock cycles (128 nsec) to fetch the sched-entry from the fetch ram. So that determines the minimum value of sched-entry interval. If it is less than this, packet spills over to the next window.
Admin command
- 802.1Q standard describes admin as a way for operator to switch to a new schedule while there is an existing (oper) schedule running. In Linux this is done by sending another tc command while one is running. A limited admin command support is provided by driver with following constraints:-
- cycle-time of the new schedule must match that of the existing schedule
- start-time must be in the past
Not supported features
- Admin command with cycle-time different from oper schedule
- Admin command at a future time
- AdminCycleTimeExtension/OperCycleTimeExtension
- Configuring of queueMaxSDUTable
- Configuring of ConfigChange
- Show ConfigPending status (tc command shows Oper and Admin schedule. So if admin schedule shows up, user application may consider this as ConfigPending)
- Show ConfigChangeError
- Show SupportedListMax - Maximum supported is 64 sched-entries if interval is < 128 usec)
3.2.2.5.4.3. Intersperse Express Traffic (IET) Frame Preemption offload¶
Caution
The IET configuration interface could be changed significantly in the future depending on Linux Kernel mainline development.
CPSW2g h/w support Intersperse Express Traffic (IET, defined in P802.3br/D2.0 spec which later is included in IEEE 802.3 2018) Frame preemption (FPE) feature and also to allow MAC layer to Verify if the peer supports IET MAC merge layer or not. MAC merge layer is responsible for preempting the transmission of frame from a preemptible queue if there is frame waiting for transmission at a higher priority Express queue. The h/w sends an initial segment of the frame satisfying min fragment size requirement and then schedule frame from the Express queue for transmission. Finally when no more frames available at the Express queue, it will resume transmission of remaining segments of the frame of the preemptible queue which was preempted. At the peer end, the segments are re-assembled and delivered to the MAC interface.
IET FPE feature is configured for a port through ethtool –set-priv-flags command. Note that this is a temporary interface to allow configure IET FPE in CPSW2g driver and is not approved by netdev subsystem maintainers in Linux Kernel Mailing List (LKML) and may change in the future. Driver configures IET FPE for a port when network device is opened (ndo_open()) if user has turned ON the iet-frame-preemption priv flag. Note that since IET is a common feature applicable to all slave ports, this has to be done before the network ports of the CPSW2g are brought up. The user may also turn ON the iec-mac-verify flag if the peer device connected to CPSW2g port is also capable of verifying MAC merge/FPE capability. For this, driver schedules a worker thread to do the MAC/Verify process as soon as the Link is up and iec-mac-verify priv flag is set. It resets the LINKFAIL bit and check if the Verify succeeds or not. On failure, the MAC Verify state machine is reset by toggling LINKFAIL bit and process repeats for 20 times before bailing out. If iec-mac-verify priv flag is not set, driver assumes that peer is capable of supporting FPE, but not able to do MAC Verify. So it configures the device into force mode. User needs to verify that peer device is capable of supporting IET FPE to use force mode.
Driver assumes highest priority h/w Queue as the express Queue and configures lower queues (Q0-QN-2, where N is the maximum number of queues configured) as preemptible queues by programming the PN_REG_IET_CTRL register if the MAC Verify succeeds or if the force mode is enabled. p0-rx-ptype-rrobin flag should be turned off before using IET feature. i.e CPSW2g h/w should be programmed into strict priority mode for IET to work.
To enable IET FPE with MAC Verify, do
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
ethtool --set-priv-flags eth0 iet-mac-verify on
To enable IET FPE with no MAC Verify (Force mode)
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
ethtool --set-priv-flags eth0 iet-frame-preemption on
To disable IET FPE and restore rrobin mode
ethtool --set-priv-flags eth0 iet-frame-preemption off
ethtool --set-priv-flags eth0 iet-mac-verify off
ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin on
Example session to enable IET FPE with MAC Verify.
Assume 2 AM65x IDKs are connected back to back over MCU Ethernet port (typically eth0 interface. Example assumes 2 h/w queues configured. Q1 will be express queue and Q0 the preemption queue in this configuration.
root@am65xx-evm:~# ip link set dev eth0 down
[ 169.798571] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
root@am65xx-evm:~# ethtool -L eth0 tx 2
root@am65xx-evm:~# ethtool -l eth0
Channel parameters for eth0:
Pre-set maximums:
RX: 1
TX: 8
Other: 0
Combined: 0
Current hardware settings:
RX: 1
TX: 2
Other: 0
Combined: 0
@am65xx-evm:~# ethtool --set-priv-flags eth0 p0-rx-ptype-rrobin off
root@am65xx-evm:~# ethtool --set-priv-flags eth0 iet-frame-preemption on
root@am65xx-evm:~# ethtool --show-priv-flags eth0
Private flags for eth0:
p0-rx-ptype-rrobin : off
iet-frame-preemption: on
iet-mac-verify : off
root@am65xx-evm:~# ethtool --set-priv-flags eth0 iet-mac-verify on
root@am65xx-evm:~# ethtool --show-priv-flags eth0
Private flags for eth0:
p0-rx-ptype-rrobin : off
iet-frame-preemption: on
iet-mac-verify : on
root@am65xx-evm:~# ip link set dev eth0 up
root@am65xx-evm:~#
root@am65xx-evm:~# [ 267.393967] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 267.400353] am65-cpsw-nuss 46000000.ethernet eth0: Starting IET/FPE MAC Verify
[ 267.465086] am65-cpsw-nuss 46000000.ethernet eth0: IET/FPE MAC Verify Success
[ 267.472276] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
Example session to enable IET FPE with no MAC Verify (Force mode)
root@am65xx-evm:~# ip link set dev eth0 down
[ 394.590576] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
root@am65xx-evm:~# ethtool --set-priv-flags eth0 iet-frame-preemption on
#if iet-mac-verify was enabled before, turn it off
root@am65xx-evm:~# ethtool --set-priv-flags eth0 iet-mac-verify off
root@am65xx-evm:~# ethtool --show-priv-flags eth0
Private flags for eth0:
p0-rx-ptype-rrobin : off
iet-frame-preemption: on
iet-mac-verify : off
root@am65xx-evm:~#
root@am65xx-evm:~# ip link set dev eth0 up
root@am65xx-evm:~# ip addr add 192.168.100.20/24 dev eth0
[ 500.502660] TI DP83867 46000f00.mdio:00: attached PHY driver [TI DP83867] (mii_bus:phy_addr=46000f00.mdio:00, irq=POLL)
root@am65xx-evm:~# [ 500.516232] am65-cpsw-nuss 46000000.ethernet eth0: Link is Down
root@am65xx-evm:~# [ 552.738077] am65-cpsw-nuss 46000000.ethernet eth0: IET Enable Force mode
[ 552.744839] am65-cpsw-nuss 46000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 552.753434] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
IET FPE example
Highest priority Queue is Express queue. I.e if there are 8 queues configured through ethtool -L command, Q7 will be express and Q0-Q6 will be preemptible. Similarly if 4 queues are configured then Q3 will be express queue and Q0-Q2 will be preemptible queues. See below an example on how to verify preemption is happening in the hardware. Setup requires 2 IDKs (Example AM65x) connected over MCU Ethernet/CPSW2g port. Assume that IET is enabled on both IDKs as in previous sections and either Force mode or MAC Verify mode is enabled. As soon as the Link comes up, the IET FPE gets enabled. The test requires MQPRIO qdisc to be configured at the Talker DUT’s eth0 port and enable classifier to map UDP frames with specific port to be to a given traffic class. Traffic class is used as the index to direct traffic to the specific h/w queue. CPSW2g stats module provide a statistics counter for following that can be used to verify the IET FPE is functional:-
- iet_rx_assembly_ok - Increments at the receiver if re-assembly of MAC fragments are successful.
- iet_rx_frag - Incremenets at the receiver if MAC fragments are received due to preemption
- iet_tx_frag - Increments at the sender side if fragments are created due to frame preemption.
So to test, need to have traffic at the preemption queue as well as at the express queue and use the above statistics counters to verify if fragmentation happens at the sender side and re-assembly at the receiver side. Below logs provide some example usage.
# At the Talker side
# Set up mqprio qdisc at eth0 - 2 Queues configured. Q0 - preemption queue and Q1 express queue
root@am65xx-evm:~# tc qdisc replace dev eth0 handle 100: parent root mqprio num_tc 2 map 0 0 0 1 0 0 0 0 0 0 0 0 0 0 0 0 queues 1@0
1@1 hw 0
root@am65xx-evm:~# tc -g class show dev eth0
+---(100:ffe1) mqprio
| +---(100:2) mqprio
|
+---(100:ffe0) mqprio
+---(100:1) mqprio
# Enable classifier at net core
root@am65xx-evm:~# tc qdisc add dev eth0 clsact
# Add tc filter rule to mark packet priority based on destination UDP port number - Port 5002 mapped to prio 2
# From above mqprio settings, TC at index 2 is 0. So this TC packets go to Q0
root@am65xx-evm:~# tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 2
[ 285.576105] u32 classifier
[ 285.578910] input device check on
[ 285.582640] Actions configured
# Add tc filter rule to map packets with UDP port number - Port 5003 to prio 3
# From above mqprio settings, TC at index 3 is 1. So this TC packets go to Q1
root@am65xx-evm:~# tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5003 0xffff action skbedit priority 3
root@am65xx-evm:~#
root@am65xx-evm:~# ip addr add 192.168.100.20/24 dev eth0
# At the Listener DUT, setup ip address and run iperf3 server session listening to port 5002 and 5003.
# ip addr add 192.168.100.30/24 dev eth0
root@am65xx-evm:~# iperf3 -s -i30 -p5002&
[1] 1224
root@am65xx-evm:~# iperf3 -s -i30 -p5003&
-----------------------------------------------------------
Server listening on 5002
-----------------------------------------------------------
[2] 1225
-----------------------------------------------------------
Server listening on 5003
-----------------------------------------------------------
root@am65xx-evm:~#
# At Listener DUT start iperf3 client session to port 5002 and 5003
root@am65xx-evm:~# iperf3 -c 192.168.100.30 -u -b200M -l1472 -u -t30 -i30 -p5002&
[1] 1050
root@am65xx-evm:~# iperf3 -c 192.168.100.30 -u -b50M -l1472 -u -t30 -i30 -p5003&
[2] 1051
root@am65xx-evm:~#
root@am65xx-evm:~# warning: UDP block size 1472 exceeds TCP MSS 1448, may result in fragmentation / drops
warning: UDP block size 1472 exceeds TCP MSS 1448, may result in fragmentation / drops
Connecting to host 192.168.100.30, port 5003
Connecting to host 192.168.100.30, port 5002
[ 5] local 192.168.100.20 port 60646 connected to 192.168.100.30 port 5003
[ 5] local 192.168.100.20 port 39515 connected to 192.168.100.30 port 5002
# Now at the Talker DUT, dump statistics counter for Q0 and Q1 as well as IET statistics
root@am65xx-evm:~# ethtool -S eth0 | grep 'tx_pri1'
p0_tx_pri1: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri1_drop: 0
p0_tx_pri1_drop_bcnt: 0
tx_pri1: 24869
tx_pri1_bcnt: 37722660
tx_pri1_drop: 0
tx_pri1_drop_bcnt: 0
root@am65xx-evm:~# ethtool -S eth0 | grep 'tx_pri0'
p0_tx_pri0: 0
p0_tx_pri0_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 100271
tx_pri0_bcnt: 152067960
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@am65xx-evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 159
root@am65xx-evm:~# ethtool -S eth0 | grep 'tx_pri1'
p0_tx_pri1: 0
p0_tx_pri1_bcnt: 0
p0_tx_pri1_drop: 0
p0_tx_pri1_drop_bcnt: 0
tx_pri1: 27718
tx_pri1_bcnt: 42047442
tx_pri1_drop: 0
tx_pri1_drop_bcnt: 0
root@am65xx-evm:~# ethtool -S eth0 | grep 'tx_pri0'
p0_tx_pri0: 0
p0_tx_pri0_bcnt: 0
p0_tx_pri0_drop: 0
p0_tx_pri0_drop_bcnt: 0
tx_pri0: 111637
tx_pri0_bcnt: 169320030
tx_pri0_drop: 0
tx_pri0_drop_bcnt: 0
root@am65xx-evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 0
iet_rx_smd_err: 0
iet_rx_frag: 0
iet_tx_hold: 0
iet_tx_frag: 175
# As seen, iet_tx_frag statistics counter increments at the Talker showing fragmentation at the Talker
# Also dump the statistics at the listener DUT
ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 248
iet_rx_smd_err: 0
iet_rx_frag: 248
iet_tx_hold: 0
iet_tx_frag: 0
root@am65xx-evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 252
iet_rx_smd_err: 0
iet_rx_frag: 252
iet_tx_hold: 0
iet_tx_frag: 0
root@am65xx-evm:~# ethtool -S eth0 | grep iet
iet_rx_assembly_err: 0
iet_rx_assembly_ok: 252
iet_rx_smd_err: 0
iet_rx_frag: 252
iet_tx_hold: 0
iet_tx_frag: 0
# As seen, iet_rx_frag and iet_rx_assembly_ok statistics counter increments at the Listener showing re-assembly at the Listener
Using IET together with EST
Express and preemption queues/Gates may be used as part of the EST schedule. If only Preemption queues are in a schedule entry, preceding an entry with Express queue, the guard band requirement reduces to 2048 nsec (0x100 = 256 * 8) so that packets don’t spill over to the next sched-entry. Otherwise, the guard band required is as explained in the EST section.
3.2.2.5.4.4. Forwarding and Queuing Enhancements for Time-Sensitive Streams (FQTSS, 802.1Qav)¶
The K3 CPSW HW supports 2 level of traffic 802.1Qav shapers which are bound to TX CPPI channels on Host P0 (CPPI Receive thread) and External Ports FIFOs which represent HW traffic classes. The HW shapers allows to configure Committed Information Rate (guaranteed) and Excess Information Rate (non guaranteed) per TX CPPI channels or External Ports Fifos.
The CPSWxG driver allows to perform Traffic Rate Limiting/shaping at:
- Host port ingress, CPPI Port Receive Rate Limiting, by configuring per TX CPPI channels shaper. Only committed information rate is supported.
- Switch egress, Ethernet Port Transmit Rate Limiting, by configuring per TX FIFO shaper. Both committed and excess information rate is supported.
The number Host port TX CPPI channels is configurable (up to 8) through ethtool commands:- -L. The Host port TX CPPI channels processing mode has to be switched in Fixed priority mode through ethtool commands: –set-priv-flags. Also note that –set-priv-flags and -L ethtool commands can be execute only when all Ethernet interfaces are down.
The Linux TC MQPRIO Qdisc can be used for mapping of packet priorities to traffic classes and routing packets to dedicated TX CPPI channels or External Ports FIFOs.
3.2.2.5.4.4.1. Host port ingress, CPPI Port Receive Rate Limiting offload¶
The netdev sysfs tx_maxrate parameter can be used to configure rate limit in Mbit/s per TX CPPI channel. The rate for shapers has to be set a little bit more then potential incoming rate, and real rates can differ, due to discreetness.
echo 100 > /sys/class/net/eth2/queues/tx-7/tx_maxrate
Host port ingress, CPPI Port Receive Rate Limiting offload example
In this example Rate Limiting is enabled only for Host port TX channels.
- tc filters are used to assign pri for iperf3 traffic using port as filter value
- pri7 traffic routed to TX CPPI channel 7, rate limit 100Mbit
- pri6 traffic routed to TX CPPI channel 6, rate limit 200Mbit
- pri0-5 traffic routed to TX CPPI channel 0
ip link set dev eth0 down
ethtool -L eth0 tx 8
ip link set dev eth0 up
tc qdisc replace dev eth0 handle 100: parent root mqprio num_tc 3 \
map 0 0 0 0 0 0 1 2 0 0 0 0 0 0 0 0 queues 1@0 1@6 1@7 hw 0
echo 106 > /sys/class/net/eth0/queues/tx-7/tx_maxrate
echo 212 > /sys/class/net/eth0/queues/tx-6/tx_maxrate
tc qdisc add dev eth0 clsact
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5001 0xffff action skbedit priority 7
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 6
iperf3 -c 192.168.1.2 -t10 -p5001 -Tpri7 & \
iperf3 -c 192.168.1.2 -t10 -p5002 -Tpri6 & \
iperf3 -c 192.168.1.2 -t10 -p5003 -Tpri0
#result
pri0: - - - - - - - - - - - - - - - - - - - - - - - - -
pri0: [ ID] Interval Transfer Bitrate Retr
pri0: [ 5] 0.00-10.00 sec 767 MBytes 644 Mbits/sec 0 sender
pri0: [ 5] 0.00-10.00 sec 766 MBytes 642 Mbits/sec receiver
pri6: - - - - - - - - - - - - - - - - - - - - - - - - -
pri6: [ ID] Interval Transfer Bitrate Retr
pri6: [ 5] 0.00-10.00 sec 238 MBytes 200 Mbits/sec 0 sender
pri6: [ 5] 0.00-10.01 sec 238 MBytes 199 Mbits/sec receiver
pri7: - - - - - - - - - - - - - - - - - - - - - - - - -
pri7: [ ID] Interval Transfer Bitrate Retr
pri7: [ 5] 0.00-10.00 sec 120 MBytes 101 Mbits/sec 0 sender
pri7: [ 5] 0.00-10.01 sec 119 MBytes 99.9 Mbits/sec receiver
#statistic
tx_pri0: 2819633
tx_pri1: 2
tx_pri2: 0
tx_pri3: 102
tx_pri4: 26
tx_pri5: 0
tx_pri6: 847449
tx_pri7: 1237148
3.2.2.5.4.4.2. Switch egress, Ethernet Port Transmit Rate Limiting offload¶
The Linux MQPRIO Qdisc in channel offload mode can be used for mapping of packet priorities to traffic classes and configuring rate limit in Mbit/s per External Ports FIFOs. The MQPRIO Qdisc shaper bw_rlimit min_rate and max_rate parameters can be used to configure External Ports FIFO shapers.
- the traffic class (TC) in terms of MQPRIO Qdisc is mapped 1:1 to External Ports FIFO. TC0 is lowest priority.
- MQPRIO Qdisk offload is expected to work with VALN/priority tagged traffic first of all and untagged traffic has to be mapped only to TC0.
- to handle properly untagged traffic from Host Port the 1:1 mapping has to be preserved between packet priority and Host TX CPPI channel used to send packet
- VALN/priority tagged packets mapped to TC0 will exit switch with VALN tag.
- if Host sends traffic to the same, rate limited External Ports FIFO then corresponding Host TX CPPI channel shapers has to be enabled and its rate has to be set equal or less than External Ports FIFO rate
- the rate for shapers has to be set a little bit more then potential incoming rate, and real rates can differ, due to discreetness.
tc qdisc add dev eth0 parent root handle 100: mqprio num_tc 3 \
map 0 0 0 0 0 0 1 2 0 0 0 0 0 0 0 0 \
queues 1@0 1@6 1@7 hw 1 mode channel \
shaper bw_rlimit min_rate 0 212mbit 106mbit max_rate 0 250mbit 150mbit
Switch egress, Ethernet Port Transmit Rate Limiting example
In this example Rate Limiting is enabled for Host port TX channels and External Ports FIFO.
- tc filters are used to assign pri for iperf3 traffic using port as filter value
- untagged traffic
- pri7 traffic routed to TX CPPI channel 7, rate limit 100Mbit
- pri6 traffic routed to TX CPPI channel 6, rate limit 200Mbit
- pri0-5 traffic routed to TX CPPI channel 0
- pri7 traffic mapped to TC2, External Ports FIFO2, cir=100Mbit, eir=150Mbit
- pri6 traffic mapped to TC1, External Ports FIFO1, cir=200Mbit, eir=250Mbit
- pri0-5 traffic mapped to TC1, External Ports FIFO0
ip link set dev eth0 down
ethtool -L eth0 tx 8
ip link set dev eth0 up
tc qdisc add dev eth0 parent root handle 100: mqprio num_tc 3 \
map 0 0 0 0 0 0 1 2 0 0 0 0 0 0 0 0 \
queues 1@0 1@6 1@7 hw 1 mode channel \
shaper bw_rlimit min_rate 0 212mbit 106mbit max_rate 0 250mbit 150mbit
echo 106 > /sys/class/net/eth0/queues/tx-7/tx_maxrate
echo 212 > /sys/class/net/eth0/queues/tx-6/tx_maxrate
tc qdisc add dev eth0 clsact
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5001 0xffff action skbedit priority 7
tc filter add dev eth0 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 6
iperf3 -c 192.168.1.2 -t10 -p5001 -Tpri7 & \
iperf3 -c 192.168.1.2 -t10 -p5002 -Tpri6 & \
iperf3 -c 192.168.1.2 -t10 -p5003 -Tpri0
#result
pri7: - - - - - - - - - - - - - - - - - - - - - - - - -
pri7: [ ID] Interval Transfer Bitrate Retr
pri7: [ 5] 0.00-10.00 sec 120 MBytes 100 Mbits/sec 0 sender
pri7: [ 5] 0.00-10.00 sec 119 MBytes 99.9 Mbits/sec receiver
pri6: - - - - - - - - - - - - - - - - - - - - - - - - -
pri6: [ ID] Interval Transfer Bitrate Retr
pri6: [ 5] 0.00-10.00 sec 238 MBytes 200 Mbits/sec 0 sender
pri6: [ 5] 0.00-10.00 sec 238 MBytes 199 Mbits/sec receiver
pri0: - - - - - - - - - - - - - - - - - - - - - - - - -
pri0: [ ID] Interval Transfer Bitrate Retr
pri0: [ 5] 0.00-10.00 sec 767 MBytes 643 Mbits/sec 0 sender
pri0: [ 5] 0.00-10.00 sec 766 MBytes 642 Mbits/sec receiver
#statistic
tx_pri0: 2012441
tx_pri1: 172147
tx_pri2: 259038
tx_pri3: 0
tx_pri4: 2
tx_pri5: 9
tx_pri6: 0
tx_pri7: 0
3.2.2.5.5. Multi port Switch mode¶
Note
This section documents the Switch mode features available with CPSW3g
The Switch mode can be enabled by configuring devlink driver parameter “switch_mode” to 1/true:
devlink dev param set platform/8000000.ethernet \
name switch_mode value true cmode runtime
Above setting can be done regardless of the state of Port’s netdev devices - UP/DOWN, but Port’s netdev devices have to be in UP state before joining the bridge. This is to avoid overwriting of bridge configuration as CPSW switch driver completely reloads its configuration when first port changes its state to UP.
When all the interfaces have joined the bridge - CPSW switch driver will enable marking packets with offload_fwd_mark flag.
All configuration is implemented via switchdev API.
3.2.2.5.5.1. Bridge setup¶
devlink dev param set platform/8000000.ethernet \
name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth0 up
ip link set dev eth1 up
ip link set dev eth0 master br0
ip link set dev eth1 master br0
[*] bridge vlan add dev br0 vid 1 pvid untagged self
[*] if vlan_filtering=1, where default_pvid=1
Note: Steps [*] are mandatory.
3.2.2.5.5.2. Turn On/Off Spanning Tree Protocol (STP)¶
ip link set dev br0 type bridge stp_state 1/0
3.2.2.5.5.3. VLAN configuration¶
bridge vlan add dev br0 vid 1 pvid untagged self <---- add cpu port to VLAN 1
This step is mandatory for bridge/default_pvid.
3.2.2.5.5.4. Adding extra VLANs¶
untagged:
bridge vlan add dev eth0 vid 100 pvid untagged master bridge vlan add dev sw0p2 vid 100 pvid untagged master bridge vlan add dev br0 vid 100 pvid untagged self <---- Add cpu port to VLAN100tagged:
bridge vlan add dev eth0 vid 100 master bridge vlan add dev sw0p2 vid 100 master bridge vlan add dev br0 vid 100 pvid tagged self <---- Add cpu port to VLAN100
3.2.2.5.5.5. Forwarding Data Bases (FDBs)¶
Forwarding entries for MAC addresses are automatically added on the appropriate switch port upon detection as default operation as an unmanaged bridge. For managed bridge operation manually add FDB entries as required.
Manually adding FDBs:
bridge fdb add aa:bb:cc:dd:ee:ff dev eth0 master vlan 100
bridge fdb add aa:bb:cc:dd:ee:fe dev sw0p2 master <---- Add on all VLANs
3.2.2.5.5.6. Multicast Data Bases (MDBs)¶
Multicast entries are automatically added on the appropriate switch port upon detection as default operation as an unmanaged bridge. For managed bridge operation manually add MDB entries as required.
Manually adding MDBs:
bridge mdb add dev br0 port eth0 grp 239.1.1.1 permanent vid 100
bridge mdb add dev br0 port eth0 grp 239.1.1.1 permanent <---- Add on all VLANs
3.2.2.5.5.7. Multicast flooding¶
CPU port mcast_flooding is always on
Turning flooding on/off on switch ports:
bridge link set dev eth0 mcast_flood on/off
3.2.2.5.5.8. Enabling Cut Through forwarding¶
Caution
The Cut Through configuration interface could be changed significantly in the future depending on Linux Kernel mainline development.
Cut Through feature allows forwarding packet from one external port to another without being stored in Port FIFOs thus reducing overall latency for packet forwarding.
Limitations:
- Feature is only available in switch mode.
- Cut Through forwarding is only supported between external ports and no support for Cut Through to host port currently.
- Cut-Thru is not supported with 10/100 half-duplex.
- Cut-Thru is not supported with any form of flow control.
- If Intersperced Express Traffic (IET) is enabled, then Cut Through can only be enabled on an express priority queue and not on preemptible queues.
Note
Currently per port priority mask is set via debugfs entries. This may change in future.
Here is the commands to setup cut-through for priority 0 traffic
ip link set dev eth0 down
ip link set dev eth1 down
devlink dev param set platform/8000000.ethernet name switch_mode value
echo 1 > /sys/kernel/debug/8000000.ethernet/Port1/cut_thru_rx_pri_mask
echo 1 > /sys/kernel/debug/8000000.ethernet/Port1/cut_thru_tx_pri_mask
echo 1 > /sys/kernel/debug/8000000.ethernet/Port2/cut_thru_rx_pri_mask
echo 1 > /sys/kernel/debug/8000000.ethernet/Port2/cut_thru_tx_pri_mask
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth0 up
sleep 1
ip link set dev eth1 up
sleep 1
ip link set dev eth0 master br0
ip link set dev eth1 master br0
ip link set dev br0 type bridge stp_state 1
ip link set dev br0 up
ip addr add 10.0.0.1/8 dev br0
bridge vlan add dev br0 vid 1 pvid untagged self
The value being written to cut_thru_rx_pri_mask and cut_thru_tx_pri_mask represents the priorties queues for which cut through feature needs to be enabled. Can be configured only when all external ports are down.
With above settings, generate a iperf3 traffic from client on Port1 to client on Port 2 and observe the ethtool statistics to see cut through taking effect
root@evm:~# ethtool -S eth1 | grep col
tx_collision_frames: 1796093
tx_single_coll_frames: 0
tx_mult_coll_frames: 3
tx_excessive_collisions: 0
tx_late_collisions: 0
root@evm:~# ethtool -S eth0 | grep col
tx_collision_frames: 3
tx_single_coll_frames: 0
tx_mult_coll_frames: 2002396
tx_excessive_collisions: 52
tx_late_collisions: 23
tx_collision_frames: Enet_Pn_TxCut Enet Port n Cut Thru with and without delay (full-duplex)
tx_single_coll_frames: Enet_pn_TxCut_SAF Enet Port n Tx Store and Forward (full-duplex)
tx_mult_coll_frames: Enet_Pn_RxCut_NoDelay Enet Port n Rx Cut Thru with no delay (full-duplex)
tx_excessive_collisions: Enet_Pn_RxCut_Delay Enet Port n Rx Cut Thru with delay (full-duplex)
tx_late_collisions: Enet_Pn_RxCut_SAF Enet Port n Rx Store and Forward (full-duplex)
3.2.2.5.5.9. Transmit Traffic Control and Rate Limiting¶
For general info see Forwarding and Queuing Enhancements for Time-Sensitive Streams (FQTSS, 802.1Qav) The main difference between one port and multi port devices is that TX CPPI channels are shared between all network devices while External Ports FIFO are per port. The MQPRIO Qdisk can be used to assign different TX CPPI channels to different ports and this way improve over all TX performance.
- the configured External Ports Fifos rate should must not be oversubscribed. If some Ext. port and Host port both send to the same priority then Ext. Ports Fifos rate for this priority has to be set as sum of Ext. and Host port rates plus some margin.
Example Host port ingress with separate TX CPPI channel per port, no QoS
- switch mode: on | off
- Port 1 assigned TX CPPI channel 0
- Port 2 assigned TX CPPI channel 1
- TX CPPI channels processing mode: Round Robin
ip link set dev eth0 down
ip link set dev eth1 down
ethtool -L eth0 tx 2
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin on
ip link set dev eth0 up
ip link set dev eth1 up
tc qdisc add dev eth0 handle 100: parent root mqprio num_tc 1 map 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 queues 1@0 hw 1 mode channel
tc qdisc add dev eth1 handle 100: parent root mqprio num_tc 1 map 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 queues 1@1 hw 1 mode channel
If TX CPPI channels processing mode is Round Robin (p0-rx-ptype-rrobin off) then Rate Limiting should for selected TX CPPI channels.
echo 800 > /sys/class/net/eth0/queues/tx-0/tx_maxrate
echo 800 > /sys/class/net/eth0/queues/tx-1/tx_maxrate
Example Host port ingress with separate TX CPPI channel per port and Rate Limiting
Linux Host send bulk and rate limited traffic to both ports. No traffic switching between P1 and P2.
to Host1│ CPSW3g Host bridge │ to Host2
│ / \ │
│ P1 P2 │
│ | | │
│ Host1 Host2 │
▼ ▼
- switch mode: on
- tc filters are used to assign pri for iperf3 traffic using port as filter value
- VLAN tagged traffic vid=100
eth0: Ports 1
- pri7 traffic routed to TX CPPI channel 7, rate limit 100Mbit
- pri6 traffic routed to TX CPPI channel 6, rate limit 200Mbit
- pri0-5 traffic routed to TX CPPI channel 0
- pri7 traffic mapped to TC2, External Ports FIFO2, cir=100Mbit
- pri6 traffic mapped to TC1, External Ports FIFO1, cir=200Mbit
- pri0-5 traffic mapped to TC0, External Ports FIFO0
eth1: Ports 2
- pri7 traffic routed to TX CPPI channel 5, rate limit 100Mbit
- pri6 traffic routed to TX CPPI channel 4, rate limit 200Mbit
- pri0-5 traffic routed to TX CPPI channel 0
- pri7 traffic mapped to TC2, External Ports FIFO2, cir=100Mbit
- pri6 traffic mapped to TC1, External Ports FIFO1, cir=200Mbit
- pri0-5 traffic mapped to TC1, External Ports FIFO0
ip link set dev eth0 down
ip link set dev eth1 down
ethtool -L eth0 tx 8
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ip link add name br0 type bridge
ip link set dev eth0 up
ip link set dev eth1 up
ip link set dev eth0 master br0
ip link set dev eth1 master br0
ip link set dev br0 up
#configure bridge...
#configure bridge vlan
ip link add link br0 name br0.100 type vlan id 100
ip link set br0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
bridge vlan add dev eth0 vid 100 master
bridge vlan add dev eth1 vid 100 master
bridge vlan add dev br0 vid 100 self
# set IP to br0.100 192.168.100.1
echo 100 > /sys/class/net/eth0/queues/tx-7/tx_maxrate
echo 200 > /sys/class/net/eth0/queues/tx-6/tx_maxrate
echo 100 > /sys/class/net/eth0/queues/tx-5/tx_maxrate
echo 200 > /sys/class/net/eth0/queues/tx-4/tx_maxrate
tc qdisc add dev br0.100 clsact
tc filter add dev br0.100 egress protocol ip prio 1 u32 match ip dport 5001 0xffff action skbedit priority 7
tc filter add dev br0.100 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 6
#eth0
tc qdisc add dev eth0 parent root handle 100: mqprio num_tc 3 \
map 0 0 0 0 0 0 1 2 0 0 0 0 0 0 0 0 \
queues 1@0 1@6 1@7 hw 1 mode channel \
shaper bw_rlimit min_rate 0 200mbit 100mbit
#eth1
tc qdisc add dev eth1 parent root handle 100: mqprio num_tc 3 \
map 0 0 0 0 0 0 1 2 0 0 0 0 0 0 0 0 \
queues 1@0 1@4 1@5 hw 1 mode channel \
shaper bw_rlimit min_rate 0 200mbit 100mbit
iperf3 -c 192.168.100.3 -t10 -p5001 -Tpri71 & \
iperf3 -c 192.168.100.3 -t10 -p5002 -Tpri61 & \
iperf3 -c 192.168.100.3 -t10 -p5003 -Tpri01 & \
iperf3 -c 192.168.100.2 -t10 -p5001 -Tpri72 & \
iperf3 -c 192.168.100.2 -t10 -p5002 -Tpri62
Example Bridging with TX CPPI channel and External Ports FIFO shapers
Linux Host send bulk and rate limited traffic to Host 2 (Port 2) pri3 200Mbit and Host 1 sends rate limited traffic to Host 2 (Port 2) pri3 200Mbit.
CPSW3g Host bridge │ to Host2
/ \ │ 200Mbit
P1 P2 │
| | │
Host1 Host2 │
▼
──────────────►
to Host2
200Mbit
- switch mode: on
- tc filters are used to assign pri for iperf3 traffic using port as filter value
- VLAN tagged traffic vid=100
- assume pri3 is class A and pri 2 is class B (not used)
eth0: Ports 1
- pri0-7 traffic routed to TX CPPI channel 0, no HW offload
eth1: Ports 2
- pri3 traffic routed to TX CPPI channel 7, rate limit 200Mbit
- pri2 traffic routed to TX CPPI channel 6, rate limit 100Mbit
- pri0,1,4-7 traffic routed to TX CPPI channel 0
- pri3 traffic mapped to TC2, External Ports FIFO2, cir=200Mbit
- pri2 traffic mapped to TC1, External Ports FIFO1, cir=100Mbit
- pri0,1,4-7 traffic mapped to TC0, External Ports FIFO0
CPSW3g Host bridge configuration
ip link set dev eth0 down
ip link set dev eth1 down
ethtool -L eth0 tx 8
ethtool --set-priv-flags eth1 p0-rx-ptype-rrobin off
ip link add name br0 type bridge
ip link set dev eth0 up
ip link set dev eth1 up
ip link set dev eth0 master br0
ip link set dev eth1 master br0
ip link set dev br0 up
#configure bridge...
#configure bridge vlan
ip link add link br0 name br0.100 type vlan id 100
ip link set br0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
bridge vlan add dev eth0 vid 100 master
bridge vlan add dev eth1 vid 100 master
bridge vlan add dev br0 vid 100 self
# set IP to br0.100 192.168.100.1
echo 200 > /sys/class/net/eth0/queues/tx-7/tx_maxrate
echo 100 > /sys/class/net/eth0/queues/tx-6/tx_maxrate
tc qdisc add dev br0.100 clsact
tc filter add dev br0.100 egress protocol ip prio 1 u32 match ip dport 5002 0xffff action skbedit priority 3
#eth0
tc qdisc add dev eth0 handle 100: parent root mqprio num_tc 1 \
map 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 0 queues 1@0 hw 0
#eth1
tc qdisc add dev eth1 parent root handle 100: mqprio num_tc 3 \
map 0 0 1 2 0 0 0 0 0 0 0 0 0 0 0 0 \
queues 1@0 1@6 1@7 hw 1 mode channel \
shaper bw_rlimit min_rate 0 100mbit 410mbit
iperf3 -c 192.168.100.2 -t10 -p5002 -Tpri22 -t30 & \
iperf3 -c 192.168.100.2 -t10 -p5003 -Tpri02 -t30 &
Host 1 configuration
ip link add link eth0 name eth0.100 type vlan id 100
ip link set eth0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
# set IP to br0.100 192.168.100.3
tc qdisc add dev eth0.100 clsact
tc filter add dev eth0.100 egress protocol ip prio 1 u32 match ip dport 5001 0xffff action skbedit priority 3
#Real QoS configuration depends Host 2 functionality
iperf3 -c 192.168.100.2 -t10 -p5001 -Tpri3 -t30
# - or -
iperf3 -c 192.168.100.2 -t10 -p5001 -Tpri3 -t30 -u -b210M
Host 2 configuration
ip link add link eth0 name eth0.100 type vlan id 100
ip link set eth0.100 type vlan egress 0:0 1:1 2:2 3:3 4:4 5:5 6:6 7:7
# set IP to br0.100 192.168.100.3
iperf3 -s -p 5001&
iperf3 -s -p 5002&
iperf3 -s -p 5003&