5.3.8. PRU-ADC Demo¶
5.3.8.1. Introduction¶
This demo shows flexible interface for Simultaneous, Coherent DAQ Using Multiple ADCs via PRU-ICSS. More details can be found at http://www.ti.com/tool/TIDA-01555
5.3.8.2. Hardware Needed¶
Please refer to the TI Design to set up the hardware needed to run this demo.
- Beaglebone Black
- TIDA-01555 adapter card
- TIDA-01555 ADC board
- Desktop power supply to provide 5.5 volts to the ADC board
- Desktop signal generator to produce a 45-55Hz sine wave as an input
5.3.8.3. Steps to Run the Demo¶
Below are the steps to run the demo with Processor SDK Linux RT build for AM335x.
First, use /boot/am335x-boneblack-pru-adc.dtb as the default dtb:
cd /boot
cp am335x-boneblack.dtb am335x-boneblack.dtb.orig
cp am335x-boneblack-pru-adc.dtb am335x-boneblack.dtb
Then, link am335x-pru*_fw to the PRU-ADC firmware binaries:
cd /lib/firmware
ln -sf /lib/firmware/pru/PRU_ADS8688_Controller.out am335x-pru0-fw
ln -sf /lib/firmware/pru/PRU_ADS8688_Interface.out am335x-pru1-fw
After that, reboot the EVM, and then execute the ARM binary:
run-pru-adc.sh