2.4. CoreSDK Linux Migration Guide

Overview

This page covers migration information for applications built on top of the Processor SDK for Linux.

2.4.1. Processor CoreSDK 09.xx Releases

2.4.1.1. Processor CoreSDK Sitara 09.01

  • Tag Info: 09.01.00.008

  • This is the fifth release in the 2023 LTS stream, with new versions of Kernel, U-boot, toolchain and Yocto branch.

  • Platforms Supported : AM62Px (HS-FS, HS-SE), AM62x ( GP, HS-FS, HS-SE), AM62x LP (HS-FS, HS-SE), AM62SIP ( HS-FS, HS-SE), AM64x 2.0 (HS-FS), AM62A (HS-FS, HS-SE)

  • Kernel 6.1.46

  • U-Boot 2023.04

  • ATF 2.9+

  • OPTEE 4.0

  • Toolchain GCC 11.4

  • Yocto Kirkstone/4.0

  • Graphics DDK 23.2

  • Tag Info: 09.01.00.007

  • This is the fourth release in the 2023 LTS stream, with new versions of Kernel, U-boot, toolchain and Yocto branch.

  • Platforms Supported : AM65x(GP, HS-SE)

  • Kernel 6.1.46

  • U-Boot 2023.04

  • ATF 2.9+

  • OPTEE 4.0

  • Toolchain GCC 11.4

  • Yocto Kirkstone/4.0

  • Graphics DDK 1.17

2.4.1.2. Processor CoreSDK Sitara 09.00

  • Tag Info: 09.01.00.001

  • This is the third release in the 2023 LTS stream, with new versions of Kernel, U-boot, toolchain and Yocto branch.

  • Platforms Supported : AM335x(GP, HS), AM437x (GP, HS)

  • Kernel 6.1

  • U-Boot 2023.04

  • Toolchain GCC 11.4

  • Yocto Kirkstone/4.0

  • Graphics DDK 1.17

  • Tag Info: 09.00.00.011

  • This is the second release in the 2023 LTS stream, with new versions of Kernel, U-boot, toolchain and Yocto branch.

  • Platforms Supported : AM62SIP ( HS-FS, HS-SE)

  • Kernel 6.1

  • U-Boot 2023.04

  • Toolchain GCC 11.4

  • ATF 2.9+

  • OPTEE 3.20

  • Yocto Kirkstone/4.0

  • Graphics DDK 23.1

  • Tag Info: 09.00.00.006

  • This is the first release in the 2023 LTS stream, with new versions of Kernel, U-boot, toolchain and Yocto branch.

  • Platforms Supported : AM64x 2.0 (HS-FS), AM62x ( GP, HS-FS, HS-SE), AM62x LP (HS-FS, HS-SE), AM62A (HS-FS, HS-SE)

  • Kernel 6.1

  • U-Boot 2023.04

  • Toolchain GCC 11.2

  • ATF 2.8+

  • OPTEE 3.20

  • Yocto Kirkstone/4.0

  • Graphics DDK 23.1

Note

  • For U-Boot builds, k3-image-gen and core-secdev-k3 are no longer needed as binman is used instead. Please refer to U-Boot build instructions for the updated steps.

  • For Linux builds, generic defconfig is used instead of custom fragments. Please refer to linux users guide for build instructions.