2.2. Yocto Layer Configuration

Processor SDK uses oe-layersetup configuration files to initialize the Yocto build environment. Configure your build with the following command:

$ ./oe-layertool-setup.sh -f <config>

Replace <config> with one of the configuration files listed below.

The oe-layersetup git repository contains the following configuration files in the configs/processor-sdk directory.

Table 2.1 Yocto Layer Configuration

Config File

Description

Supported machines/platforms

processor-sdk-scarthgap-11.02.05.02-config.txt

Processor SDK 11.02.05.02 Release

am65xx-evm