5.1. Developer NotesΒΆ
- 5.1.1. Connect to an EVM via Telnet
- 5.1.2. How to Setup a Samba Server
- 5.1.3. Boot Sequence
- 5.1.4. Moving Files to the Target System
- 5.1.5. How to Flash Linux System from U-boot
- 5.1.6. SDK File System Optimization/Customization
- 5.1.7. How to add a JVM
- 5.1.8. How to use a Mouse instead of the Touchscreen with Matrix
- 5.1.9. Update U-Boot Environment Variables stored in SPI Flash from Linux
- 5.1.10. How to change dtb files
- 5.1.11. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM65xx?
- 5.1.12. How to Build a Ubuntu Linux host under VMware
- 5.1.13. K3 Resource Partitioning Tool