3.11. OP-TEEΒΆ
Overview
OP-TEE is a Trusted Execution Environment (TEE) designed as companion to a non-secure Linux kernel running on Arm; Cortex-A cores using the TrustZone technology. OP-TEE implements TEE Internal Core API v1.1.x which is the API exposed to Trusted Applications and the TEE Client API v1.0, which is the API describing how to communicate with a TEE. Those APIs are defined in the GlobalPlatform API specifications.
Getting the OP-TEE Source Code
$ git clone https://github.com/OP-TEE/optee_os.git
Getting Security Dev Tool
$ git clone git://git.ti.com/security-development-tools/core-secdev-k3.git -b master
$ export TI_SECURE_DEV_PKG=`pwd`/core-secdev-k3
Building OP-TEE
on GP
$ make CROSS_COMPILE64=aarch64-linux-gnu- PLATFORM=k3-am65x CFG_ARM64_core=y
on HS
$ make CROSS_COMPILE64=aarch64-linux-gnu- PLATFORM=k3-am65x CFG_ARM64_core=y
$ {TI_SECURE_DEV_PKG}/scripts/secure-binary-image.sh ./out/arm-plat-k3/core/tee-pager_v2.bin ./out/arm-plat-k3/core/tee-pager_v2.bin.signed