Processor SDK Linux for AM65X
07_03_00
  • 1. Overview
  • 2. Release Specific
  • 3. Foundational Components
  • 4. Industrial Protocols
  • 5. Examples and Demos
  • 6. How to Guides
    • 6.1. Developer Notes
      • 6.1.1. Connect to an EVM via Telnet
      • 6.1.2. How to Setup a Samba Server
      • 6.1.3. Boot Sequence
      • 6.1.4. Moving Files to the Target System
      • 6.1.5. How to Flash Linux System from U-boot
      • 6.1.6. SDK File System Optimization/Customization
      • 6.1.7. How to add a JVM
      • 6.1.8. How to use a Mouse instead of the Touchscreen with Matrix
      • 6.1.9. Update U-Boot Environment Variables stored in SPI Flash from Linux
      • 6.1.10. How to change dtb files
      • 6.1.11. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM65xx?
      • 6.1.12. How to Build a Ubuntu Linux host under VMware
      • 6.1.13. K3 Resource Partitioning Tool
    • 6.2. Hardware EVM Setup
  • 7. Documentation Tarball
Processor SDK Linux for AM65X
  • Docs »
  • 6. How to Guides »
  • 6.1. Developer Notes

6.1. Developer NotesΒΆ

  • 6.1.1. Connect to an EVM via Telnet
  • 6.1.2. How to Setup a Samba Server
  • 6.1.3. Boot Sequence
  • 6.1.4. Moving Files to the Target System
  • 6.1.5. How to Flash Linux System from U-boot
  • 6.1.6. SDK File System Optimization/Customization
  • 6.1.7. How to add a JVM
  • 6.1.8. How to use a Mouse instead of the Touchscreen with Matrix
  • 6.1.9. Update U-Boot Environment Variables stored in SPI Flash from Linux
  • 6.1.10. How to change dtb files
  • 6.1.11. How do I integrate a different version of open source software than what is packaged in Processor SDK Linux AM65xx?
  • 6.1.12. How to Build a Ubuntu Linux host under VMware
  • 6.1.13. K3 Resource Partitioning Tool
    • 6.1.13.1. Getting started
    • 6.1.13.2. Usage
      • 6.1.13.2.1. NAVSS resource partitioning
      • 6.1.13.2.2. Review resource allocation
      • 6.1.13.2.3. QoS configuration
      • 6.1.13.2.4. Firewall configuration
      • 6.1.13.2.5. Generating output files
    • 6.1.13.3. Troubleshooting
    • 6.1.13.4. Developer notes
      • 6.1.13.4.1. Directory structure
      • 6.1.13.4.2. Updating the device data
Next Previous

© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale