2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor-SDK) for Linux provides a fundamental software platform for development, deployment and execution of Linux based applications and includes the following:
- Bootloaders & Filesystems
- SDK Installer
- Setup Scripts
- Makefiles
- WLAN support (Wilink 8)
- Code Composer Studio
2.1.2. Licensing¶
Please refer to the software manifest, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page. The manifest can be found on the SDK download page or in the installed directory as indicated below. In addition, see Processor SDK Linux GPLv3 Disclaimer.
2.1.3. Documentation¶
- Processor SDK Linux Software Developer’s Guide: Provides information on features, functions, delivery package and, compile tools for the Processor SDK Linux release. This also provides detailed information regarding software elements and software infrastructure to allow developers to start creating applications.
- Processor SDK Linux Getting Started Guide: Provides information on getting the software and running examples/demonstrations bundled in the SDK.
- Software Manifest: Provides license information on software
included in the SDK release. This document is in the release at
[INSTALL-DIR]/docs. - EVM Quick Start Guide: Provides information on hardware setup and running the demonstration application that is loaded on flash. This document is provided as part of the EVM kit.
2.1.4. Release 07.03.00¶
Released May 2021
What’s New
SDK Components & Versions
| Component | Version |
|---|---|
| Linux Kernel | 5.4.106 |
| U-Boot | 2020.01 |
| Yocto Project | 3.1 (dunfell) |
| ARM Toolchain (gcc) | 9.2-2019.12 hard-float |
| TI C66x CGT Compiler | 8.3.2 |
2.1.5. Supported Platforms¶
See here for a list of supported platforms and links to more information.
2.1.6. Build Information¶
2.1.6.1. U-Boot¶
2.1.6.2. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
Generic Kernel Release Notes
2.1.6.3. Yocto¶
meta-ti
meta-arago
2.1.7. Issues Tracker¶
2.1.7.1. Issues opened in previous releases that were closed on this release¶
| Record ID | Summary |
|---|---|
| LCPD-19785 | Uboot: usbhost has problem with detection |
| LCPD-19784 | DFU MMC test fails |
| LCPD-19781 | OE: ti-rpmsg-char: Library header files and primary so file are missing in FS |
| LCPD-19772 | ATF/Uboot GTC frequency handover bug |
| LCPD-19740 | TLS1.2 hangs on handshake |
| LCPD-19717 | am654-gpevm: kernel image boot reports corruption |
| LCPD-19695 | am654-gpevm: kernel image boot reports corruption |
| LCPD-19264 | Uboot: No usb controllers found |
| LCPD-19249 | Kernel WARN observed in some cases, tisci timeout reported |
| LCPD-19180 | AM65 PG1 fails to boot with MMC/SD |
| LCPD-18620 | AM65x PG2: U-Boot MMC/SD does not work at greater than 25MHz clock |
2.1.7.2. Issues found and closed on this release that may be applicable to prior releases¶
| Record ID | Summary |
|---|---|
| LCPD-21348 | K3: CPSWxG: can’t disable rate limit for TX CPPI channels on Host P0 |
| LCPD-20623 | AM654x UART boot failing to boot |
| LCPD-20618 | k3: cpswxg: bindings not updated |
| LCPD-20170 | am654x UART boot not working |
| LCPD-20099 | U-Boot: AM65: broken boot (Both PG1.0 and 2.0) |
| LCPD-20026 | AM654: PG1.0: MMC boot failure with SDK 7.1 on some boards |
| LCPD-20024 | OPTEE dunfell bleeding builds fail |
| LCPD-19946 | remoteproc/k3-r5f: Fix couple of warnings |
| LCPD-19864 | AM65xx: Support SD card modes not documented in the SDK documentation |
2.1.7.3. Errata workarounds¶
| Record ID | Summary | Workaround | ErrataID |
|---|---|---|---|
| LCPD-18979 | MCAN: Message Transmitted with Wrong Arbitration and Control Fields (Early Start of Frame) | i939 | |
| LCPD-14579 | DSS : DSS Does Not Support YUV Pixel Data Formats | i2000 | |
| LCPD-17788 | PCI-Express: GEN3 (8GT/s) Operation Not Supported. | i2104 | |
| LCPD-17783 | USB: USB2PHY Charger Detect is enabled by default without VBUS presence | i2075 | |
| LCPD-19447 | DSS: Disabling a layer connected to Overlay may result in synclost during the next frame | i2097 | |
| LCPD-19965 | OSPI PHY Controller Bug Affecting Read Transactions | i2189 |
2.1.7.4. SDK Known Issues¶
| Record ID | Summary | Workaround |
|---|---|---|
| LCPD-21527 | AM654x -GLMark2 Wayland benchmark test fails | |
| LCPD-19948 | Yocto: stream recipe is incorrect | |
| LCPD-19858 | OE: OPTEE label used in SDK is old and wrong | |
| LCPD-18270 | Ivi shell test fails. Lib ivi-controller.so and other components are missing from the file system | |
| LCPD-17449 | libasan_preinit.o is missing in devkit | |
| LCPD-17413 | QT Webengine-based browser: the mouse does not work within the web page with QPA EGLFS | |
| LCPD-17412 | QT5 Webengine-based browser crashing with any resize operation | |
| LCPD-13817 | Qt5 Webengine-based broswer does not work on AM654x with pagesize = 64k | |
| LCPD-13816 | Chromium-wayland broswer does not work on AM654x with page size = 64k |
2.1.7.5. U-Boot Known Issues¶
| Record ID | Summary | Workaround |
|---|---|---|
| LCPD-22188 | j721e and am65 hs fails to build on 2021.01 uboot | |
| LCPD-18627 | uboot does not read the reserve-memory from the fdt | |
| LCPD-17770 | U-Boot: Fix order of MCU R5 shutdown depending on cluster mode | |
| LCPD-16696 | U-Boot does not recognize SD-Card after re-insert/change | |
| LCPD-16524 | Need to adjust RMW bit when using enabling ECC | None |
| LCPD-15873 | There is no dtbo in u-boot for PCIe x1 + usb3 daughter card | None |
| LCPD-14843 | U-boot should support default settings for netboot | None |
2.1.7.6. Linux Kernel Known Issues¶
| Record ID | Summary | Workaround |
|---|---|---|
| LCPD-22239 | 2021.00 idk and pcie dtbs are missing for am654 | |
| LCPD-21536 | AM654x - Display port tests fail due to tidss not found | |
| LCPD-20243 | AM65x Transition Kernel: pru-icssg support for100M half duplex mode is broken | |
| LCPD-20014 | remoteproc: TX_PRU: IRQ vring, IRQ kick not found error message on console | |
| LCPD-19929 | Industrial protocols documentation | |
| LCPD-19924 | [AM65xx] ICSS-G TCP receive throughput degraded | |
| LCPD-19923 | [AM65x] Linux reboot command fails | |
| LCPD-19873 | Pings not received by DUT over Ethernet VLAN | |
| LCPD-19861 | ICSSG: Unregistered multicast MAC packets are still visible in non-promiscuous mode | |
| LCPD-19859 | ETH ICSSG netperf benchmark returns lower performance than expected | |
| LCPD-19580 | am654- unable to select a mode (sdhci?) | |
| LCPD-19447 | DSS: Disabling a layer connected to Overlay may result in synclost during the next frame | |
| LCPD-18979 | MCAN: Message Transmitted with Wrong Arbitration and Control Fields (Early Start of Frame) | |
| LCPD-18860 | isolcpus in the command line is not honored | |
| LCPD-18788 | Uboot: Could not bring up PCIe interface | |
| LCPD-18756 | ICSSG: eth5 and eth6 unknown interfaces | |
| LCPD-18684 | syscalls sync failures: fdatasync03, fsync04, sync03, syncfs01, sync_file_range02 | |
| LCPD-18665 | Am65x Pg2: Board cannot do soft reboot when booting from SD card | |
| LCPD-18297 | AM6: OV5640: 176x144 does not work | |
| LCPD-18289 | pcie-usb tests sometimes fail | |
| LCPD-18258 | IPSEC perfomance failures | |
| LCPD-18233 | MMC irq affinity to core 1 is not working. | |
| LCPD-18228 | PCI PM runtime suspend is not increasing | |
| LCPD-18212 | am6 failed to boot due to FDT creation failed! hanging 3 of 100 times | |
| LCPD-17908 | ICSSG: dual-emac: udp packets ocassionally sent out of order on egress | |
| LCPD-17800 | CPSW: Master/Slave resolution failed message seen at console | |
| LCPD-17798 | 2020 LTS: INTA/INTR smp_affinity failure and IRQ allocation issues. | |
| LCPD-17777 | AES HW is not exercised | |
| LCPD-17673 | No software documentation for the Timer module | |
| LCPD-17471 | device hang when restarting crashed R5F | |
| LCPD-17115 | BUG: sleeping function called from invalid context at kernel/locking/rtmutex.c:967 | |
| LCPD-16845 | OPP freq update in DT impacts only cluster0 | |
| LCPD-16534 | remoteproc/k3-r5f: PDK IPC echo_test image fails to do IPC in remoteproc mode on second run | None |
| LCPD-16406 | Seeing “e1000#0: ERROR: Hardware Initialization Failed” sometimes when do dhcp via pcie-eth | |
| LCPD-15819 | tidss: the driver should reject dual-display setup, as it is not supported | |
| LCPD-15540 | uvc-gadget results in segmentation fault | |
| LCPD-14183 | am654x-idk failed to login to kernel a few times (7/1000) | |
| LCPD-13938 | PCIe EP read/write/copy test failed with larger sizes | |
| LCPD-13936 | Uboot dhcp timeout 1 of 100 times | |
| LCPD-13653 | am65x-evm could not boot from MMC/SD when MMC/SD is backup boot mode | No workaround |
| LCPD-13603 | One board could not boot rootfs from more than one SDHC card | |
| LCPD-13445 | Seldom kernel oops triggered by prueth_netdev_init | |
| LCPD-13410 | Reboot command is not operational |
2.1.7.7. RT Linux Kernel Known Issues¶
| Record ID | Summary | Workaround |
|---|---|---|
| LCPD-6663 | [RT] Kmemleak is buggy and boot is crashed randomly | |
| LCPD-22238 | RT linux build sometimes fails to boot - might be related to remoteproc2 |
2.1.8. Installation and Usage¶
The Software Developer’s Guide provides instructions on how to setup up your Linux development environment, install the SDK and start your development. It also includes User’s Guides for various Example Applications and Code Composer Studio.
2.1.9. Host Support¶
The Processor SDK is developed, built and verified on Ubuntu 16.04 and 18.04. Details on how to create a virtual machine to load Ubuntu are described in this page.
Note
Processor SDK Installer is 64-bit, and installs only on 64-bit host machine. Support for 32-bit host is dropped as Linaro toolchain is available only for 64-bit machines