3.6.3.4. PRU_ICSSG Two Port Ethernet Switch
PRU_ICSSG can operate as VLAN aware Switch mode with two external physical ports and one internal host port. By default, interfaces come up in Dual independent EMAC mode and can be changed to operate in Switch mode at runtime. Note that changing from Dual EMAC to Switch mode needs loading of different firmwares to various PRU cores and thus have to follow specific sequence as shown in below sections:
3.6.3.4.1. Enabling Switch mode
Example assuming ETH1 and ETH2 as ICSSG0 interfaces:
ip link set dev eth1 down
ip link set dev eth2 down
devlink dev param set platform/icssg0-eth name switch_mode value 1 cmode runtime
ip link add name br0 type bridge
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev br0 up
ip link set dev eth1 up
ip link set dev eth2 up
bridge vlan add dev br0 vid 1 pvid untagged self
3.6.3.4.2. Going back to Dual EMAC mode
ip link set dev br0 down
ip link set dev eth1 nomaster
ip link set dev eth2 nomaster
ip link set dev eth1 down
ip link set dev eth2 down
devlink dev param set platform/icssg0-eth name switch_mode value 0 cmode runtime
ip link del name br0 type bridge
ip link set dev eth1 up
ip link set dev eth2 up
3.6.3.4.3. Turn On/Off Spanning Tree Protocol (STP)
ip link set dev br0 type bridge stp_state 1/0
3.6.3.4.4. VLAN configuration
bridge vlan add dev br0 vid 1 pvid untagged self <---- add cpu port to VLAN 1
This step is mandatory for bridge/default_pvid.
3.6.3.4.5. Adding extra VLANs
untagged:
bridge vlan add dev eth1 vid 100 pvid untagged master bridge vlan add dev eth1 vid 100 pvid untagged master bridge vlan add dev br0 vid 100 pvid untagged self <---- Add cpu port to VLAN100tagged:
bridge vlan add dev eth1 vid 100 master bridge vlan add dev eth1 vid 100 master bridge vlan add dev br0 vid 100 pvid tagged self <---- Add cpu port to VLAN100
3.6.3.4.6. Forwarding Data Bases (FDBs)
Forwarding entries for MAC addresses are automatically added on the appropriate switch port upon detection as default operation as an unmanaged bridge. For managed bridge operation manually add FDB entries as required.
Manually adding FDBs:
bridge fdb add aa:bb:cc:dd:ee:ff dev eth1 master vlan 100
bridge fdb add aa:bb:cc:dd:ee:fe dev eth1 master <---- Add on all VLANs
3.6.3.4.7. Multicast Data Bases (MDBs)
Multicast entries are automatically added on the appropriate switch port upon detection as default operation as an unmanaged bridge. For managed bridge operation manually add MDB entries as required.
Manually adding MDBs:
bridge mdb add dev br0 port eth1 grp 239.1.1.1 permanent vid 100
bridge mdb add dev br0 port eth1 grp 239.1.1.1 permanent <---- Add on all VLANs
3.6.3.4.8. Multicast flooding
CPU port mcast_flooding is always on
Turning flooding on/off on switch ports:
bridge link set dev eth1 mcast_flood on/off
3.6.3.4.9. Limitations of switch mode offloading support
VLAN offloading is limited to 0-256 VIDs.
MDB/FDB static entries are limited to 511 entries and different FDBs can hash to same bucket and thus may not be completely offloaded
3.6.3.4.10. Cut Through Forwarding
Caution
The Cut Through configuration interface could be changed significantly in the future depending on Linux Kernel mainline development.
ICSSG Switch firmware now supports cut through forwarding. Cut Through feature allows forwarding packet from one external port to another without being stored in Port FIFOs thus reducing overall latency for packet forwarding.
Limitations
Feature is not available in dual EMAC mode.
Cut Through forwarding is only supported between external ports and no support for Cut Through to host port currently.
Cut Through is not supported with 10/100 half-duplex.
Cut Through is not supported with any form of flow control.
If Intersperced Express Traffic (IET) is enabled, then Cut Through can only be enabled on an express priority queue and not on preemptible queues.
Assuming eth1 and eth2 are the active ports of ICSSG2 on AM654x-IDK, to enable cut through run below commands,
ip link set eth1 down
ip link set eth2 down
devlink dev param set platform/icssg2-eth name cut_thru value 1 cmode runtime # To enable cut thru for tx0 queue
devlink dev param set platform/icssg2-eth name cut_thru value 2 cmode runtime # To enable cut thru for tx1 queue
devlink dev param set platform/icssg2-eth name cut_thru value 3 cmode runtime # To enable cut thru for tx0 and tx1 queues
ip link set eth1 up
ip link set eth2 up
To enable cut through for multiple (assume q1, q2 and q3) queues. Pass the value 2q1 + 2q2 + 2q3 to the devlink command.
To show the current cut through status, run the below command,
devlink dev param show platform/icssg2-eth name cut_thru
platform/icssg2-eth:
name cut_thru type driver-specific
values:
cmode runtime value 133
Here the value is shown as 133 (Binary 10000101). This means that cut through is enabled for q0, q2 and q7 queues. As bit 0,1 and 7 are set in the binary representation of the value 133.
To disable cut through on all queues
devlink dev param set platform/icssg2-eth name cut_thru value 0 cmode runtime
3.6.3.4.11. SRAM Requirement
The ICSSG Ethernet driver can be used in switch mode. Two icssg ports are used per switch.
SRAM Required for each switch (per two ports) is 256 KB.
For each ICSSG switch, the SRAM required needs to be contiguous.
PRUETH only uses the required amount of SRAM from the SRAM/MSMC pool. If PRUETH doesn’t get the required amount of SRAM, the prueth_probe() API will return with -ENOMEM error.