3.2.2.20. MMCSD
3.2.2.20.1. Introduction
The multimedia card secure digital (MMCSD) host controller provides an interface between a local host (LH) such as a microprocessor unit (MPU) or digital signal processor (DSP) and either embedded multimedia card (eMMC), secure digital (SD), or secure digital input/output (SDIO) devices. The MMCSD host controller handles MMCSD and SDIO protocol with minimal LH intervention.
The following image shows the MMCSD Driver Architecture:
3.2.2.20.2. References
3.2.2.20.3. Features
The MMCSD driver supports the following features:
Support ADMA for DMA transfers
HS400 speed mode (SR1.2)
HS200 speed mode (SR1.1)
Support for both built-in and module mode
ext2/ext3/ext4 file system support
3.2.2.20.4. Supported ultra high speed (UHS) modes
SD
Platform |
SDR12 |
SDR25 |
SDR50 |
DDR50 |
SDR104 |
|---|---|---|---|---|---|
AM62* |
Y |
Y |
Y |
Y |
Y |
AM62ax |
Y |
Y |
Y |
Y |
Y |
am64x |
Y |
Y |
Y |
Y |
Y |
am62px |
Y |
Y |
Y |
Y |
Y |
am62lx |
N |
N |
N |
N |
N |
eMMC
Platform |
DDR52 |
HS200 |
HS400 |
|---|---|---|---|
AM62* |
Y |
Y |
N |
AM62ax |
Y |
Y |
N |
am64x |
Y |
Y |
N |
am62px SR1.1 |
Y |
Y |
N |
am62px SR1.2 |
Y |
Y |
Y |
am62lx |
Y |
Y |
N |
3.2.2.20.5. Driver configuration
The default kernel configuration enables support for MMCSD driver as built-in to kernel. TI SDHCI driver is used. Following options need to be configured in Linux Kernel for successfully selecting SDHCI driver for AM64x.
Enable SDHCI support (CONFIG_MMC_SDHCI)
Device Drivers -->
MMC/SD/SDIO card support -->
<*> Secure Digital Host Controller Interface support
Enable SDHCI platform helper (CONFIG_MMC_SDHCI_PLTFM)
Device Drivers -->
MMC/SD/SDIO card support -->
Secure Digital Host Controller Interface support -->
<*> SDHCI platform and OF driver helper
Enable SDHCI controller for TI device (CONFIG_MMC_SDHCI_AM654)
Device Drivers -->
MMC/SD/SDIO card support -->
<*> Support for the SDHCI Controller in TI's AM654 SOCs
3.2.2.20.6. MMC support in Linux
There is no missing MMC support for AM64x device.
3.2.2.20.7. Steps for working around SD card issues in Linux
In some cases, failures can be seen while using some SD cards:
Kernel fails to enumerate SD, thus failing to mount the root file system. This is the case when kernel hangs during boot with a message similar to the following:
[ 2.563279] Waiting for root device PARTUUID=835b171b-02...A lot of SDHCI register dumps logs getting printed continuously:
[ 10.811723] mmc1: Got data interrupt 0x00000002 even though no data operation was in progress. [ 10.820321] mmc1: sdhci: ============ SDHCI REGISTER DUMP =========== [ 10.826745] mmc1: sdhci: Sys addr: 0x00000080 | Version: 0x00001004 [ 10.833169] mmc1: sdhci: Blk size: 0x00007200 | Blk cnt: 0x00000080 [ 10.839593] mmc1: sdhci: Argument: 0x00000000 | Trn mode: 0x00000033 [ 10.846016] mmc1: sdhci: Present: 0x01f70000 | Host ctl: 0x0000001f [ 10.852440] mmc1: sdhci: Power: 0x0000000f | Blk gap: 0x00000080 [ 10.858864] mmc1: sdhci: Wake-up: 0x00000000 | Clock: 0x00000007 [ 10.865287] mmc1: sdhci: Timeout: 0x00000000 | Int stat: 0x00000000 [ 10.871711] mmc1: sdhci: Int enab: 0x03ff008b | Sig enab: 0x03ff008b [ 10.878134] mmc1: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000000 [ 10.884557] mmc1: sdhci: Caps: 0x3de8c801 | Caps_1: 0x18002407 [ 10.890981] mmc1: sdhci: Cmd: 0x00000c1a | Max curr: 0x00000000 [ 10.897404] mmc1: sdhci: Resp[0]: 0x00000b00 | Resp[1]: 0x0075cf7f [ 10.903828] mmc1: sdhci: Resp[2]: 0x32db7900 | Resp[3]: 0x00000900 [ 10.910251] mmc1: sdhci: Host ctl2: 0x0000000b [ 10.914682] mmc1: sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x00000000a2e90200
Given below are the list of various workarounds that can be done in the device tree node to get SD card working. The workarounds are ordered from least to most performance impacting.
Note
All the changes mentioned below, are to be done in the MMCSD device tree node corresponding to the SD instance. This is usually the first (index starting from zero) instance.
Restricting to a given speed mode
By default the kernel driver tries to enumerate an SD card in the highest supported speed mode. Below is the order that the driver tries to enumerate an SD card:
SDR104
DDR50
SDR50
SD HS
SD legacy
The sdhci-caps-mask can be added to the DT node to cap at a specific mode:
Limit to DDR50:
sdhci-caps-mask = <0x00000003 0x00000000>Limit to SD HS:
sdhci-caps-mask = <0x00000007 0x00000000>Limit to SD legacy:
sdhci-caps-mask = <0x00000007 0x00200000>
The following is an example DT node with the added sdhci-caps-mask:
&sdhci1 { /* SD/MMC */ vmmc-supply = <&vdd_mmc1>; vqmmc-supply = <&vdd_sd_dv>; pinctrl-names = "default"; pinctrl-0 = <&main_mmc1_pins_default>; ti,driver-strength-ohm = <50>; disable-wp; sdhci-caps-mask = <0x00000003 0x00000000>; /* Limiting to DDR50 speed mode */ };
Limiting to SD HS speed mode can also be done by using the property no-1-8-v. This disables switching to 1.8V, which is required for UHS speed modes(SDR104, DDR50, SDR50, SDR25, SDR12):
&sdhci1 { /* SD/MMC */ vmmc-supply = <&vdd_mmc1>; vqmmc-supply = <&vdd_sd_dv>; pinctrl-names = "default"; pinctrl-0 = <&main_mmc1_pins_default>; ti,driver-strength-ohm = <50>; disable-wp; no-1-8-v; /* disabling all the UHS modes */ };
Reduce the bus width
The SD interface supports a bus width of 4. It can be reduced to 1 by changing the bus-width device tree property from 4 to 1.
diff --git a/arch/arm64/boot/dts/ti/k3-am62-main.dtsi b/arch/arm64/boot/dts/ti/k3-am62-main.dtsi index 7bbfcb158842..2ef974f7206f 100644 --- a/arch/arm64/boot/dts/ti/k3-am62-main.dtsi +++ b/arch/arm64/boot/dts/ti/k3-am62-main.dtsi @@ -424,7 +424,7 @@ ti,itap-del-sel-sdr12 = <0x0>; ti,itap-del-sel-sdr25 = <0x0>; ti,clkbuf-sel = <0x7>; - bus-width = <4>; + bus-width = <1>; }; sdhci2: mmc@fa20000 {
3.2.2.20.8. Listing MMC devices from Linux
eMMC and SD cards register with the MMC subsystem and are available as a block device
as /dev/mmcblkn. To find the device index n corresponding to an eMMC device,
check which device includes mmcblknboot0 and mmcblknboot1. Here,
mmcblk0* is in eMMC.
root@<machine>:~# ls -l /dev/mmcblk*
brw-rw---- 1 root disk 179, 0 Jan 1 00:10 /dev/mmcblk0
brw-rw---- 1 root disk 179, 32 Jan 8 2025 /dev/mmcblk0boot0
brw-rw---- 1 root disk 179, 64 Jan 8 2025 /dev/mmcblk0boot1
brw-rw---- 1 root disk 179, 1 Jan 1 00:14 /dev/mmcblk0p1
crw------- 1 root root 239, 0 Jan 1 00:00 /dev/mmcblk0rpmb
brw-rw---- 1 root disk 179, 96 Jan 8 2025 /dev/mmcblk1
brw-rw---- 1 root disk 179, 97 Jan 1 00:00 /dev/mmcblk1p1
brw-rw---- 1 root disk 179, 98 Jan 8 2025 /dev/mmcblk1p2
The disk partitions for each MMC device are displayed as /dev/mmcblknpx.
To check existing or mounted disk partitions for an eMMC device, use the
command lsblk, such as:
root@<machine>:~# lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mmcblk0 179:0 0 14.8G 0 disk
mmcblk0boot0 179:32 0 31.5M 1 disk
mmcblk0boot1 179:64 0 31.5M 1 disk
mmcblk1 179:96 0 14.8G 0 disk
|-mmcblk1p1 179:97 0 128M 0 part /run/media/boot-mmcblk1p1
`-mmcblk1p2 179:98 0 1.9G 0 part /
Use the mount and umount commands to mount and unmount formatted disk partitions, usually to virtual file allocation table (vfat) or fourth extended file system (ext4) types.
3.2.2.20.9. Create partitions in eMMC UDA
In eMMC, the user data area (UDA) HW partition is the primary storage space generally used
to flash the root filesystem (rootfs). To create disk partitions in UDA, use the fdisk command.
For ex: fdisk /dev/mmcblkn in which n is typically 0 or 1. In the previous example,
eMMC is fdisk /dev/mmcblk0.
For documentation on using fdisk command, go to: fdisk how-to.
Erase eMMC UDA
In Linux, before creating disk partitions, we can optionally erase eMMC UDA by using dd command:
root@<machine>:~# umount /dev/mmcblk0*
root@<machine>:~# dd if=/dev/zero of=/dev/mmcblk0 bs=1M count=n
where n should be determined according to the following formula: count = total size UDA (bytes) / bs.
3.2.2.20.9.1. Create “boot” partition
In this example create a “boot” partition of size 400 MiB which can be formatted to vfat type and will store the boot loader binaries.
root@<machine>:~# fdisk /dev/mmcblk0
Welcome to fdisk (util-linux 2.39.3).
Changes will remain in memory only, until you decide to write them.
Be careful before using the write command.
Command (m for help): n
Partition type
p primary (0 primary, 0 extended, 4 free)
e extended (container for logical partitions)
Select (default p):
Using default response p.
Partition number (1-4, default 1):
First sector (2048-31080447, default 2048):
Last sector, +/-sectors or +/-size{K,M,G,T,P} (2048-31080447, default 31080447): +400M
Created a new partition 1 of type 'Linux' and of size 400 MiB.
Partition #1 contains a vfat signature.
Do you want to remove the signature? [Y]es/[N]o: y
The signature will be removed by a write command.
Command (m for help): a
Selected partition 1
The bootable flag on partition 1 is enabled now.
Command (m for help): t
Selected partition 1
Hex code or alias (type L to list all): c
Changed type of partition 'Linux' to 'W95 FAT32 (LBA)'.
Command (m for help): w
The partition table has been altered.
[ 644.818358] mmcblk0: p1
Calling ioctl() to re-read partition table.
Syncing disks.
Make sure bootable flag is set for “boot” partition, ROM might not boot from this partition if bootable flag is not set.
3.2.2.20.9.2. Create “root” partition
In this example create a “root” partition which can be formatted to ext4 type and will store Linux kernel Image, DTB, and the rootfs.
root@<machine>:~# fdisk /dev/mmcblk0
Welcome to fdisk (util-linux 2.39.3).
Changes will remain in memory only, until you decide to write them.
Be careful before using the write command.
This disk is currently in use - repartitioning is probably a bad idea.
It's recommended to umount all file systems, and swapoff all swap
partitions on this disk.
Command (m for help): n
Partition type
p primary (1 primary, 0 extended, 3 free)
e extended (container for logical partitions)
Select (default p):
Using default response p.
Partition number (2-4, default 2):
First sector (821248-31080447, default 821248):
Last sector, +/-sectors or +/-size{K,M,G,T,P} (821248-31080447, default 31080447):
Created a new partition 2 of type 'Linux' and of size 14.4 GiB.
Command (m for help): t
Partition number (1,2, default 2): 2
Hex code or alias (type L to list all): 83
Changed type of partition 'Linux' to 'Linux'.
Command (m for help): w
The partition table has been altered.
Syncing disks.
3.2.2.20.10. Formatting eMMC partitions from Linux
After creating a partition/s, the partition can be formatted with the mkfs command.
For ex: mkfs -t ext4 /dev/mmcblkn where mmcblk{n} is the MMC device with the new
disk partitions to format. The general syntax for formatting disk partitions in Linux is:
mkfs.vfat [OPTIONS] TARGET [BLOCKS]
mkfs.ext4 [-c|-l filename] [-b block-size] [-C cluster-size]
3.2.2.20.10.1. Format to vfat
In this example, format the “boot” partition to type vfat.
root@<machine>:~# mkfs.vfat -F 32 -n "boot" /dev/mmcblk0p1
3.2.2.20.10.2. Format to ext4
In this example, format the “root” partition to type ext4.
root@<machine>:~# mkfs.ext4 -L "root" /dev/mmcblk0p2
Verify partitions
Verify setup of
mmcblk0p1andmmcblk0p2with lsblk command.root@<machine>:~# lsblk -o name,mountpoint,label,size,uuid NAME MOUNTPOINT LABEL SIZE UUID mmcblk0 14.8G |-mmcblk0p1 boot 400M E4D4-4879 `-mmcblk0p2 root 14.4G 74d40075-07e4-4bce-9401-6fccef68e934 mmcblk0boot0 31.5M mmcblk0boot1 31.5M mmcblk1 29.7G |-mmcblk1p1 /run/media/boot-mmcblk1p1 boot 128M 681F-55DD `-mmcblk1p2 / root 8.7G ead4c8bb-fa37-4c4d-9ba3-47a1f3824764
3.2.2.20.11. Flash eMMC for MMCSD boot
In this example, we show one simple method for flashing to eMMC for MMCSD boot from eMMC UDA in filesystem (FS) mode. Know this is not the only method for flashing the eMMC for this boot mode.
This example assumes the current boot mode is MMCSD boot from SD (FS mode)
3.2.2.20.11.1. Flash to eMMC “boot” partition
root@<machine>:~# umount /run/media/*
root@<machine>:~# mkdir /mnt/eboot /mnt/sdboot
root@<machine>:~# mount /dev/mmcblk0p1 /mnt/eboot
root@<machine>:~# mount /dev/mmcblk1p1 /mnt/sdboot
Verify the partitions are mounted to the correct folders by using lsblk command in the
column labeled MOUNTPOINTS.
root@<machine>:~# lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mmcblk0 179:0 0 14.8G 0 disk
|-mmcblk0p1 179:1 0 400M 0 part /mnt/eboot
`-mmcblk0p2 179:2 0 14.4G 0 part
mmcblk0boot0 179:32 0 31.5M 1 disk
mmcblk0boot1 179:64 0 31.5M 1 disk
mmcblk1 179:96 0 29.7G 0 disk
|-mmcblk1p1 179:97 0 128M 0 part /mnt/sdboot
`-mmcblk1p2 179:98 0 8.7G 0 part /
Now we can copy boot loader binaries to eMMC and umount the partitions when writes finish.
root@<machine>:~# ls /mnt/sdboot/
tiboot3.bin tispl.bin u-boot.img uEnv.txt
root@<machine>:~# cp /mnt/sdboot/* /mnt/eboot/
root@<machine>:~# sync && umount /mnt/*
3.2.2.20.11.2. Flash to eMMC “root” partition
root@<machine>:~# umount /run/media/*
root@<machine>:~# mkdir /mnt/eroot /mnt/sdroot
root@<machine>:~# mount /dev/mmcblk0p2 /mnt/eroot
[69229.982452] EXT4-fs (mmcblk0p2): mounted filesystem 74d40075-07e4-4bce-9401-6fccef68e934 r/w with ordered data mode. Quota mode: none.
root@<machine>:~# mount /dev/mmcblk1p2 /mnt/sdroot
Verify the partitions are mounted to the correct folders by using lsblk command in the
column labeled MOUNTPOINTS.
root@<machine>:~# lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINTS
mmcblk0 179:0 0 14.8G 0 disk
|-mmcblk0p1 179:1 0 400M 0 part
`-mmcblk0p2 179:2 0 14.4G 0 part /mnt/eroot
mmcblk0boot0 179:32 0 31.5M 1 disk
mmcblk0boot1 179:64 0 31.5M 1 disk
mmcblk1 179:96 0 29.7G 0 disk
|-mmcblk1p1 179:97 0 128M 0 part
`-mmcblk1p2 179:98 0 8.7G 0 part /mnt/sdroot
/
Now we can copy rootfs to eMMC (either from SD rootfs or from tar file) and umount the partitions when writes finish.
From SD
root@<machine>:~# ls /mnt/sdroot
bin dev home lost+found mnt proc run srv tmp var
boot etc lib media opt root sbin sys usr
root@<machine>:~# cp -r -a /mnt/sdroot/* /mnt/eroot
root@<machine>:~# sync
root@<machine>:~# umount /mnt/*
[70154.205154] EXT4-fs (mmcblk0p2): unmounting filesystem 74d40075-07e4-4bce-9401-6fccef68e934.
From tar file
This sections requires for tisdk-base-image-<soc>evm.rootfs.tar.xz to have been previously copied to the SD card rootfs.
root@<machine>:~# ls
tisdk-base-image-<soc>-evm.rootfs.tar.xz
root@<machine>:~# tar -xpf tisdk-base-image-<soc>-evm.rootfs.tar.xz -C /mnt/eroot
root@<machine>:~# sync
root@<machine>:~# umount /mnt/*