2.1. Release Notes
2.1.1. Overview
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM64x installer provides everything needed as discussed below to create the embedded system from “scratch” :
Platform/board-support software and configuration files for Linux
U-Boot and Kernel sources and configuration files
An ARM cross-compiling toolchain as well as other host binaries and components
A Yocto/OE compliant filesystem and sources for example applications
A variety of scripts and Makefiles to automate certain tasks
Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
Reference Examples, benchmarks
This release supports SR2.0 High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide
2.1.2. Release versioning scheme
Processor SDK releases follow the 5-duplet versioning scheme YY.RR.EE.CC.SS, where:
YY- Yearly baseline. Increments with each new LTS baseline.RR- Release index within the yearly baseline. Each yearly baseline includes many stable releases.EE- Extended release index within a stable baseline.CC- Release Candidate for common foundational BSP components such as Linux, U-Boot, ATF, OPTEE, Firmware and OE manifest including meta-ti, meta-arago.SS- SDK Release identifier for Distro layers (Yocto meta-tisdk, Armbian, Buildroot) with OOB Demos and Installers.
2.1.3. Licensing
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
Linux Manifest:
<PSDK_PATH>/manifest/software_manifest.htmDebian Manifest:
2.1.4. Software Bill of Materials (SBOM)
Processor SDK AM64x releases include Software Bill of Materials (SBOM) files in SPDX 3.0 format by default. SBOMs for all released artifacts are bundled into a single archive and can be found on the AM64x-SDK-Download-page. For more refer Working with SBOM.
2.1.5. Release 12.01.00.05.03
Released on July 2026
2.1.5.1. What’s new
Processor SDK Linux AM64X Release has following new features:
Second 2026 LTS Reference Release Including RT combined branch model
Important Bug Fixes on top of Processor SDK 12.00.00.07 Release
Review Issue Tracker Section for the new fixes.
Key Release References:
RT Kernel : Real-Time Linux Interrupt Latency numbers here - RT Interrupt Latencies
Snagfactory Support - Snagfactory Tool
Component version:
Kernel 6.18.38
U-Boot 2026.01
Toolchain GCC 15.2
ATF 2.15
OPTEE 4.10.0+
TIFS Firmware v12.01.02 (Click on the link for more information)
Yocto Wrynose/6.0
Security: Post Quantum Cryptography using Module Lattice (ML) Key Encapsulation Mechanism (KEM) or ML-KEM, ML Digital Signature Algorithm (DSA) or ML-DSA, and Stateless Hash-Based (SLH) DSA or SLH-DSA - Post Quantum Cryptography
DM Firmware 12.01.00.18
2.1.6. Build Information
2.1.6.1. Arago (Yocto/OE)
Component |
Branch Info |
Tag Info |
Config Info |
|---|---|---|---|
U-Boot |
|||
TF-A |
|||
OPTEE |
k3-am64x |
||
Linux Firmware |
|||
Linux Kernel |
|||
meta-ti |
am64xx-evm |
||
meta-arago |
|||
meta-tisdk |
2.1.6.2. Debian (Armbian)
Component |
Branch Info |
Tag Info |
Config Info |
|---|---|---|---|
U-Boot |
|||
TF-A |
|||
OPTEE |
|||
Linux Firmware |
|||
Linux Kernel |
|||
Armbian Build |
Build: k3_common.inc + k3.conf
|
2.1.6.3. Buildroot (Buildroot External TI)
Component |
Branch Info |
Tag Info |
Config Info |
|---|---|---|---|
U-Boot |
|||
ATF |
|||
OPTEE |
|||
Linux Firmware |
|||
Linux Kernel |
|||
Buildroot External TI |
|||
Buildroot |
2.1.7. Issues Tracker
Note
Release Specific Issues including details will be published through Software Incident Report (SIR) portal
Further Information can be found at SIR Portal <https://sir.ext.ti.com/>
2.1.7.1. Errata Resolved
Record ID |
Title |
|---|---|
USB2 PHY locks up due to short suspend |
|
USART: Erroneous clear/trigger of timeout interrupt |
|
MMCSD: HS200 and SDR104 Command Timeout Window Too Small |
2.1.7.2. Issues Resolved
Record ID |
Title |
|---|---|
PRUETH: 100M Link fails if auto negotiation disabled |
|
MMCSD: PHY DLL frequency is setting incorrectly for any clock < 200MHz |
2.1.7.3. Issues Open
Record ID |
Title |
|---|---|
am64x: incorrect device id in icssg0_mdio devicetree node |
|
AM64x: DFU Boot hangs on repetitive test |
|
ICSSG: HSR packet out of order |
|
U-Boot binman does not have the provision of SWREV for Board Configurations |
|
Docs: Incorrect secure boot flow description |
|
AM64x CICD does not test PRU |
|
PRU RPMsg swaps which message is sent to which core |
|
cdns: device mode: Linux hangs when USB cable is disconnected |
|
AM64x: Lower core count on variant devices no supported |