3.6.3.4. PRU_ICSSG Two Port Ethernet Switch
PRU_ICSSG can operate as VLAN aware Switch mode with two external physical ports and one internal host port. By default, interfaces come up in Dual independent EMAC mode and can be changed to operate in Switch mode at runtime. Note that changing from Dual EMAC to Switch mode needs loading of different firmwares to various PRU cores and thus have to follow specific sequence as shown in below sections:
3.6.3.4.1. Enabling Switch mode
Example assuming ETH1 and ETH2 as ICSSG0 interfaces:
ip link add name br0 type bridge
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev br0 up
bridge vlan add dev br0 vid 1 pvid untagged self
3.6.3.4.2. Going back to Dual EMAC mode
ip link set dev br0 down
ip link set dev eth1 nomaster
ip link set dev eth2 nomaster
ip link del name br0 type bridge
3.6.3.4.3. Turn On/Off Spanning Tree Protocol (STP)
ip link set dev br0 type bridge stp_state 1/0
3.6.3.4.4. VLAN configuration
bridge vlan add dev br0 vid 1 pvid untagged self <---- add cpu port to VLAN 1
This step is mandatory for bridge/default_pvid.
3.6.3.4.5. Adding extra VLANs
untagged:
bridge vlan add dev eth1 vid 100 pvid untagged master bridge vlan add dev eth1 vid 100 pvid untagged master bridge vlan add dev br0 vid 100 pvid untagged self <---- Add cpu port to VLAN100tagged:
bridge vlan add dev eth1 vid 100 master bridge vlan add dev eth1 vid 100 master bridge vlan add dev br0 vid 100 pvid tagged self <---- Add cpu port to VLAN100
3.6.3.4.6. Forwarding Data Bases (FDBs)
Forwarding entries for MAC addresses are automatically added on the appropriate switch port upon detection as default operation as an unmanaged bridge. For managed bridge operation manually add FDB entries as required.
Manually adding FDBs:
bridge fdb add aa:bb:cc:dd:ee:ff dev eth1 master vlan 100
bridge fdb add aa:bb:cc:dd:ee:fe dev eth1 master <---- Add on all VLANs
3.6.3.4.7. Multicast Data Bases (MDBs)
Multicast entries are automatically added on the appropriate switch port upon detection as default operation as an unmanaged bridge. For managed bridge operation manually add MDB entries as required.
Manually adding MDBs:
bridge mdb add dev br0 port eth1 grp 239.1.1.1 permanent vid 100
bridge mdb add dev br0 port eth1 grp 239.1.1.1 permanent <---- Add on all VLANs
3.6.3.4.8. Multicast flooding
CPU port mcast_flooding is always on
Turning flooding on/off on switch ports:
bridge link set dev eth1 mcast_flood on/off
3.6.3.4.9. Limitations of switch mode offloading support
VLAN offloading is limited to 0-256 VIDs.
MDB/FDB static entries are limited to 511 entries and different FDBs can hash to same bucket and thus may not be completely offloaded
3.6.3.4.10. Cut Through Forwarding
Caution
The Cut Through configuration interface could be changed significantly in the future depending on Linux Kernel mainline development.
ICSSG Switch firmware now supports cut through forwarding. Cut Through feature allows forwarding packet from one external port to another without being stored in Port FIFOs thus reducing overall latency for packet forwarding.
Limitations
Feature is not available in dual EMAC mode.
Cut Through forwarding is only supported between external ports and no support for Cut Through to host port currently.
Cut Through is not supported with 10/100 half-duplex.
Cut Through is not supported with any form of flow control.
If Intersperced Express Traffic (IET) is enabled, then Cut Through can only be enabled on an express priority queue and not on preemptible queues.
The devlink command to enable cut-through takes a u16 value. All 16 bits of it represent queues. BIT 0 to BIT 7 are slice0 queues where as BIT 8 to BIT 15 are slice1 queues. To enable cut-through forwarding in both directions, cut-through will need to be enabled on both slice0 and slice1.
In general, to enable cut through for slice0 qM, qN queues and slice1 qX, qY queues, pass the value \(2^M + 2^N + 2^{8+X} + 2^{8+Y}\) to the devlink command.
Assuming eth1 and eth2 are the active ports of ICSSG1 on AM64xx-EVM, to enable cut through run below commands,
# To enable cut through for slice0 q0
devlink dev param set platform/icssg1-eth name cut_thru value 1 cmode runtime
# To enable cut through for slice0 q1
devlink dev param set platform/icssg1-eth name cut_thru value 2 cmode runtime
# To enable cut through for slice0 q0, q1
devlink dev param set platform/icssg1-eth name cut_thru value 3 cmode runtime
# To enable cut through for slice0 q0, q1 and slice1 q0, q1
devlink dev param set platform/icssg1-eth name cut_thru value 771 cmode runtime
To show the current cut through status, run the below command,
devlink dev param show platform/icssg1-eth name cut_thru
platform/icssg1-eth:
name cut_thru type driver-specific
values:
cmode runtime value 771
Here the value is shown as 771 (Binary 0000 0011 0000 0011). This means that cut through is enabled for q0, q1 of slice0 and q0, q1 of slice1. As bit 0,1,8 and 9 are set in the binary representation of the value 711.
To disable cut through on all queues
devlink dev param set platform/icssg1-eth name cut_thru value 0 cmode runtime
Note
Set up the cut through value first before enabling switch mode to ensure that cut through is working properly. This order ensures that the firmware has the expected cut through value. Setting up switch mode will automatically stop and start the firmware so no need to bring links down and back up again.
3.6.3.4.11. PTP
PTP can be run during switch mode. To run PTP in switch mode, 3 AM64x EVMs need to be connected with middle EVM acting as the switch. Use the following ptp config file on all slave EVMs. For Master EVM, priority1 filed needs to be changed.
# 802.1AS example configuration containing those attributes which
# differ from the defaults. See the file, default.cfg, for the
# complete list of available options.
#
[global]
gmCapable 1
priority1 248
priority2 248
logAnnounceInterval 0
logSyncInterval -3
syncReceiptTimeout 3
neighborPropDelayThresh 800
min_neighbor_prop_delay -20000000
assume_two_step 1
path_trace_enabled 1
follow_up_info 1
transportSpecific 0x1
ptp_dst_mac 01:80:C2:00:00:0E
network_transport L2
delay_mechanism P2P
ingressLatency 88
egressLatency 288
Steps:
On EVM1 run below command assuming eth1 is the ICSSG interface connected and ptp2 is the device associated with it.
ptp4l -P -2 -H -i eth1 -f gPTP.cfg --step_threshold=1 -m -q -p /dev/ptp2On EVM3 run below command assuming eth2 is the ICSSG interface connected and ptp2 is the device associated with it.
ptp4l -P -2 -H -i eth2 -f gPTP.cfg --step_threshold=1 -m -q -p /dev/ptp2On EVM2 acting as the switch run below command assuming eth1 and eth2 are the ICSSG interfaces connected and ptp2 is the device associated with them.
# Edit priority1 of EVM2 to make sure it runs as master. sed -i 's/priority1 248/priority1 100/g' gPTP.cfg # Add mdb entry for switch interface with multicast mac address used for forwarding PTP packets. # This address is same as ptp_dst_mac field in gPTP.cfg file. bridge mdb add dev br0 port br0 grp $ptp_dst_mac permanent vid 1 # Start PTP on Master EVM ptp4l -P -2 -H -i eth1 -i eth2 -f gPTP.cfg --step_threshold=1 -m -q -p /dev/ptp2
Observed Outputs:
On EVM1
root@am64xx-evm:~# cat gPTP.cfg | grep priority priority1 248 priority2 248 root@am64xx-evm:~# ptp4l -P -2 -H -i eth1 -f gPTP.cfg --step_threshold=1 -m -q -p /dev/ptp2 ptp4l[3673.262]: selected /dev/ptp2 as PTP clock ptp4l[3673.296]: port 1: INITIALIZING to LISTENING on INIT_COMPLETE ptp4l[3673.297]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE ptp4l[3676.325]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES ptp4l[3676.325]: selected local clock 70ff76.fffe.1e2db3 as best master ptp4l[3676.325]: port 1: assuming the grand master role ptp4l[3677.050]: port 1: new foreign master 70ff76.fffe.1f3f8e-1 ptp4l[3679.050]: selected best master clock 70ff76.fffe.1f3f8e ptp4l[3679.050]: port 1: MASTER to UNCALIBRATED on RS_SLAVE ptp4l[3679.433]: port 1: UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED ptp4l[3680.183]: rms 11123 max 14721 freq +9512 +/- 7654 delay 83 +/- 0 ptp4l[3681.184]: rms 2050 max 3143 freq +2824 +/- 2781 delay 83 +/- 0 ptp4l[3682.184]: rms 3425 max 3591 freq -3401 +/- 910 delay 83 +/- 0 ptp4l[3683.185]: rms 2175 max 2887 freq -4622 +/- 87 delay 83 +/- 0 ptp4l[3684.185]: rms 705 max 1163 freq -3960 +/- 252 delay 83 +/- 0 ptp4l[3685.185]: rms 124 max 196 freq -3218 +/- 159 delay 84 +/- 0 ptp4l[3686.186]: rms 203 max 216 freq -2865 +/- 49 delay 84 +/- 0 ptp4l[3687.186]: rms 121 max 156 freq -2810 +/- 8 delay 84 +/- 0 ptp4l[3688.186]: rms 39 max 64 freq -2846 +/- 13 delay 84 +/- 0 ptp4l[3689.187]: rms 6 max 12 freq -2886 +/- 8 delay 84 +/- 0 ptp4l[3690.187]: rms 14 max 20 freq -2910 +/- 7 delay 84 +/- 0 ptp4l[3691.188]: rms 7 max 12 freq -2911 +/- 5 delay 84 +/- 0 ptp4l[3692.188]: rms 5 max 9 freq -2909 +/- 6 delay 85 +/- 0 ptp4l[3693.189]: rms 4 max 8 freq -2908 +/- 6 delay 84 +/- 0 ptp4l[3694.189]: rms 5 max 7 freq -2907 +/- 7 delay 85 +/- 0 ptp4l[3695.189]: rms 3 max 8 freq -2911 +/- 4 delay 84 +/- 0 ptp4l[3696.190]: rms 4 max 8 freq -2913 +/- 5 delay 84 +/- 0 ptp4l[3697.190]: rms 3 max 4 freq -2908 +/- 4 delay 84 +/- 0 ptp4l[3698.191]: rms 4 max 9 freq -2908 +/- 6 delay 83 +/- 0 ptp4l[3699.191]: rms 5 max 9 freq -2905 +/- 6 delay 83 +/- 0 ptp4l[3700.191]: rms 5 max 9 freq -2913 +/- 5 delay 85 +/- 0 ptp4l[3701.192]: rms 4 max 7 freq -2911 +/- 5 delay 83 +/- 0 ptp4l[3702.192]: rms 4 max 5 freq -2908 +/- 5 delay 83 +/- 0 ptp4l[3703.192]: rms 5 max 8 freq -2905 +/- 6 delay 84 +/- 0 ptp4l[3704.193]: rms 6 max 8 freq -2897 +/- 3 delay 84 +/- 0 ptp4l[3705.193]: rms 5 max 8 freq -2898 +/- 7 delay 84 +/- 0 ptp4l[3706.193]: rms 5 max 12 freq -2904 +/- 6 delay 84 +/- 0 ptp4l[3707.194]: rms 4 max 9 freq -2907 +/- 5 delay 85 +/- 0 ptp4l[3708.194]: rms 3 max 6 freq -2907 +/- 4 delay 86 +/- 0 ptp4l[3709.195]: rms 5 max 7 freq -2905 +/- 7 delay 85 +/- 0
On EVM2 actings as switch
root@am64xx-evm:~# cat gPTP.cfg | grep priority priority1 100 priority2 248 root@am64xx-evm:~# ptp4l -P -2 -H -i eth1 -i eth2 -f gPTP.cfg --step_threshold=1 -m -q -p /dev/ptp2 ptp4l[3635.479]: selected /dev/ptp2 as PTP clock ptp4l[3635.516]: port 1: INITIALIZING to LISTENING on INIT_COMPLETE ptp4l[3635.548]: port 2: INITIALIZING to LISTENING on INIT_COMPLETE ptp4l[3635.549]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE ptp4l[3638.522]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES ptp4l[3638.522]: selected local clock 70ff76.fffe.1f3f8e as best master ptp4l[3638.522]: port 1: assuming the grand master role ptp4l[3639.278]: port 2: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES ptp4l[3639.278]: selected local clock 70ff76.fffe.1f3f8e as best master ptp4l[3639.278]: port 1: assuming the grand master role ptp4l[3639.278]: port 2: assuming the grand master role ptp4l[3660.790]: port 2: new foreign master 70ff76.fffe.1f3e6a-1 ptp4l[3662.790]: selected best master clock 70ff76.fffe.1f3e6a ptp4l[3662.790]: port 1: assuming the grand master role ptp4l[3662.791]: port 2: assuming the grand master role ptp4l[3663.800]: port 1: new foreign master 70ff76.fffe.1e2db3-1 ptp4l[3665.800]: selected best master clock 70ff76.fffe.1e2db3 ptp4l[3665.800]: port 1: assuming the grand master role ptp4l[3665.800]: port 2: assuming the grand master role
On EVM3
root@am64xx-evm:~# cat gPTP.cfg | grep priority priority1 248 priority2 248 root@am64xx-evm:~# ptp4l -P -2 -H -i eth2 -f gPTP.cfg --step_threshold=1 -m -q -p /dev/ptp2 ptp4l[3651.298]: selected /dev/ptp2 as PTP clock ptp4l[3651.336]: port 1: INITIALIZING to LISTENING on INIT_COMPLETE ptp4l[3651.337]: port 0: INITIALIZING to LISTENING on INIT_COMPLETE ptp4l[3654.775]: port 1: LISTENING to MASTER on ANNOUNCE_RECEIPT_TIMEOUT_EXPIRES ptp4l[3654.775]: selected local clock 70ff76.fffe.1f3e6a as best master ptp4l[3654.775]: port 1: assuming the grand master role ptp4l[3655.266]: port 1: new foreign master 70ff76.fffe.1f3f8e-2 ptp4l[3657.266]: selected best master clock 70ff76.fffe.1f3f8e ptp4l[3657.266]: port 1: MASTER to UNCALIBRATED on RS_SLAVE ptp4l[3657.520]: port 1: UNCALIBRATED to SLAVE on MASTER_CLOCK_SELECTED ptp4l[3658.270]: rms 6047 max 8004 freq +5665 +/- 4160 delay 88 +/- 0 ptp4l[3659.271]: rms 1112 max 1709 freq +2037 +/- 1510 delay 89 +/- 0 ptp4l[3660.271]: rms 1865 max 1953 freq -1356 +/- 501 delay 89 +/- 0 ptp4l[3661.271]: rms 1190 max 1582 freq -2032 +/- 45 delay 90 +/- 0 ptp4l[3662.272]: rms 386 max 637 freq -1668 +/- 142 delay 89 +/- 0 ptp4l[3663.272]: rms 71 max 111 freq -1256 +/- 89 delay 89 +/- 0 ptp4l[3664.272]: rms 109 max 119 freq -1070 +/- 27 delay 89 +/- 0 ptp4l[3665.273]: rms 67 max 83 freq -1037 +/- 5 delay 89 +/- 0 ptp4l[3666.273]: rms 22 max 35 freq -1056 +/- 8 delay 89 +/- 0 ptp4l[3667.273]: rms 6 max 11 freq -1073 +/- 8 delay 89 +/- 0 ptp4l[3668.274]: rms 10 max 13 freq -1094 +/- 4 delay 89 +/- 0 ptp4l[3669.274]: rms 3 max 5 freq -1090 +/- 3 delay 89 +/- 0 ptp4l[3670.274]: rms 3 max 5 freq -1087 +/- 4 delay 89 +/- 0 ptp4l[3671.274]: rms 5 max 7 freq -1086 +/- 6 delay 89 +/- 0 ptp4l[3672.275]: rms 4 max 7 freq -1089 +/- 5 delay 89 +/- 0 ptp4l[3673.275]: rms 5 max 7 freq -1087 +/- 7 delay 89 +/- 0 ptp4l[3674.275]: rms 3 max 4 freq -1088 +/- 4 delay 88 +/- 0 ptp4l[3675.276]: rms 4 max 8 freq -1091 +/- 5 delay 88 +/- 0 ptp4l[3676.276]: rms 5 max 6 freq -1084 +/- 5 delay 90 +/- 0 ptp4l[3677.276]: rms 3 max 6 freq -1085 +/- 5 delay 90 +/- 0 ptp4l[3678.276]: rms 5 max 10 freq -1084 +/- 7 delay 90 +/- 0 ptp4l[3679.277]: rms 4 max 9 freq -1088 +/- 5 delay 89 +/- 0 ptp4l[3680.277]: rms 5 max 8 freq -1092 +/- 5 delay 88 +/- 0 ptp4l[3681.277]: rms 3 max 5 freq -1089 +/- 4 delay 89 +/- 0 ptp4l[3682.277]: rms 5 max 8 freq -1084 +/- 6 delay 88 +/- 0 ptp4l[3683.278]: rms 4 max 7 freq -1088 +/- 6 delay 89 +/- 0 ptp4l[3684.278]: rms 5 max 7 freq -1086 +/- 7 delay 89 +/- 0 ptp4l[3685.278]: rms 3 max 8 freq -1087 +/- 5 delay 88 +/- 0 ptp4l[3686.279]: rms 4 max 8 freq -1088 +/- 5 delay 88 +/- 0 ptp4l[3687.279]: rms 4 max 8 freq -1088 +/- 5 delay 88 +/- 0
Results: It can be observed that the clocks on Slave devices are getting synchronised with the clock on Master device.
3.6.3.4.12. SRAM Requirement
The ICSSG Ethernet driver can be used in switch mode. Two icssg ports are used per switch.
SRAM Required for each switch (per two ports) is 256 KB.
For each ICSSG switch, the SRAM required needs to be contiguous.
PRUETH only uses the required amount of SRAM from the SRAM/MSMC pool. If PRUETH doesn’t get the required amount of SRAM, the prueth_probe() API will return with -ENOMEM error.