3.2.2.8. HSR Offload

Introduction

HSR (High-availability Seamless Redundancy) framework in Linux allows offloading following functionalities to the device hsr-fwd-offload: For forwarding HSR frames one port to another i.e port-to-port forwarding

hsr-dup-offload: Duplicate the outgoing HSR frame

The (Programmable Real-time Unit and Industrial Communication Subsystem) PRU-ICSS HSR firmware supports port-to-port forwarding, Tx packet duplication and this allows to offload these capabilities from HSR driver in software to the PRU subsystem.

To enable offloading using below commands To enable port-to-port offload

ethtool -K <interface> hsr-fwd-offload on

To enable Tx packet duplication

ethtool -K <interface> hsr-fwd-offload on
ethtool -K <interface> hsr-dup-offload on

Note

The ICSS HSR firmware always run with port-to-port forwarding. So whenever any of the HSR features are to be offloaded, the port-to-port forwarding must also be offloaded. It is not possible to offload only transmission (Tx) packet duplication functionality.

The below script sets up an HSR interface with the port-to-port forwarding and Tx packet duplication offloaded

#!/bin/sh

#For non offload - sh hsr_setup.sh hsr_sw <INTF_A> <INTF_B> <HSR_INTF_IP_ADDR>
#For offload - sh hsr_setup.sh hsr_hw <INTF_A> <INTF_B> <HSR_INTF_IP_ADDR>

if [ "$#" != "4" ]
then
        echo "$0 <hsr_sw/hsr_hw> <intf1> <intf2> <ip addr>"
        exit
fi

if [ "$1" != "hsr_sw" ] && [ "$1" != "hsr_hw" ]
then
        echo "$0 <hsr_sw|hsr_hw>"
        exit
fi

if=hsr0

ifa=$2
ifb=$3

ip=$4
mac=$(ifconfig "$ifa" | grep ether | cut -d " " -f 10)

echo "ip=$ip"
echo "if=$if"
echo "mac=$mac"
echo "slave-a=$ifa"
echo "slave-b=$ifb"

ip link set $if down
ip link delete $if  2> /dev/null

ip link set $ifa down
ip link set $ifb down
sleep 1

if [ "$1" = "hsr_hw" ]
then
        ethtool -k "$ifa" | grep hsr
        ethtool -K "$ifa" hsr-fwd-offload on
        ethtool -K "$ifa" hsr-dup-offload on
        ethtool -K "$ifa" hsr-tag-ins-offload on
        ethtool -K "$ifa" hsr-tag-rm-offload on
        ethtool -k "$ifa" | grep hsr

        ethtool -k "$ifb" | grep hsr
        ethtool -K "$ifb" hsr-fwd-offload on
        ethtool -K "$ifb" hsr-dup-offload on
        ethtool -K "$ifb" hsr-tag-ins-offload on
        ethtool -K "$ifb" hsr-tag-rm-offload on
        ethtool -k "$ifb" | grep hsr
fi

ip link set dev "$ifa" address "$mac"
ip link set dev "$ifb" address "$mac"

ip link add name $if type hsr slave1 "$ifa" slave2 "$ifb" supervision 45 version 1

sleep 3

ip addr add "$ip"/24 dev $if
ip link set $if up
ip link set $ifa up
ip link set $ifb up
sleep 1

To create HSR interface with IP address 192.168.2.20 using eth1 and eth2, run the script by passing the arguments as below

sh hsr_setup.sh hsr_hw eth1 eth2 192.168.2.20

Multicast Filtering

All multi-cast addresses not registered will be filtered out.

Multicast Add/Delete

Multicast MAC address can be added/deleted using ip maddr commands or Linux socket ioctl SIOCADDMULTI/SIOCDELMULTI.

Show multicast address

Show current list of multicast address for the HSR interface

ip maddr show dev <hsr_intf>

Example:

# ip maddr show dev hsr0
7:      hsr0
        link  33:33:00:00:00:01 users 3
        link  01:00:5e:00:00:01 users 3
        link  33:33:ff:1e:e8:10 users 3
        link  01:00:5e:00:00:fb users 3
        link  01:00:5e:00:00:fc users 3
        link  33:33:00:00:00:fb users 3
        link  33:33:00:01:00:03 users 3
        inet  224.0.0.252
        inet  224.0.0.251
        inet  224.0.0.1
        inet6 ff02::1:3
        inet6 ff02::fb
        inet6 ff02::1:ff1e:e810
        inet6 ff02::1
        inet6 ff01::1

Add multicast address

Add a multicast address

ip maddr add <multicast_mac_addr> dev <hsr_intf>

Example: To add a multicast address and display the list in HSR and slave ports

# ip maddr add 01:80:c4:00:00:0e dev hsr0
# ip maddr show dev hsr0
7:      hsr0
        link  33:33:00:00:00:01 users 3
        link  01:00:5e:00:00:01 users 3
        link  33:33:ff:1e:e8:10 users 3
        link  01:00:5e:00:00:fb users 3
        link  01:00:5e:00:00:fc users 3
        link  33:33:00:00:00:fb users 3
        link  33:33:00:01:00:03 users 3
        link  01:80:c4:00:00:0e users 3 static
        inet  224.0.0.252
        inet  224.0.0.251
        inet  224.0.0.1
        inet6 ff02::1:3
        inet6 ff02::fb
        inet6 ff02::1:ff1e:e810
        inet6 ff02::1
        inet6 ff01::1

# ip maddr show dev eth1
5:      eth1
        link  01:00:5e:00:00:01 users 2
        link  33:33:00:00:00:01 users 2
        link  33:33:ff:1e:e8:10 users 2
        link  01:80:c2:00:00:00
        link  01:80:c2:00:00:03
        link  01:80:c2:00:00:0e
        link  33:33:00:00:00:fb users 2
        link  33:33:00:01:00:03 users 2
        link  01:00:5e:00:00:fb
        link  01:00:5e:00:00:fc
        link  01:80:c4:00:00:0e
        inet  224.0.0.1
        inet6 ff02::1:3
        inet6 ff02::fb
        inet6 ff02::1:ff1e:e810
        inet6 ff02::1 users 2
        inet6 ff01::1

# ip maddr show dev eth2
6:      eth2
        link  01:00:5e:00:00:01 users 2
        link  33:33:00:00:00:01 users 2
        link  33:33:ff:1e:e8:10 users 2
        link  01:80:c2:00:00:00
        link  01:80:c2:00:00:03
        link  01:80:c2:00:00:0e
        link  01:00:5e:00:00:fb
        link  01:00:5e:00:00:fc
        link  33:33:00:00:00:fb users 2
        link  33:33:00:01:00:03 users 2
        link  01:80:c4:00:00:0e
        inet  224.0.0.1
        inet6 ff02::1:3
        inet6 ff02::fb
        inet6 ff02::1:ff1e:e810
        inet6 ff02::1 users 2
        inet6 ff01::1

Delete multicast address

Delete a multicast address

ip maddr del <multicast_mac_addr> dev <hsr_intf>

Example: To delete an added multicast address and dislay the list of HSR and slave intefaces.

# ip maddr del 01:80:c4:00:00:0e dev hsr0

# ip maddr show dev hsr0
7:      hsr0
        link  33:33:00:00:00:01 users 3
        link  01:00:5e:00:00:01 users 3
        link  33:33:ff:1e:e8:10 users 3
        link  01:00:5e:00:00:fb users 3
        link  01:00:5e:00:00:fc users 3
        link  33:33:00:00:00:fb users 3
        link  33:33:00:01:00:03 users 3
        inet  224.0.0.252
        inet  224.0.0.251
        inet  224.0.0.1
        inet6 ff02::1:3
        inet6 ff02::fb
        inet6 ff02::1:ff1e:e810
        inet6 ff02::1
        inet6 ff01::1

# ip maddr show dev eth1
5:      eth1
        link  01:00:5e:00:00:01 users 2
        link  33:33:00:00:00:01 users 2
        link  33:33:ff:1e:e8:10 users 2
        link  01:80:c2:00:00:00
        link  01:80:c2:00:00:03
        link  01:80:c2:00:00:0e
        link  33:33:00:00:00:fb users 2
        link  33:33:00:01:00:03 users 2
        link  01:00:5e:00:00:fb
        link  01:00:5e:00:00:fc
        inet  224.0.0.1
        inet6 ff02::1:3
        inet6 ff02::fb
        inet6 ff02::1:ff1e:e810
        inet6 ff02::1 users 2
        inet6 ff01::1

# ip maddr show dev eth2
6:      eth2
        link  01:00:5e:00:00:01 users 2
        link  33:33:00:00:00:01 users 2
        link  33:33:ff:1e:e8:10 users 2
        link  01:80:c2:00:00:00
        link  01:80:c2:00:00:03
        link  01:80:c2:00:00:0e
        link  01:00:5e:00:00:fb
        link  01:00:5e:00:00:fc
        link  33:33:00:00:00:fb users 2
        link  33:33:00:01:00:03 users 2
        inet  224.0.0.1
        inet6 ff02::1:3
        inet6 ff02::fb
        inet6 ff02::1:ff1e:e810
        inet6 ff02::1 users 2
        inet6 ff01::1

Multicast Filtering for VLAN Interfaces

Multicast filtering for VLAN interfaces is also supported.

Show current list of multicast address for the HSR VLAN interface

ip maddr show dev <hsr_vlan_intf>

Example:

# ip maddr show dev hsr0.5

Add multicast address for the HSR VLAN interface

ip maddr add <multicast_mac_addr> dev <hsr_vlan_intf>

Example:

# ip maddr add 01:80:c4:00:00:0e dev hsr0.5

Delete multicast address for the HSR VLAN interface

ip maddr del <multicast_mac_addr> dev <hsr_vlan_intf>

Example:

# ip maddr del 01:80:c4:00:00:0e dev hsr0.5

Performance

This section describes the throughput and CPU usage metrics in the offload case

Setup

A sample test setup is as show below

../../../../../_images/HSR_Offload_Setup_AM64x.png

Test Procedure

  1. Connect the LAN cables between the DANH as shown in the Section 1

  2. Execute the commands to setup and create HSR interface

    1. To setup HSR non-offload on Node A and Node C,

      sh hsr_setup.sh hsr_sw <INTF_A> <INTF_B> <HSR_INTF_IP_ADDR>
      
    2. To Setup HSR offload on Node B,

      sh hsr_setup.sh hsr_hw <INTF_A> <INTF_B> <HSR_INTF_IP_ADDR>
      
  3. Confirm ping across all Nodes

    1. Node A < - - > Node B

    2. Node B < - - > Node C

    3. Node C < - - > Node A

  4. Disconnect the LAN cable between Node A and Node C

  5. Monitor the CPU usage on Node B

    mpstat -P ALL 1
    
  6. Run iperf3 server on Node C

    iperf3 -s -i 1
    
  7. Run iperf3 client on Node A for 60 secs

    iperf3 -c -1 -t 60 <Node_C_IP_Addr>
    

CPU Usage on Node B

CPU usage at Node B found to be negligible

** Snippet from the continuous stats **
CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest   %idle
all    0.00    0.00    0.50    0.00    0.00    0.00    0.00    0.00   99.50
  0    0.00    0.00    1.00    0.00    0.00    0.00    0.00    0.00   99.00
  1    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00

CPU    %usr   %nice    %sys %iowait    %irq   %soft  %steal  %guest   %idle
all    0.50    0.00    0.00    0.00    0.00    0.00    0.00    0.00   99.50
  0    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00
  1    0.00    0.00    0.00    0.00    0.00    0.00    0.00    0.00  100.00

Througput at Node A

Table 3.1 Throughput performance

Sender

Receiver

505 Mbits/sec

504 Mbits/sec