3.2.2.12. PCIe Root Complex

Introduction

The PCI Express (PCIe) module is a multi-lane I/O interconnect providing low pin count, high reliability, and high-speed data transfer at rates of up to 8.0 Gbps per lane per direction. It is a 3rd Generation I/O Interconnect technology succeeding ISA and PCI bus that is designed to be used as a general-purpose serial I/O interconnect in multiple market segments, including desktop, mobile, server, storage and embedded communications.

Features of AM64

There is one instance of the PCIe subsystem. Following are some of the main features:

  • The instance can be configured to operate in Root Complex mode or End Point mode

  • One lane configuration, capable up to 5.0 Gbps/lane (Gen2)

  • Support for Legacy, MSI and MSI-X Interrupt

  • There can be 32 different address mappings in outbound address translation unit. The mappings can be from regions reserved for each PCIe instance.

    • For instance PCIE0, there are two regions in SoC Memory Map:

      • 128 MB region with address in lower 32 bits

      • 4 GB region with address above 32 bits

Capabilities of AM64 EVM

Following are some of the details for PCIE0 instance:

Instance

Supported lanes

Supported Connector

PCIE0

1 lane

Standard female connector

Hardware Setup Details

AM64x is, by default, intended to be operated in Root Complex mode.

Refer to the following image to toggle between Root Complex mode and End Point mode.

../../../../../_images/am64-pcie-rc-ep-sel.png

RC Software Architecture

Following is the software architecture for Root Complex mode:

../../../../../_images/Linux_PCIe_subsystem.png

Following is a brief explanation of layers shown in the diagram:

  • There are different drivers for the connected PCIe devices like pci_endpoint_test, tg-3, r8169, xhci-pci, ahci, etc. It could be vendor-specific like most of the ethernet cards (tg3, r8169) or class-specific like xhci-pci and ahci. Each of these drivers will also interact with it’s own domain-specific stack. For example, tg3 will interface with network stack, and xhci-pci will interface with USB stack.

  • The PCI core layer scans the PCIe bus to identify and detect any PCIe devices. It also binds the driver from the layer above, for the PCIe device, based on vendorid, deviceid and class.

  • The PCI BIOS layer handles resource management. For example, allocation of memory resources for BARs.

  • The bottom-most layer consists of the PCIe platform drivers like pcie-cadence, pcie-designware, etc. pci-j721e and pci-dra7xx are TI’s wrappers over these drivers. They configure platform-specific controllers and perform actual register writes.

RC Device Configuration

DTS Modification

The default dts for AM64x is configured to be used in root complex mode.

Linux Driver Configuration

The following config options have to be enabled in order to configure the PCI controller to be used in Root Complex mode.

CONFIG_SOCIONEXT_SYNQUACER_PREITS=y
CONFIG_PCI=y
CONFIG_PCI_MSI=y
CONFIG_PCI_J721E=y
CONFIG_PCIE_CADENCE=y
CONFIG_PCIE_CADENCE_HOST=y

Compliance Mode

In RC mode of operation, the Endpoint device can be forced to enter Compliance Mode for PCIe compliance testing by setting the “EC” bit in the LINK_CTRL_STATUS_2 register of the respective PCIe RC instance. Setting “EC” to 1 initiates a hot reset thereby forcing the Endpoint device into Compliance mode. The “EC” bit can be set from command-line by using devmem2 utility as follows:

devmem2 <address> w <value>

where <address> is the address of LINK_CTRL_STATUS_2 register and <value> is the resulting value to be written with “EC” bit of the register set.

64-Bit Address Space with 4 GB Size

The PCIe Controller support for 64-Bit addressing in the System’s Address Space with 4 GB Size is enabled in the device-tree. The 4 GB region is split as:

  1. 4 KB ECAM region for Configuration Accesses

  2. 1 MB IO region

  3. Remaining region (4 GB - 1 MB - 4 KB) as 32-bit Non-Prefetchable MEM

Testing Details

The RC should enumerate any off-the-shelf PCIe cards. It has been tested with Ethernet cards, NVMe cards, PCIe USB card, PCIe WiFi card, PCIe SATA card and also to AM64x in loopback mode.

In order to see if the connected card is detected, lspci utility should be used. Different utilities can be used depending on the cards.

Following are the outputs for some of them:

root@am64xx-evm:~# lspci
0000:00:00.0 PCI bridge: Texas Instruments Device b010
0000:01:00.0 Unassigned class [ff00]: Texas Instruments Device b010
  • WiFi card

    • lspci output

    root@am64xx-evm:~# lspci
    0000:00:00.0 PCI bridge: Texas Instruments Device b010
    0000:01:00.0 Network controller: Intel Corporation Wireless 3160 (rev 6b)
    
    • Test using ping

    root@am64xx-evm:~# ping 192.168.10.1 -w 10|
    PING 192.168.10.1 (192.168.10.1): 56 data bytes
    64 bytes from 192.168.10.1: seq=0 ttl=64 time=176.985 ms
    64 bytes from 192.168.10.1: seq=1 ttl=64 time=49.840 ms
    64 bytes from 192.168.10.1: seq=2 ttl=64 time=32.125 ms
    64 bytes from 192.168.10.1: seq=3 ttl=64 time=4.652 ms
    64 bytes from 192.168.10.1: seq=4 ttl=64 time=70.805 ms
    64 bytes from 192.168.10.1: seq=6 ttl=64 time=195.564 ms
    64 bytes from 192.168.10.1: seq=7 ttl=64 time=9.321 ms
    64 bytes from 192.168.10.1: seq=8 ttl=64 time=5.784 ms
    64 bytes from 192.168.10.1: seq=9 ttl=64 time=18.015 ms
    
  • NVMe SSD

    • lspci output

    root@am64xx-evm:~# lspci -vv
    00:00.0 PCI bridge: Texas Instruments Device b010 (prog-if 00 [Normal decode])
        Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx+
        Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
        Latency: 0
        Interrupt: pin A routed to IRQ 44
        Region 0: Memory at <unassigned> (64-bit, prefetchable)
        Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
        I/O behind bridge: [disabled]
        Memory behind bridge: 68100000-681fffff [size=1M]
        Prefetchable memory behind bridge: [disabled]
        Secondary status: 66MHz- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- <SERR- <PERR-
        BridgeCtl: Parity- SERR+ NoISA- VGA- VGA16- MAbort- >Reset- FastB2B-
                PriDiscTmr- SecDiscTmr- DiscTmrStat- DiscTmrSERREn-
        Capabilities: [80] Power Management version 3
                Flags: PMEClk- DSI- D1+ D2- AuxCurrent=0mA PME(D0+,D1+,D2-,D3hot+,D3cold-)
                Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
        Capabilities: [90] MSI: Enable+ Count=1/1 Maskable+ 64bit+
                Address: 0000000001000000  Data: 0000
                Masking: 00000000  Pending: 00000000
        Capabilities: [b0] MSI-X: Enable- Count=1 Masked-
                Vector table: BAR=0 offset=00000000
                PBA: BAR=0 offset=00000008
        Capabilities: [c0] Express (v2) Root Port (Slot+), MSI 00
                DevCap: MaxPayload 128 bytes, PhantFunc 0
                        ExtTag- RBE+
                DevCtl: CorrErr- NonFatalErr- FatalErr- UnsupReq-
                        RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
                        MaxPayload 128 bytes, MaxReadReq 512 bytes
                DevSta: CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
                LnkCap: Port #0, Speed 5GT/s, Width x1, ASPM L1, Exit Latency L1 <8us
                        ClockPM- Surprise- LLActRep- BwNot+ ASPMOptComp+
                LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- CommClk-
                        ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                LnkSta: Speed 5GT/s (ok), Width x1 (ok)
                        TrErr- Train- SlotClk- DLActive- BWMgmt- ABWMgmt+
                SltCap: AttnBtn- PwrCtrl- MRL- AttnInd- PwrInd- HotPlug- Surprise-
                        Slot #0, PowerLimit 0.000W; Interlock- NoCompl-
                SltCtl: Enable: AttnBtn- PwrFlt- MRL- PresDet- CmdCplt- HPIrq- LinkChg-
                        Control: AttnInd Off, PwrInd Off, Power+ Interlock-
                SltSta: Status: AttnBtn- PowerFlt- MRL+ CmdCplt- PresDet- Interlock-
                        Changed: MRL- PresDet- LinkState-
                RootCap: CRSVisible-
                RootCtl: ErrCorrectable- ErrNon-Fatal- ErrFatal- PMEIntEna+ CRSVisible-
                RootSta: PME ReqID 0000, PMEStatus- PMEPending-
                DevCap2: Completion Timeout: Range B, TimeoutDis+, NROPrPrP-, LTR+
                         10BitTagComp-, 10BitTagReq-, OBFF Via message, ExtFmt+, EETLPPrefix+, MaxEETLPPrefixes 1
                         EmergencyPowerReduction Not Supported, EmergencyPowerReductionInit-
                         FRS-, LN System CLS Not Supported, TPHComp-, ExtTPHComp-, ARIFwd-
                         AtomicOpsCap: Routing- 32bit- 64bit- 128bitCAS-
                DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR+, OBFF Disabled ARIFwd-
                         AtomicOpsCtl: ReqEn- EgressBlck-
                LnkCtl2: Target Link Speed: 5GT/s, EnterCompliance- SpeedDis-
                         Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                         Compliance De-emphasis: -6dB
                LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete-, EqualizationPhase1-
                         EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
        Capabilities: [100 v2] Advanced Error Reporting
                UESta:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
                CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
                AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                        MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
                HeaderLog: 00000000 00000000 00000000 00000000
                RootCmd: CERptEn- NFERptEn- FERptEn-
                RootSta: CERcvd- MultCERcvd- UERcvd- MultUERcvd-
                         FirstFatal- NonFatalMsg- FatalMsg- IntMsg 0
                ErrorSrc: ERR_COR: 0000 ERR_FATAL/NONFATAL: 0000
        Capabilities: [150 v1] Device Serial Number 00-00-00-00-00-00-00-00
        Capabilities: [300 v1] Secondary PCI Express
                LnkCtl3: LnkEquIntrruptEn-, PerformEqu-
                LaneErrStat: 0
        Capabilities: [4c0 v1] Virtual Channel
                Caps:   LPEVC=0 RefClk=100ns PATEntryBits=1
                Arb:    Fixed- WRR32- WRR64- WRR128-
                Ctrl:   ArbSelect=Fixed
                Status: InProgress-
                VC0:    Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                        Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                        Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                        Status: NegoPending- InProgress-
                VC1:    Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                        Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                        Ctrl:   Enable- ID=1 ArbSelect=Fixed TC/VC=00
                        Status: NegoPending- InProgress-
                VC2:    Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                        Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                        Ctrl:   Enable- ID=2 ArbSelect=Fixed TC/VC=00
                        Status: NegoPending- InProgress-
                VC3:    Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                        Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                        Ctrl:   Enable- ID=3 ArbSelect=Fixed TC/VC=00
                        Status: NegoPending- InProgress-
        Capabilities: [900 v1] L1 PM Substates
                L1SubCap: PCI-PM_L1.2+ PCI-PM_L1.1+ ASPM_L1.2+ ASPM_L1.1+ L1_PM_Substates+
                          PortCommonModeRestoreTime=255us PortTPowerOnTime=26us
                L1SubCtl1: PCI-PM_L1.2- PCI-PM_L1.1- ASPM_L1.2- ASPM_L1.1-
                           T_CommonMode=0us LTR1.2_Threshold=0ns
                L1SubCtl2: T_PwrOn=10us
        Capabilities: [a20 v1] Precision Time Measurement
                PTMCap: Requester:- Responder:+ Root:+
                PTMClockGranularity: 4ns
                PTMControl: Enabled:- RootSelected:-
                PTMEffectiveGranularity: Unknown
        Kernel driver in use: pcieport
        Kernel modules: pci_endpoint_test
    
    01:00.0 Non-Volatile memory controller: Intel Corporation Optane SSD 900P Series (prog-if 02 [NVM Express])
            Subsystem: Intel Corporation 900P Series [Add-in Card]
            Control: I/O- Mem+ BusMaster+ SpecCycle- MemWINV- VGASnoop- ParErr- Stepping- SERR- FastB2B- DisINTx+
            Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
            Latency: 0
            Interrupt: pin A routed to IRQ 43
            Region 0: Memory at 68110000 (64-bit, non-prefetchable) [size=16K]
            Expansion ROM at 68100000 [virtual] [disabled] [size=64K]
            Capabilities: [40] Power Management version 3
                    Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
                    Status: D0 NoSoftRst+ PME-Enable- DSel=0 DScale=0 PME-
            Capabilities: [50] MSI-X: Enable+ Count=32 Masked-
                    Vector table: BAR=0 offset=00002000
                    PBA: BAR=0 offset=00003000
            Capabilities: [60] Express (v2) Endpoint, MSI 00
                    DevCap: MaxPayload 256 bytes, PhantFunc 0, Latency L0s <4us, L1 <4us
                            ExtTag+ AttnBtn- AttnInd- PwrInd- RBE+ FLReset+ SlotPowerLimit 0.000W
                    DevCtl: CorrErr- NonFatalErr- FatalErr- UnsupReq-
                            RlxdOrd+ ExtTag+ PhantFunc- AuxPwr- NoSnoop+ FLReset-
                            MaxPayload 128 bytes, MaxReadReq 512 bytes
                    DevSta: CorrErr- NonFatalErr- FatalErr- UnsupReq- AuxPwr- TransPend-
                    LnkCap: Port #0, Speed 8GT/s, Width x4, ASPM L0s, Exit Latency L0s <4us
                            ClockPM- Surprise- LLActRep- BwNot- ASPMOptComp+
                    LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- CommClk-
                            ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
                    LnkSta: Speed 5GT/s (downgraded), Width x1 (downgraded)
                            TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
                    DevCap2: Completion Timeout: Range ABCD, TimeoutDis+, NROPrPrP-, LTR-
                             10BitTagComp-, 10BitTagReq-, OBFF Not Supported, ExtFmt-, EETLPPrefix-
                             EmergencyPowerReduction Not Supported, EmergencyPowerReductionInit-
                             FRS-, TPHComp-, ExtTPHComp-
                             AtomicOpsCap: 32bit- 64bit- 128bitCAS-
                    DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled
                             AtomicOpsCtl: ReqEn-
                    LnkCtl2: Target Link Speed: 8GT/s, EnterCompliance- SpeedDis-
                             Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
                             Compliance De-emphasis: -6dB
                    LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete-, EqualizationPhase1-
                             EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
            Capabilities: [100 v1] Advanced Error Reporting
                    UESta:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UEMsk:  DLP- SDES- TLP- FCP- CmpltTO- CmpltAbrt- UnxCmplt- RxOF- MalfTLP- ECRC- UnsupReq- ACSViol-
                    UESvrt: DLP+ SDES+ TLP- FCP+ CmpltTO- CmpltAbrt- UnxCmplt- RxOF+ MalfTLP+ ECRC- UnsupReq- ACSViol-
                    CESta:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr-
                    CEMsk:  RxErr- BadTLP- BadDLLP- Rollover- Timeout- AdvNonFatalErr+
                    AERCap: First Error Pointer: 00, ECRCGenCap+ ECRCGenEn- ECRCChkCap+ ECRCChkEn-
                            MultHdrRecCap- MultHdrRecEn- TLPPfxPres- HdrLogCap-
                    HeaderLog: 00000000 00000000 00000000 00000000
            Capabilities: [150 v1] Virtual Channel
                    Caps:   LPEVC=0 RefClk=100ns PATEntryBits=1
                    Arb:    Fixed- WRR32- WRR64- WRR128-
                    Ctrl:   ArbSelect=Fixed
                    Status: InProgress-
                    VC0:    Caps:   PATOffset=00 MaxTimeSlots=1 RejSnoopTrans-
                            Arb:    Fixed- WRR32- WRR64- WRR128- TWRR128- WRR256-
                            Ctrl:   Enable+ ID=0 ArbSelect=Fixed TC/VC=ff
                            Status: NegoPending- InProgress-
            Capabilities: [180 v1] Power Budgeting <?>
            Capabilities: [190 v1] Alternative Routing-ID Interpretation (ARI)
                    ARICap: MFVC- ACS-, Next Function: 0
                    ARICtl: MFVC- ACS-, Function Group: 0
            Capabilities: [270 v1] Device Serial Number 55-cd-2e-41-4e-31-12-50
            Capabilities: [2a0 v1] Secondary PCI Express
                    LnkCtl3: LnkEquIntrruptEn-, PerformEqu-
                    LaneErrStat: 0
            Kernel driver in use: nvme
            Kernel modules: nvme
    
    • Test using hdparm

    root@am64xx-evm:~# hdparm -tT /dev/nvme0n1
    
    /dev/nvme0n1:
    Timing cached reads: 1062 MB in  2.00 seconds = 530.42 MB/sec
    Timing buffered disk reads: 812 MB in  3.01 seconds = 270.03 MB/sec
    
    • Test using dd

    root@am64xx-evm:~# time dd if=/dev/urandom of=/home/root/srctest_file_pci_2199 bs=1M count=10
    10+0 records in
    10+0 records out
    real        0m 0.22s
    user        0m 0.00s
    sys     0m 0.20s