2.1. Release Notes
2.1.1. Overview
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM64x installer provides everything needed as discussed below to create the embedded system from “scratch” :
Platform/board-support software and configuration files for Linux
U-Boot and Kernel sources and configuration files
An ARM cross-compiling toolchain as well as other host binaries and components
A Yocto/OE compliant filesystem and sources for example applications
A variety of scripts and Makefiles to automate certain tasks
Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
Reference Examples, benchmarks
This release supports SR2.0 High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide
2.1.2. Licensing
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
Linux Manifest:
<PSDK_PATH>/manifest/software_manifest.htm
2.1.3. Release 11.00.09.04
Released on April 2025
2.1.3.1. What’s new
Processor SDK Linux AM64X Release has following new features:
First 2025 LTS Reference Release Including RT combined branch model - Important Bug Fixes on top of Processor SDK 10.01.10.04 Release - Review Issue Tracker Section for the new fixes.
Key Release References:
RT Kernel : Real-Time Linux Interrupt Latency numbers here - RT Interrupt Latencies
Snagfactory Support - Snagfactory Tool
Component version:
Kernel 6.12.17
U-Boot 2025.01
Toolchain GCC 13.3
ATF 2.12+
OPTEE 4.5.0
TIFS Firmware v11.00.07 (Click on the link for more information)
Yocto scarthgap 5.0
2.1.4. Build Information
2.1.4.1. U-Boot
u-boot
2.1.4.2. TF-A
2.1.4.3. OP-TEE
2.1.4.4. ti-linux-firmware
2.1.4.5. Kernel
Linux Kernel
2.1.4.6. Yocto
meta-ti
meta-arago
meta-tisdk
2.1.5. Issues Tracker
Note
Release Specific Issues including details will be published through Software Incident Report (SIR) portal
Further Information can be found at SIR Portal <https://sir.ext.ti.com/>
2.1.5.1. Errata Resolved
Record ID |
Title |
---|---|
EXT_EP-12122 |
USB2 PHY locks up due to short suspend |
EXT_EP-12123 |
USART: Erroneous clear/trigger of timeout interrupt |
2.1.5.2. Issues Resolved
Record ID |
Title |
---|---|
EXT_EP-12315 |
eMMC High Speed SDR mode is not configured correctly in the U-Boot |
EXT_EP-12311 |
AM64x: Software Build Sheet needs update at SOC level SW readiness |
EXT_EP-12111 |
Linux SDK v10.0: TI-added support for W25N01JW SPI NAND breaks other existing Flash support |
EXT_EP-12051 |
AM64x: Linux hangs on repetitive probe/removal of gadget zero |
EXT_EP-12071 |
sdk-doc: missing SK-AM64B information in CDNS3 USB page |
EXT_EP-12337 |
ICSSG: TAPRIO - Firmware can’t handle base-time which is not a multiple of cycle-time. |
EXT_EP-12338 |
ICSSG: PA_STATS are not sequenced properly |
EXT_EP-12339 |
Switch/MAC/HSR firmware does not drop corrupted packets |
2.1.5.3. Issues Open
Record ID |
Title |
---|---|
EXT_EP-12310 |
Resource Table generating wrong format for rm-cfg.yaml |
EXT_EP-12285 |
SK-AM64B: Deferred probe of i2c bus warning |
EXT_EP-12300 |
ICSSG: Ethernet: Promiscuous mode is always enabled in bridge mode |
EXT_EP-12075 |
U-boot gets stuck when DDR size changed to 512 MB |
EXT_EP-12060 |
AM64x: Lower core count on variant devices no supported |
EXT_EP-12336 |
Last 1B of payload missing in forwarding scenario |