3.1.1.5. SD, eMMC and USB
The following guide shows how to flash and boot from storage media like the embedded multimedia card (eMMC), secure digital (SD) card, and USB storage devices. While this is a step-by-step guide, it is in no way extensive and does not cover all the per-platform corner-cases. For any issues/questions on this guide, please reach out to: Help e2e.
3.1.1.5.1. MMC
3.1.1.5.1.1. Listing MMC devices
Usually in all the platforms there will be two MMC instances of which one would be SD and the other would be eMMC. The index of them can vary from one class of platforms to the other. For a given platform, the device number: mmcdev=[0:1] can be found in the following way:
=> mmc list
sdhci@fa10000: 0 (eMMC)
sdhci@fa00000: 1 (SD)
The device number “0” for eMMC will be needed when flashing to the eMMC device in: Flash and boot SPL from eMMC.
3.1.1.5.1.2. Selecting MMC device and paritions
To selct an MMC device in u-boot, the command: mmc dev could be used. The general syntax is:
=> mmc dev [dev] [partition]
The following lists examples and their explanation for each MMC device and partitions according to the example in: Listing MMC devices.
=> mmc dev 0 0 # select eMMC user HW partition (UDA)
=> mmc dev 0 1 # select eMMC boot0 HW partition
=> mmc dev 0 2 # select eMMC boot1 HW partition
=> mmc dev 1 1 # select SD "boot" partition
=> mmc dev 1 2 # select SD "root" partition
3.1.1.5.1.3. View MMC partition contents
This section assumes an SD card or eMMC was prepared previously to boot the device.
Note
For eMMC, typically, the device ships without a partition table If there is a need to create a partition in UDA (to flash the rootfs), please go to: Create software partitions in eMMC UDA and format the partition: Formatting eMMC partitions from Linux before proceeding to look at the eMMC partition contents.
To verify partitions in any MMC device from u-boot prompt, use the command: mmc part.
=> mmc dev 0
switch to partitions #0, OK
mmc0(part 0) is current device
=> mmc part
Partition Map for MMC device 0 -- Partition Type: DOS
Part Start Sector Num Sectors UUID Type
1 2048 31078400 8ece5cfe-01 83
If the partitions are formatted with a file system type that is supported by u-boot, you can view the contents of the MMC partition as show below:
=> ls mmc 0:1
<DIR> 4096 .
<DIR> 4096 ..
<SYM> 7 bin
<DIR> 4096 boot
<DIR> 4096 dev
<DIR> 4096 etc
<DIR> 4096 home
<SYM> 7 lib
<DIR> 4096 media
<DIR> 4096 mnt
<DIR> 4096 opt
<DIR> 4096 proc
<DIR> 4096 root
<DIR> 4096 run
<SYM> 8 sbin
<DIR> 4096 srv
<DIR> 4096 sys
<DIR> 4096 tmp
<DIR> 4096 usr
<DIR> 4096 var
=> ls mmc 0:1 boot/dtb/ti
<DIR> 4096 .
<DIR> 4096 ..
60319 k3-am625-sk.dtb
Where the general syntax is:
$ ls <interface> [<dev[:partition]> [directory]]
3.1.1.5.1.4. Flash and boot SPL from eMMC
The K3 based processors supports and recommends booting from the eMMC boot0/1 HW partitions. In the following example, we use the fatload and mmc write commands to load binaries from an SD card and write them to the eMMC boot0 HW partition:
=> mmc dev 0 1
=> fatload mmc 1 ${loadaddr} tiboot3.bin
=> mmc write ${loadaddr} 0x0 0x800
=> fatload mmc 1 ${loadaddr} tispl.bin
=> mmc write ${loadaddr} 0x800 0x1000
=> fatload mmc 1 ${loadaddr} u-boot.img
=> mmc write ${loadaddr} 0x1800 0x2000
3.1.1.5.1.4.1. eMMC layout
+----------------------------------+0x0 +-------------------------+0x0
| tiboot3.bin (1 MB) | | |
+----------------------------------+0x800 | |
| tispl.bin (2 MB) | | |
+----------------------------------+0x1800 | rootfs |
| u-boot.img (4 MB) | | |
+----------------------------------+0x3800 | |
| environment (128 KB) | | |
+----------------------------------+0x3900 | |
| backup environment (128 KB) | | |
+----------------------------------+0x3A00 +-------------------------+
boot0 HW partition (8 MB) user partition
3.1.1.5.1.4.2. eMMC boot configuration
To boot from any eMMC, the master (ROM) will require some configuration which can be set using the mmc bootbus and mmc partconf commands.
The mmc bootbus command sets the BOOT_BUS_WIDTH field where mmc bootbus 0 2 0 0 selects x8 (sdr/ddr) buswidth in boot operation mode.
The mmc partconf command can be used to configure what hardware partition to boot from. The general syntax is:
$ mmc partconf <dev> [[varname] | [<boot_ack> <boot_partition> <partition_access>]]
For more information on these commands, please refer to: MMC CMD.
Boot from boot0 HW partition of eMMC:
=> mmc partconf 0 1 1 1
=> mmc bootbus 0 2 0 0
Boot from boot1 HW hardware partition of eMMC:
=> mmc partconf 0 1 2 1
=> mmc bootbus 0 2 0 0
Note
When booting from boot1 HW partition, make sure to flash the partition using:
mmc dev 0 2.
Boot from UDA HW partition of eMMC:
=> mmc partconf 0 1 7 1
=> mmc bootbus 0 2 0 0
Enable warm reset
On eMMC devices, warm reset will not work if EXT_CSD[162] bit is unset since the reset input signal will be ignored. Warm reset is required to be enabled in order for the eMMC to be in a “clean state” on power-on reset so that ROM can do a clean enumeration. To set the EXT_CSD[162] bit, stop at u-boot prompt and execute the following command:
=> mmc rst-function 0 1
Warning
This is a write-once field. For more information, please refer to the u-boot doc: MMC CMD.
3.1.1.5.1.5. Boot Linux from eMMC
To flash & boot the rootfs from eMMC UDA HW partition, first prepare UDA: Create software partitions in eMMC UDA. The new software partition then needs to be formatted as a ext4 filesystem: Formatting eMMC partitions from Linux, and then the rootfs has to be written. It is not possible to format a partition to ext4 in U-Boot. The Linux kernel image and DT are expected to be present in the /boot folder of rootfs.
To boot Linux from eMMC, use the following commands after flashing rootfs to UDA:
=> setenv mmcdev 0
=> setenv bootpart 0
=> boot
3.1.1.5.1.6. Flashing an MMC device using USB-DFU
To flash the eMMC device (boot0 HW partition) using USB-DFU, the device should be booted to u-boot prompt and a USB cable connected from the host machine to the device USB port configured to USB peripheral mode.
From u-boot prompt execute the following:
=> setenv dfu_alt_info ${dfu_alt_info_emmc}
=> dfu 0 mmc 0
and on the host machine have the bootloader binaries ready to flash to eMMC boot0 HW partition. Execute the dfu-util to transfer files to the device. The general syntax for dfu-util command is:
$ sudo dfu-util -R -a <dfu-target> -D <binary>
To see what are the dfu-targets, on the host machine run: sudo dfu-util -l
$ sudo dfu-util -l
dfu-util 0.9
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=6, name="sysfw.itb.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=5, name="u-env.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=4, name="u-boot.img.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=3, name="tispl.bin.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=2, name="tiboot3.bin.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=1, name="rootfs", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=0, name="rawemmc", serial="0000000000000591"
Then transfer each desired binary from the host to the device:
Host:
$ sudo dfu-util -R -a tiboot3.bin.raw -D tiboot3.bin
Device:
##DOWNLOAD ... OK Ctrl+C to exit ...
3.1.1.5.1.7. Flashing an SD card from a host PC
This section assumes that you have flashed an SD card using the script “create-sdcard.sh” packaged in the installer or have made a compatible layout manually. In this case, you will need to copy the boot images:
tiboot3.bintispl.binu-boot.img
to the SD card boot partition. At this point, the device can boot to u-boot prompt.
3.1.1.5.2. USB
3.1.1.5.2.1. Configuring USB in Host Mode
Note
USB instance in AM64 SoC is brought out using a USB 2.0 micro-AB port on the GP EVM. This port can be used in both host and device modes. By default in U-Boot, peripheral mode is supported. For accessing USB storage devices in U-Boot, dr_mode should be set to host in the U-Boot dts. The following diff shows the required changes to be done. On Starter Kit, USB instance in AM64 SoC is brought out using a USB 3.0 Type A port, so the mode is set to host by default and the following diff would not be required.
diff --git a/arch/arm/dts/k3-am642-evm-u-boot.dtsi b/arch/arm/dts/k3-am642-evm-u-boot.dtsi
index d066973f89f1..ff8afee09402 100644
--- a/arch/arm/dts/k3-am642-evm-u-boot.dtsi
+++ b/arch/arm/dts/k3-am642-evm-u-boot.dtsi
@@ -55,7 +55,7 @@
};
&usb0 {
- dr_mode="peripheral";
+ dr_mode="host";
u-boot,dm-spl;
};
3.1.1.5. Loading images from USB storage
For loading images from a FAT partition on a different media than mmc, replace the mmc command with the required media. For example, to load images from a FAT partition on a USB storage device connected to the zeroth instance of USB:
=> fatload usb 0 ${loadaddr} <file name>
3.1.1.5.2.2. Flash and boot SPL from USB storage
Booting to U-Boot prompt from USB storage is supported. The following are the steps to be followed:
Build the bootloader images using default “am64x_evm_r5_defconfig” and “am64x_evm_a53_defconfig” configs files. For instructions to build the bootloader images please refer to Build U-Boot.
Create a FAT32 partition with boot flag enabled on the USB storage device.
Copy the bootloader images(tiboot3.bin, tispl.bin, u-boot.img) into the above created partition.
Set the boot mode switches to usb host mode (For boot switch details refer to the Initialization/Boot Mode Pins chapter of TRM.)
Connect the USB Mass storage device with the bootloader images and boot up the board.
The board should now boot to u-boot prompt.
Note
While using usb reset or usb start commands in U-Boot, or
booting from a USB Mass storage device, some of the USB devices fail to get
detected. This issue is seen because these USB devices are failing to follow the
spec for power good delay. It can be resolved by overriding the power good delay
using the environment variable usb_pgood_delay, setting it to 2000 should be
good enough for all cases.
3.1.1.5.2.3. Boot Linux from USB storage
To load the Linux kernel, Device Tree and the Root file system from USB Mass storage device, the following changes are required to be done:
U-Boot
In U-Boot the USB controller can be used in either host or peripheral mode. For booting to linux kernel from USB storage device, the USB port is to be set as host.
By default, the USB controller is set in peripheral mode.
If the boot media used to boot to U-Boot is USB Host mode(Flash and boot SPL from USB storage) then, the USB controller is set to host mode during runtime. Therefore, no changes would be required in this case.
If a boot media other than USB Host is used, the USB controller needs to be set host mode and custom bootloader images are required to be built. Please refer to note in section Configuring USB in Host Mode
Linux
In Linux, by default the USB subsystem is built as modules. For booting from USB mass storage device, USB subsytem is required to be built into the image. This can be done by making the following changes in the configuration used for building kernel:
CONFIG_USB=y CONFIG_USB_XHCI_HCD=y CONFIG_USB_XHCI_PLATFORM=y CONFIG_USB_STORAGE=y CONFIG_USB_GADGET=y CONFIG_USB_CDNS3=y CONFIG_USB_CDNS3_GADGET=y CONFIG_USB_CDNS3_HOST=y CONFIG_USB_CDNS3_TI=y
Copying the images to USB storage device
After making the required changes mentioned above, build the kernel, device tree file and modules. The USB Mass storage device should have two partitions:
- boot
For creating this parition please refer Flash and boot SPL from USB storage
- rootfs
- A partition with ext4 filesystem and the following images in /boot/ directory
Linux kernel Image
Device tree (dtb) file
Run usbboot
During boot, cancel the autoboot at U-Boot and run the following command at u-boot prompt:
=> run usbboot
3.1.1.5.2.4. Steps for working around SD card issues in u-boot
In some cases, issues can be seen while using some SD cards, like:
Error while trying to initialize:
U-Boot SPL 2021.01-g74fc69c889 (May 19 2022 - 02:44:29 +0000) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.3.2--v08.03.02 (Jolly Jellyfi') Trying to boot from MMC2 spl: mmc init failed with error: -110 SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###
Given below are the list of various workarounds that can be done in the device tree MMC node to get SD card working. The workarounds are ordered in increasing order of reducing performance.
Note
All the mentioned below, are to be done in the MMC device tree node corresponding to the SD instance. This is usually the first (index starting from zero) instance.
Restricting to a given speed mode
By default the U-Boot driver tries to enumerate a SD card in the highest supported speed mode. Given below is the order in which the driver tries to enumerate a SD card:
SDR104
SDR50
DDR50
SD HS
SD legacy
The sdhci-caps-mask can be added to the DT node to cap at a specific mode:
Limit to DDR50:
sdhci-caps-mask = <0x00000003 0x00000000>Limit to SD HS:
sdhci-caps-mask = <0x00000007 0x00000000>Limit to SD legacy:
sdhci-caps-mask = <0x00000007 0x00200000>
&sdhci1 { /* SD/MMC */ vmmc-supply = <&vdd_mmc1>; vqmmc-supply = <&vdd_sd_dv>; pinctrl-names = "default"; pinctrl-0 = <&main_mmc1_pins_default>; ti,driver-strength-ohm = <50>; disable-wp; sdhci-caps-mask = <0x00000003 0x00000000>; /* Limiting to DDR50 speed mode */ };
Increase power cycle period
Increasing the delay while power cycling the SD card. This can be done by increasing the delay value in the diff indicated below,
diff --git a/drivers/mmc/mmc.c b/drivers/mmc/mmc.c index f486e2a2c364..38cc956b3d53 100644 --- a/drivers/mmc/mmc.c +++ b/drivers/mmc/mmc.c @@ -2761,7 +2761,7 @@ static int mmc_power_cycle(struct mmc *mmc) * SD spec recommends at least 1ms of delay. Let's wait for 2ms * to be on the safer side. */ - udelay(2000); + udelay(4000); return mmc_power_on(mmc); }
Reduce the bus width
The SD interface supports a bus width of 4. It can be reduced to 1 by changing the bus-width device tree property from 4 to 1.
diff --git a/arch/arm/dts/k3-am62-main.dtsi b/arch/arm/dts/k3-am62-main.dtsi index c06ec7355035..4ab29b6aa4b7 100644 --- a/arch/arm/dts/k3-am62-main.dtsi +++ b/arch/arm/dts/k3-am62-main.dtsi @@ -373,7 +373,7 @@ ti,itap-del-sel-sdr12 = <0x0>; ti,itap-del-sel-sdr25 = <0x0>; ti,clkbuf-sel = <0x7>; - bus-width = <4>; + bus-width = <1>; }; sdhci2: mmc@fa20000 {