2.1. Release Notes
2.1.1. Overview
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM64x installer provides everything needed as discussed below to create the embedded system from “scratch” :
Platform/board-support software and configuration files for Linux
U-Boot and Kernel sources and configuration files
An ARM cross-compiling toolchain as well as other host binaries and components
A Yocto/OE compliant filesystem and sources for example applications
A variety of scripts and Makefiles to automate certain tasks
Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
Reference Examples, benchmarks
This release supports SR2.0 High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide
2.1.2. Licensing
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
Linux Manifest:
<PSDK_PATH>/docs/software_manifest.html
2.1.3. Release 10.01.10.04
Released on December 2024
2.1.3.1. What’s new
Processor SDK Linux AM64X Release has following new features:
LTS Stable Kernel update to 6.6.58
Important Bug Fixes on top of Processor SDK 10.00.07.04 Release
RT Kernel : Real-Time Linux Interrupt Latency numbers here - RT Interrupt Latencies
Snagfactory Support - Snagfactory Tool
Component version:
Kernel 6.6.58
RT Kernel 6.6.58-rt45
U-Boot 2024.04
Toolchain GCC 13.3
ATF 2.11+
OPTEE 4.4.0
TIFS Firmware v10.01.08
DM Firmware 10.01.00.10
Yocto scarthgap 5.0
2.1.4. Build Information
2.1.4.1. U-Boot
u-boot
2.1.4.2. TF-A
2.1.4.3. OP-TEE
2.1.4.4. ti-linux-firmware
2.1.4.5. Kernel
Linux Kernel
Real Time (RT) Linux Kernel
2.1.4.6. Yocto
meta-ti
meta-arago
meta-tisdk
2.1.5. Issues Tracker
Note
Release Specific Issues including details will be published through Software Incident Report (SIR) portal
Further Information can be found at SIR Portal <https://sir.ext.ti.com/>
2.1.5.1. Errata Resolved
Record ID |
Title |
---|---|
EXT_EP-12122 |
USB2 PHY locks up due to short suspend |
EXT_EP-12123 |
USART: Erroneous clear/trigger of timeout interrupt |
2.1.5.2. Issues Resolved
Record ID |
Title |
---|---|
EXT_EP-12108 |
audit for potential bugs with 6.6.44 stable merge |
EXT_EP-12050 |
AM642-EVM: PCIe0 EP node is not defined |
EXT_EP-12098 |
Uboot docs: document renaming tiboot3-<evm>.bin file |
EXT_SITMPUSW-29 |
TI Debian SDK: Docker not working |
EXT_SITMPUSW-31 |
IPC Firmwares missing from base images. |
EXT_EP-12055 |
ICSSG HSR offload Multicast packets with VLAN IDs not filter classified |
EXT_EP-12054 |
ICSSG interfaces in switch mode running linuxptp not functional |
EXT_EP-12095 |
Watchdog reset not functional: ESM interrupts are wrong |
EXT_EP-12082 |
AM64 Processor SDK UG: Invalid eMMC Programming Steps in U-Boot Section |
EXT_EP-12068 |
AM64x dts file calls SYNC2_OUT the wrong name |
EXT_EP-12110 |
am64xx-evm : OSPI NOR boot fails |
EXT_EP-12049 |
AM64X EVM: Fastboot is not functional |
EXT_EP-12104 |
AM64x NAND dtso file missing in kernel 6.6 |
SYSFW-6426 |
Ownership of a firewall region can be transferred to an invalid host |
SYSFW-6432 |
Set device API doesn’t return Error when PD is in transition state |
EXT_SITMPUSW-32 |
SDK Makefile: Fix logic to pick key directory for mkimage |
2.1.5.3. Issues Open
Record ID |
Title |
---|---|
EXT_EP-12111 |
Linux SDK v10.0: TI-added support for W25N01JW SPI NAND breaks other existing Flash support |
EXT_EP-12075 |
U-boot gets stuck when DDR size changed to 512 MB |
EXT_EP-12051 |
AM64x: Linux hangs on repetitive probe/removal of gadget zero |
EXT_EP-12066 |
CPSW EST schedule triggers netdev watchdog |
EXT_EP-12065 |
CPSW Ethernet EST schedule is not taken down on link down |
EXT_EP-12071 |
sdk-doc: missing SK-AM64B information in CDNS3 USB page |
EXT_EP-12060 |
AM64x: Lower core count on variant devices no supported |
SYSFW-4518 |
Security handover does not enable use of all SA2UL threads |
SYSFW-6621 |
No available region to configure for Firewall ID 24 |
SYSFW-7781 |
Get device API does not return error when the LPSC is in transition state |