2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM64x installer provides everything needed as discussed below to create the embedded system from “scratch” :
Platform/board-support software and configuration files for Linux
U-Boot and Kernel sources and configuration files
An ARM cross-compiling toolchain as well as other host binaries and components
A Yocto/OE compliant filesystem and sources for example applications
A variety of scripts and Makefiles to automate certain tasks
Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
Reference Examples, benchmarks
This release supports SR2.0 High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide
2.1.2. Licensing¶
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
Linux Manifest: “/docs/software_manifest.html”
2.1.3. Release 09.02.00¶
Released on March 2024
2.1.3.1. What’s new¶
Processor SDK 9.2 Sitara Release has following Major Updates
Kernel: MMC Highspeed tuning and Performance Improvements
RT Kernel : Significant Improvements to Real-Time Linux Interrupt Latency, RT Interrupt Latencies
Bug Fixes and Stability Improvements
DMSC Firmware: PLL Configuration sequence updated to latest recommendation
DMSC Firmware: No longer re-initializing ICSSG clocks
HSR Tx Tag Insertion and Rx Tag Removal offload on ICSSG
Component version:
Kernel 6.1.80
RT Kernel 6.1.80-rt26
U-Boot 2023.04
Toolchain GCC 11.4
ATF 2.10
OPTEE 4.1
DMSC Firmware v09.02.07
2.1.4. Build Information¶
2.1.4.1. U-Boot¶
u-boot
2.1.4.2. TF-A¶
2.1.4.3. OP-TEE¶
2.1.4.4. ti-linux-firmware¶
2.1.4.5. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
2.1.4.6. Yocto¶
meta-ti
meta-arago
meta-tisdk
2.1.5. Issues Tracker¶
2.1.5.1. Errata Workarounds Available in this Release¶
Record ID |
Title |
Platform |
|---|---|---|
LCPD-37352 |
CDNS: USB2 PHY locks up due to short suspend |
am64xx-evm |
LCPD-32825 |
PCIe: ls -al /dev/disk/by-id shows no nvme device |
am64xx-hsevm |
LCPD-27886 |
USART: Erroneous clear/trigger of timeout interrupt |
am64xx-evm,am62axx_sk-fs,am62xxsip_sk-fs,am62xxsip_sk-se,am62xx-sk,j721e-idk-gw,j7200-evm,j784s4-evm,j784s4-hsevm |
LCPD-25264 |
BCDMA: Blockcopy Gets Corrupted if TR Read Responses Interleave with Source Data Fetch |
am64xx-evm,am64xx-hsevm,am64xx_sk-fs |
LCPD-19965 |
OSPI PHY Controller Bug Affecting Read Transactions |
am654x-idk,am64xx-evm,j721e-idk-gw,j7200-evm |
2.1.5.2. Known Issues¶
Record ID |
Platform |
Title |
Workaround |
|---|---|---|---|
LCPD-37795 |
am62axx_sk-fs,am62pxx_sk-fs,am64xx_sk-fs |
RAM size not updated, when ECC is enabled |
https://git.ti.com/cgit/ti-u-boot/ti-u-boot/commit/?&id=26c81a4d5b31 |
LCPD-37389 |
am64xx-evm,am64xx-hssk,am62xx_sk-fs,am62xxsip_sk-fs,am62pxx_sk-fs,am64xx_sk-fs,am64xx_sk-se |
Building Kernel from sources doesn’t cover list of dependencies |
|
LCPD-37388 |
am64xx-hssk,am62xx_sk-fs,am62xxsip_sk-fs,am62xxsip_sk-se,am62pxx_sk-fs,am62pxx_sk-se,am64xx_sk-fs,am64xx_evm-se |
Building U-Boot from sources doesn’t cover list of dependencies |
|
LCPD-37197 |
am64xx-evm, am64xx-hsevm |
AM64x: ICSSG: Firmware is not updating the Host Port statistics |
|
LCPD-36993 |
am654x-evm,am654x-idk,am654x-hsevm,am64xx-evm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,beagleplay-gp,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am62axx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am62pxx_sk-fs,am62pxx_sk-se,am62lxx_evm-fs,am62lxx_evm-se,am62pxx-zebu,am62lxx-vlab,am62lxx-zebu,am62xx_p0_sk-fs,am64xx_sk-fs,am64xx_evm-se,am64xx_sk-se,am68_sk-fs,am69_sk-fs,beaglebone,bbai,bbai64-gp,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j7200-evm,j7200-hsevm,j784s4-evm,j784s4-hsevm,j722s_evm-fs,J784S4_BASESIM |
U-Boot: lpddr4.c: Error handling missing failure cases |
|
LCPD-36985 |
am64xx-hsevm |
AM64 Yocto SDK UG: Invalid eMMC Programming Steps in U-Boot Section |
|
LCPD-36981 |
am64xx-evm,am64xx-hsevm |
AM64x missing DMTimer support |
|
LCPD-36876 |
am64xx-hsevm |
running linuxptp (ptp4l, phc_ctl or ts2phc, setting clock) it will cause PPS incoherence |
|
LCPD-36864 |
am64xx-evm |
ICSSG1 is not working in Debian but working in Yocto |
|
LCPD-36414 |
am64xx-evm,am62xx_sk-fs |
Performance numbers for NOR, eMMC missing in doc |
|
LCPD-36361 |
am64xx-hsevm,am62xxsip_sk-se |
Boot failure over UART |
|
LCPD-36358 |
am64xx-evm |
am64x: eth2 link fails to come up for test_nway test |
|
LCPD-35352 |
am64xx-evm,am64xx_sk-fs |
AM64x dts file calls SYNC2_OUT the wrong name |
|
LCPD-35022 |
am64xx-hsevm |
AM64x: Benchmark OOB doesn’t show any load on A53 and R5 (core 0) with latest ti-rpmsg-char v6.1 |
|
LCPD-29861 |
am64xx-evm,am64xx-hsevm,am64xx-hssk,am64xx_sk-fs |
AM64x: IPC tests fail |
|
LCPD-25540 |
am64xx-hsevm,am64xx_sk-fs |
AM64: u-boot: usb host boot failed |
|
LCPD-25494 |
am64xx-evm |
AM64 EVM TSN IET tests is failing |
|
LCPD-24823 |
am64xx-evm,am64xx_sk-fs |
Clarify Single-Core usage in ti,k3-r5f-rproc.yaml |
|
LCPD-24595 |
am64xx-evm,am64xx_sk-fs,j721e-idk-gw,j721e-sk,j7200-evm |
j721e-idk-gw USB Suspend/Resume with RTC Wakeup fail (Impact 1) |
|
LCPD-24537 |
am654x-evm,am64xx-evm,am64xx-hsevm |
am654x-idk nslookup times out when all netwokring interfaces are active |
|
LCPD-24456 |
am654x-evm,am654x-idk,am654x-hsevm,am64xx-evm,am64xx-hsevm,am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am335x-evm,am335x-hsevm,am335x-ice,am335x-sk,am43xx-epos,am43xx-gpevm,am43xx-hsevm,am437x-idk,am437x-sk,am571x-idk,am572x-idk,am574x-idk,am574x-hsidk,am57xx-evm,am57xx-beagle-x15,am57xx-hsevm,am62xx-sk,am64xx_sk-fs,beaglebone,bbai,beaglebone-black,dra71x-evm,dra71x-hsevm,dra72x-evm,dra72x-hsevm,dra76x-evm,dra76x-hsevm,dra7xx-evm,dra7xx-hsevm,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j7200-evm,j7200-hsevm,omapl138-lcdk |
Move IPC validation source from github to git.ti.com |
|
LCPD-24448 |
am64xx-evm,am64xx-hsevm |
Verify IPC kernel: main-r5f0(s)/main-r5f1(s) |
|
LCPD-22912 |
am64xx-evm |
am64xx-evm SMP dual core test fails sporadically |
|
LCPD-22892 |
am654x-evm,am654x-idk,am64xx-evm |
icssg: due to FW bug both interfaces has to be loaded always |
|
LCPD-22834 |
am64xx-evm |
am64xx-evm stress boot test fails |
|
LCPD-20105 |
am64xx-evm |
AM64x: Kernel: ADC: RX DMA channel request fails |
|
SYSFW-6432 |
am62x,am62ax,am62px,am64x,am65x |
Set device API doesn’t return Error when PD is in transition state |
|
SYSFW-6426 |
am62x,am62ax,am62px,am64x,am65x |
Ownership of a firewall region can be transferred to an invalid host |
|
SITSW-3922 |
am64xx-evm, am64xx-sk, am62xx-sk, am62xx-sk-lp, am62x-sip-sk, am62p-sk |
Flash writer: Benchmark script fails for emmc logs |
2.1.5.3. Issues opened in previous releases that were closed on this release¶
Record ID |
Title |
Platform |
|---|---|---|
LCPD-37742 |
AM64x: uboot eMMC speed check test fails |
am64xx-evm,am64xx-hsevm,am64xx-hssk |
LCPD-37721 |
ICSSG : RX Frame Drop during XDP |
am654x-idk,am64xx-evm,am64xx-hsevm |
LCPD-37524 |
ti-rpmsg-char: remove references to ti.ipc4.ping-pong |
am654x-evm,am654x-idk,am64xx-evm,am62xx_sk-fs,am62axx_sk-fs,am62pxx_sk-fs |
LCPD-37503 |
Multicast filtering with HSR non-offload does not work |
am64xx-evm |
LCPD-37501 |
HSR two board setup requires running hsr setup script twice |
am64xx-evm,am64xx-hsevm |
LCPD-37500 |
Multicast filtering with HSR does not work after running HSR hw offload setup twice |
am64xx-evm |
LCPD-37352 |
CDNS: USB2 PHY locks up due to short suspend |
am64xx-evm |
LCPD-37327 |
eMMC: Doc and testcase update needed to enable RST_FUNCTION for warm reboot |
am654x-evm,am654x-idk,am654x-hsevm,am64xx-evm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,beagleplay-gp,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am62axx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am62pxx_sk-fs,am62pxx_sk-se,am62lxx_evm-fs,am62lxx_evm-se |
LCPD-37309 |
Search is broken, never completes in 9.1 Linux SDKs |
am64xx-evm,am64xx-hsevm,am62xx_sk-fs,am64xx_sk-fs |
LCPD-37300 |
AM64x SDK v9.1 SDK Images don’t boot on SK-AM64B due to U-Boot using incorrect DTS File from EVM |
am64xx-hsevm,am64xx-hssk |
LCPD-37223 |
AM64x: ICSSG1 MII mode isn’t working |
am64xx-evm,am64xx-hsevm |
LCPD-37207 |
Docker is disabled in RT Linux |
am64xx-hssk,am62xx_lp_sk-fs,am62xxsip_sk-fs,am62pxx_sk-fs |
LCPD-32640 |
Kernel HSR does not work on base image (same command works on default) |
am64xx-evm |
SYSFW-6763 |
TISCI_MSG_SET_DEVICE_RESETS message returns success for invalid device reset range |
am62x,am62ax,am62px |
SYSFW-7056 |
Implement New PLL sequence Proposed by HW team |
am62x,am62ax,am62px,am64x |
SYSFW-6941 |
TISCI_MSG_SYS_RESET fails for negative testcase |
am62x,am62ax,am62px |
SYSFW-6892 |
TISCI Clock api returns success for invalid Clock ID |
am62x,am62ax,am62px,am64x,am65x |
SYSFW-6903 |
REF_DEF Value must be 1 for proper PLL operations |
am64x |
2.1.5.4. Issues found and closed on this release that may be applicable to prior releases¶
Record ID |
Title |
Platform |
|---|---|---|
LCPD-37084 |
AM64x : GPMC NAND Boot |
am64xx-evm,am64xx-hsevm,am64xx-hssk,am64xx_evm-se |
LCPD-36992 |
U-Boot: k3-ddrss.c: Missing ‘const’ on k3_ddrss_ops |
am654x-evm,am654x-idk,am654x-hsevm,am64xx-evm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,beagleplay-gp,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am62axx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am62pxx_sk-fs,am62pxx_sk-se,am62lxx_evm-fs,am62lxx_evm-se,am62pxx-zebu,am62lxx-vlab,am62lxx-zebu,am62xx_p0_sk-fs,am64xx_sk-fs,am64xx_evm-se,am64xx_sk-se,am68_sk-fs,am69_sk-fs,beaglebone,bbai,bbai64-gp,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j721s2_evm-se,j7200-evm,j7200-hsevm,j784s4-evm,j784s4-hsevm,j722s_evm-fs,J784S4_BASESIM |
LCPD-36868 |
AM64x MMC1 HS OTAPSEL value is incorrect in kernel device tree |
am64xx-evm,am64xx-hsevm,am64xx-hssk |
LCPD-36850 |
HSR switching offload firmware needs to be loaded twice |
am64xx-hsevm |
LCPD-36847 |
doc: ltp-ddt documentation is not upto date |
am64xx-hsevm,am62xx_sk-fs,am62axx_sk-fs,am62pxx_sk-fs,am68_sk-fs,am69_sk-fs,j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm |
LCPD-36842 |
ETH_XS_FUNC_ICSSG_TESTS_SPEED Fails |
am64xx-hsevm |
LCPD-36744 |
Linux SDK: CPSW: Bridge interface cannot ping in Switch Mode |
am64xx-evm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,am64xx_sk-fs,am64xx_evm-se,am64xx_sk-se,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j7200-evm,j7200-hsevm,j784s4-evm,j784s4-hsevm |
LCPD-36645 |
AM64X: Linux HSR - Multicast filtering support |
am64xx-evm |
LCPD-36395 |
MMC delaybuffer duration, DLL / delay chain select, and DLL Ref Frequency are not programmed to PHY_CTRL5 register |
am64xx-evm,am64xx_sk-fs |
LCPD-35108 |
AM64x: eMMC boot fails using flashed using DFU |
am64xx-evm |
LCPD-35096 |
OPTEE xtest failures |
am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am62axx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am62pxx_sk-fs,am62pxx_sk-se,am68_sk-fs |
LCPD-34800 |
eMMC itapdly sel is not programmed to PHY_CTRL4 register |
am64xx-evm,am64xx_sk-fs |
LCPD-34780 |
DT property ti,driver-strength-ohm is only applicable to AM64x MMC0 |
am64xx-evm,am62xx_sk-fs,am62xx_lp_sk-fs,am62axx_sk-fs,am62xx-lp-sk,am62xx-sk,am64xx_sk-fs |
LCPD-32868 |
Kernel crash from PRU auto-forwarding packet |
am654x-idk,am64xx-evm |
LCPD-32481 |
AM64x: Environment variables for DFU to NAND |
am64xx-evm,am64xx-hsevm |
LCPD-29597 |
AM64x: dts: main_rti nodes are defined twice |
am64xx-evm |
LCPD-29489 |
M4F Core should be able to load data to OC_SRAM |
am64xx-evm,am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62xx-lp-sk,am62xx-sk,am64xx_sk-fs |
LCPD-29445 |
AM62ax: MCAN CAN_S_FUNC_MODULAR test is failing |
am64xx-evm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am62axx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am62pxx_sk-fs,am62pxx_sk-se |
LCPD-24288 |
am64xx-evm NCM/ACM network performance test crashes with RT images |
am64xx-evm,am64xx-hsevm |
LCPD-23011 |
Missing u-boot README file for AM64x |
am64xx-evm,am62xx_sk-fs,am62xx_sk-se,am62xx-sk,am64xx_sk-fs |
LCPD-20006 |
AM64x: remoteproc may be stuck in the start phase after a few times of stop/start |
am64xx-evm |