4. How to GuidesΒΆ
- 4.1. Host
- 4.2. Target
- 4.3. Developer Notes
- 4.1.1. Connect to an EVM via Telnet
- 4.1.2. How to Setup a Samba Server
- 4.1.3. Moving Files to the Target System
- 4.2.1. SDK File System Optimization/Customization
- 4.3.1. How to verify IPC between Linux and MCU R5 in Keystone devices?
- 4.3.2. How to check some device tree information from user-space of Linux?
- 4.3.3. How do I integrate a different version of open source software than what is packaged in Processor SDK?
- 4.1.4. K3 Resource Partitioning Tool
- 4.1.5. How to Setup and Debug using Lauterbach
- 4.1.6. Enabling and Parsing SYSFW Trace
- 4.4. Hardware EVM Setup
- 4.5. Frequently Asked Questions