2.1. Release Notes¶
2.1.1. Overview¶
The Processor Software Development Kit (Processor SDK) is a unified software platform for TI embedded processors providing easy setup and fast out-of-the-box access to benchmarks and demos. All releases of Processor SDK are consistent across TI’s broad portfolio, allowing developers to seamlessly reuse and develop software across devices. Developing a scalable platform solutions has never been easier than with the Processor SDK and TI’s embedded processor solutions.
To simplify the end user experience, Processor SDK Linux AM64x installer provides everything needed as discussed below to create the embedded system from “scratch” :
Platform/board-support software and configuration files for Linux
U-Boot and Kernel sources and configuration files
An ARM cross-compiling toolchain as well as other host binaries and components
A Yocto/OE compliant filesystem and sources for example applications
A variety of scripts and Makefiles to automate certain tasks
Other components needed to build an embedded system that don’t fit neatly into one of the above buckets
Reference Examples, benchmarks
This release supports SR2.0 High Security - Field Securable (HS-FS) devices. For migration guide and other info, refer GP to HS-FS Migration Guide
2.1.2. Licensing¶
Please refer to the software manifests, which outlines the licensing status for all packages included in this release. The manifest can be found on the SDK download page or in the installed directory as indicated below.
Linux Manifest: “/docs/software_manifest.html”
2.1.3. Release 09.01.00¶
Released on December 2023
2.1.3.1. What’s new¶
Processor SDK 9.1 Sitara Release has following Major Updates
Significant Improvements to Real-Time Linux Interrupt Latency, RT Interrupt Latencies
Bug Fixes and Stability Improvements
Kernel: GPMC NAND
IPC: Graceful Shutdown
Connectivity: HSR Tx Packet Duplication offload, Cut-thru support in switch mode
Major Refresh of component version:
Kernel 6.1
U-Boot 2023.04
Toolchain GCC 11.4
ATF 2.9+
OPTEE 4.0
2.1.4. Build Information¶
2.1.4.1. U-Boot¶
u-boot
2.1.4.2. TF-A¶
2.1.4.3. OP-TEE¶
2.1.4.4. Ti-linux-firmware¶
2.1.4.5. Kernel¶
Linux Kernel
Real Time (RT) Linux Kernel
2.1.4.6. Yocto¶
meta-ti
meta-arago
meta-tisdk
2.1.5. Issues Tracker¶
2.1.5.1. Errata Workarounds Available in this Release¶
Record ID |
Title |
Platform |
|---|---|---|
LCPD-32825 |
PCIe: ls -al /dev/disk/by-id shows no nvme device |
am64xx-hsevm |
LCPD-27886 |
USART: Erroneous clear/trigger of timeout interrupt |
am64xx-evm,am62axx_sk-fs,am62xxsip_sk-fs,am62xxsip_sk-se,am62xx-sk,j721e-idk-gw,j7200-evm,j784s4-evm,j784s4-hsevm |
LCPD-25264 |
BCDMA: Blockcopy Gets Corrupted if TR Read Responses Interleave with Source Data Fetch |
am64xx-evm,am64xx-hsevm,am64xx_sk-fs |
LCPD-19965 |
OSPI PHY Controller Bug Affecting Read Transactions |
am654x-idk,am64xx-evm,j721e-idk-gw,j7200-evm |
2.1.5.2. U-Boot Known Issues¶
Record ID |
Platform |
Title |
Workaround |
|---|---|---|---|
LCPD-28503 |
am64xx-evm,am62xx_sk-fs,am62xx_sk-se,am62xx-sk,am64xx_sk-fs |
Need to sync up DTS files between u-boot and kernel for at least AM62x, possibly other boards too |
|
LCPD-25540 |
am64xx-hsevm,am64xx_sk-fs |
AM64: u-boot: usb host boot failed |
2.1.5.3. Linux Known Issues¶
Record ID |
Platform |
Title |
Workaround |
|---|---|---|---|
LCPD-37197 |
am64xx-evm,am64xx-hsevm |
AM64x: ENET ICSSG: Firmware is not updating the Host Port statistics |
|
LCPD-36975 |
am64xx-evm |
HSR Error: 8021q: VLANs not supported on device. |
|
LCPD-36876 |
am64xx-hsevm |
running linuxptp (ptp4l, phc_ctl or ts2phc, setting clock) it will cause PPS incoherence |
|
LCPD-36804 |
am64xx-evm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am64xx_sk-fs,am64xx_evm-se,am64xx_sk-se |
IPC performance test fail - modprobe fails |
|
LCPD-36622 |
am654x-evm,am654x-idk,am654x-hsevm,am64xx-evm |
Errata i2028: USB3.0 Host and Device Non-Functional |
|
LCPD-36361 |
am64xx-hsevm,am62xxsip_sk-se |
Boot failure over UART |
|
LCPD-35352 |
am64xx-evm,am64xx_sk-fs |
AM64x dts file calls SYNC2_OUT the wrong name |
|
LCPD-35022 |
am64xx-hsevm |
AM64x: Benchmark OOB doesn’t show any load on A53 and R5 (core 0) with latest ti-rpmsg-char v6.1 |
|
LCPD-32868 |
am654x-idk,am64xx-evm |
Kernel crash from PRU auto-forwarding packet |
|
LCPD-27871 |
am64xx-evm |
GPMC NAND driver misleading error |
|
LCPD-25494 |
am64xx-evm |
AM64 EVM TSN IET tests is failing |
|
LCPD-24823 |
am64xx-evm,am64xx_sk-fs |
Clarify Single-Core usage in ti,k3-r5f-rproc.yaml |
|
LCPD-24595 |
am64xx-evm,am64xx_sk-fs,j721e-idk-gw,j721e-sk,j7200-evm |
j721e-idk-gw USB Suspend/Resume with RTC Wakeup fail (Impact 1) |
|
LCPD-24537 |
am654x-evm,am64xx-evm,am64xx-hsevm |
am654x-idk nslookup times out when all netwokring interfaces are active |
|
LCPD-24456 |
am654x-evm,am654x-idk,am654x-hsevm,am64xx-evm,am64xx-hsevm,am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am335x-evm,am335x-hsevm,am335x-ice,am335x-sk,am43xx-epos,am43xx-gpevm,am43xx-hsevm,am437x-idk,am437x-sk,am571x-idk,am572x-idk,am574x-idk,am574x-hsidk,am57xx-evm,am57xx-beagle-x15,am57xx-hsevm,am62xx-sk,am64xx_sk-fs,beaglebone,bbai,beaglebone-black,dra71x-evm,dra71x-hsevm,dra72x-evm,dra72x-hsevm,dra76x-evm,dra76x-hsevm,dra7xx-evm,dra7xx-hsevm,j721e-hsevm,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2-hsevm,j721s2_evm-fs,j7200-evm,j7200-hsevm,omapl138-lcdk |
Move IPC validation source from github to git.ti.com |
|
LCPD-24288 |
am64xx-evm,am64xx-hsevm |
am64xx-evm NCM/ACM network performance test crashes with RT images |
|
LCPD-22912 |
am64xx-evm |
am64xx-evm SMP dual core test fails sporadically |
|
LCPD-22892 |
am654x-evm,am654x-idk,am64xx-evm |
icssg: due to FW bug both interfaces has to be loaded always |
|
LCPD-22834 |
am64xx-evm |
am64xx-evm stress boot test fails |
|
LCPD-22215 |
am64xx-evm |
PCIE NVM card stops enumerating on am64xx after some time |
|
LCPD-20705 |
am64xx-evm |
USB stick attached to PCIe USB card is not enumerated |
|
LCPD-20105 |
am64xx-evm |
AM64x: Kernel: ADC: RX DMA channel request fails |
|
LCPD-20006 |
am64xx-evm |
AM64x: remoteproc may be stuck in the start phase after a few times of stop/start |
|
LCPD-18854 |
am64xx-evm,dra71x-evm,dra76x-evm |
ov5640 sensor capture fails for raw format capture |
2.1.5.4. Issues opened in previous releases that were closed on this release¶
Record ID |
Title |
Platform |
|---|---|---|
LCPD-34852 |
Few times payload is packed at size boundary by binman |
am654x-evm,am64xx-evm,am62xx_sk-se,j721e-idk-gw,j721s2-evm,j7200-evm |
LCPD-34840 |
AM64: Networking failures including ICSSG |
am64xx-hsevm |
LCPD-34697 |
am64x: dtsi: mcu_gpio0 compatible property typo |
am64xx-evm,am64xx_sk-fs |
LCPD-34687 |
MMC itapdly sel values are not specified in kernel DTS |
am64xx-evm,am64xx_sk-fs |
LCPD-34686 |
MMC itapdly sel values are not specified in uboot DTS |
am64xx-evm,am62axx_sk-fs |
LCPD-34583 |
AM64x: some sdcards boot fail in u-boot |
am64xx-evm,am64xx_sk-fs |
LCPD-34548 |
k3-image-gen generate error messages |
am64xx-evm |
LCPD-34413 |
RT Linux: Interrupt latency issue with >200us outliers |
am654x-evm,am654x-hsevm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_lp_sk-fs,am62axx_sk-fs,am62xx-sk,am64xx_sk-fs,j721e-sk,j721s2-evm,j721s2_evm-fs,j7200-evm,j784s4-evm |
LCPD-34258 |
Upstream: kernel: Bug: “ti,j721e-esm” should be described bindings and devicetree update |
am654x-evm,am654x-idk,am64xx-evm,am64xx_sk-fs,am68_sk-fs,am69_sk-fs,j721e-idk-gw,j721e-sk,j721s2-evm,j721s2_evm-fs,j7200-evm,j784s4-evm |
LCPD-32958 |
AM6xx/J7: Issue with MCSPI clocking in Linux driver |
am654x-evm,am654x-idk,am654x-hsevm,am64xx-evm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am62axx_sk-se,am62xx-lp-sk,am62xx-sk,am64xx_sk-fs |
LCPD-32946 |
RT Linux: PRU Ethernet link down causes kernel crash |
am654x-evm,am654x-idk,am64xx-evm |
LCPD-32825 |
PCIe: ls -al /dev/disk/by-id shows no nvme device |
am64xx-hsevm |
LCPD-32823 |
ICSS firmware does not process Rx packets once Min error frame is received |
am654x-idk,am64xx-evm |
LCPD-32815 |
Packet get truncated on Transmit side when high traffic is applied |
am654x-idk,am64xx-evm |
LCPD-29880 |
CAN_S_FUNC_MODULAR test fail |
am64xx-evm,j721s2-evm,j7200-evm,j784s4-evm |
LCPD-29854 |
MCU UART TX baud rate is doubled |
am64xx-evm,am64xx-hsevm,am64xx-hssk,am64xx_sk-fs |
LCPD-29739 |
AM64: NAND device not detected in U-boot |
am64xx-hsevm |
LCPD-29651 |
AM64: NAND Flash device not detected |
am64xx-hsevm |
LCPD-29597 |
AM64x: dts: main_rti nodes are defined twice |
am64xx-evm |
LCPD-29588 |
CPSW documentation: Time Sync Router no longer firewalled |
am654x-evm,am654x-idk,am64xx-evm,am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62axx_sk-fs,am62xx-lp-sk,am62xx-sk,am64xx_sk-fs |
LCPD-29508 |
AM64x: EMMC speed test fails: MMC not running on HS400 mode |
am64xx-evm,am64xx-hsevm,am64xx_sk-fs |
LCPD-29500 |
AM64x: ETH CPSW2g TAS: tests fail with undefined method error |
am64xx-evm,am64xx-hsevm,am64xx_sk-fs |
LCPD-29499 |
AM64x: ETH CPSW2g TAS: tests fail with queue 0 did not increase |
am64xx-evm,am64xx-hsevm,am64xx_sk-fs |
LCPD-29498 |
AM64x: ETH CPSW2g TAS: Invalid traffic schedule |
am64xx-evm,am64xx-hsevm,am64xx_sk-fs |
LCPD-29446 |
Linux SDK docs should explicitly state what peripherals are supported |
am654x-evm,am654x-idk,am64xx-evm,am62xx_sk-fs,am62xx_sk-se,am335x-evm,am335x-ice,am335x-sk,am43xx-gpevm,am437x-idk,am437x-sk,am62xx-sk,am64xx_sk-fs |
LCPD-29442 |
Docs: AM62x-SK: Kernel User Guide uses tisdk_am64xx defconfigs |
am62xx_sk-fs,am62xx_sk-se,am62xx-sk |
LCPD-29362 |
AM64x EVM Devicetree should disable unused MCU peripherals |
am64xx-evm,am64xx_sk-fs |
LCPD-29305 |
AM64x Uboot SRAM addresses are outdated |
am64xx-evm,am64xx_sk-fs |
LCPD-28688 |
AM62x Kernel User Guide: Document AM62x default kernel config |
am64xx-evm,am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62axx_sk-fs,am62xx-lp-sk,am62xx-sk,am64xx_sk-fs |
LCPD-28672 |
CPSW: Add more details about driver config |
am64xx-evm,am62xx_sk-fs,am62xx_sk-se,am62axx_sk-fs,am62xx-sk,am64xx_sk-fs |
LCPD-28660 |
AM64x: tiboot3.bin generated by U-Boot build is confusing users |
am64xx-evm,am64xx-hsevm,am64xx_sk-fs |
LCPD-26692 |
Hardware + Software IPSec Performance Test Failures |
am64xx-evm,am335x-evm,am43xx-gpevm,am57xx-evm,j721e-idk-gw |
LCPD-24649 |
dma-heaps-test fails to build with 5.16-rc3 kernel+ |
am64xx-evm,am335x-evm,dra71x-evm,j721e-idk-gw |
LCPD-23020 |
am64xx-evm: U-Boot PHY autonegotiation failed 2 out of 100 times |
am64xx-evm |
LCPD-23011 |
Missing u-boot README file for AM64x |
am64xx-evm,am62xx_sk-fs,am62xx_sk-se,am62xx-sk,am64xx_sk-fs |
LCPD-22931 |
RemoteProc documentation missing |
am654x-evm,am654x-idk,am64xx-evm,am64xx_sk-fs |
LCPD-22319 |
OpenSSL performance test data out of bounds |
am64xx-evm,am62axx_sk-fs,am62xx-sk,j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm |
LCPD-20038 |
OPTEE test applications are missing from rootfs |
am64xx-hsevm |
2.1.5.5. Issues found and closed on this release that may be applicable to prior releases¶
Record ID |
Title |
Platform |
|---|---|---|
LCPD-37151 |
am62: am64: i2c set/get tests are failing |
am62xx_sk-fs,am62xx_sk-se,am62xx_lp_sk-fs,am62xx_lp_sk-se,am62axx_sk-fs,am62axx_sk-se,am62xxsip_sk-fs,am62xxsip_sk-se,am62pxx_sk-fs,am62pxx_sk-se,am62xx-sk |
LCPD-36850 |
HSR switching offload firmware needs to be loaded twice |
am64xx-hsevm |
LCPD-36847 |
doc: ltp-ddt documentation is not upto date |
am64xx-hsevm,am62xx_sk-fs,am62axx_sk-fs,am62pxx_sk-fs,am68_sk-fs,am69_sk-fs,j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm |
LCPD-36744 |
Linux SDK: CPSW: Bridge interface cannot ping in Switch Mode |
am64xx-evm,am64xx-hsevm,am64xx-hssk,am62xx_sk-fs,am62xx_sk-se,am64xx_sk-fs,am64xx_evm-se,am64xx_sk-se,j721e-hsevm,j721e-evm-ivi,j721e-idk-gw,j7200-evm,j7200-hsevm,j784s4-evm,j784s4-hsevm |
LCPD-36645 |
AM64X: Linux HSR - Multicast filtering support |
am64xx-evm |
LCPD-36621 |
K3: OPENSSL: Fix testcases and make it platform specific |
am62xx_sk-se,am62axx_sk-fs,am64xx_sk-fs,am68_sk-fs,am69_sk-fs,j721e-idk-gw,j721e-sk,j721s2-evm,j7200-hsevm,j784s4-evm |
LCPD-36587 |
U-Boot: CPSW: Phy-Mode not configured correctly for ports |
am64xx-evm,am64xx-hsevm,am62xx_sk-fs,am62xx_sk-se,am64xx_sk-fs,am64xx_sk-se |
LCPD-36549 |
ICSSG: Ping to bridge not working in switch mode |
am654x-idk,am64xx-hsevm |
LCPD-36494 |
Migrate to OPTEE 4.0.0 to address PSIRT |
am62xx_sk-fs,am62axx_sk-fs,am64xx_sk-fs,j721e-idk-gw,j721s2-evm,j7200-evm,j784s4-evm |
LCPD-36473 |
ICSSG UDP Performance Failure |
am64xx-hsevm |
LCPD-36287 |
Doc: Update Toolchain documentation to 11.2+ |
am62xx_sk-fs,am64xx_sk-fs,j721e-idk-gw |
LCPD-35300 |
Doc Bugs - Link/Add TISCI chapters and remove MSMC chapter |
am64xx-hsevm,am62xx_sk-fs |
LCPD-35108 |
AM64x: eMMC boot fails using flashed using DFU |
am64xx-evm |
LCPD-35033 |
AM64: ICSSG VLAN testcase is failing in 9.0-rc6 |
am64xx-hsevm |
LCPD-34994 |
AM64x: fitImage not booting |
am64xx-hsevm |
LCPD-34993 |
AM64x: sf probe fails on hs-fs |
am64xx-hsevm |
LCPD-34992 |
AM64x DFU Boot fails with signed images |
am64xx-hsevm |
LCPD-34966 |
rpmsg_ctrl device mapping errors see with 6.1 kernel |
am64xx-evm,am62xx_sk-fs,am62axx_sk-fs,am62xx-lp-sk,am62xx-sk,am64xx_sk-fs,j721e-evm-ivi,j721e-idk-gw,j721e-sk,j721s2-evm,j784s4-evm |
2.1.5.6. Linux SDK known issues¶
Record ID |
Title |
Platform |
|---|---|---|
LCPD-37207 |
Docker is disabled in RT Linux |
am64xx-hssk, am62xx_lp_sk-fs, am62xxsip_sk-fs, am62pxx_sk-fs |