4.1.7. SYSFW Trace ParserΒΆ
This chapter gives details on how a helper script packaged in the SDK can be used to parse the TISCI trace data. For more details on the TIFS trace refer to Trace chapter of TISCI documentation.
SDK packages a SYSFW trace parser utility (bin/sysfw_trace_parser.py
) which
helps in parsing the hex strings that are output in UART when trace is enabled.
Usage of this tool is described below. Current version of trace (Option -Tv) is 0x03006
.
usage: ./sysfw_trace_parser.py [-h] (-l LOG_FILE | -d SERIAL_PORT)
(-o OUTPUT_FILE | -O) [-Tv TRACE_DATA_VERSION]
[-t] [-r RULES_FILE] [-Pm]
Required arguments - Choose one of the inputs:
-l LOG_FILE, --log_file LOG_FILE
Log File provided as input (default: None)
-d SERIAL_PORT, --serial_port SERIAL_PORT
Provide Device as input: Requires pyserial package
installed: See https://pyserial.readthedocs.io/
(default: None)
Required arguments - Choose one of the outputs:
-o OUTPUT_FILE, --output_file OUTPUT_FILE
Parse out the output to a file (default: None)
-O, --output_console Log File to parse and report results to console
(default: False)
optional arguments:
-h, --help show this help message and exit
-Tv TRACE_DATA_VERSION, --trace_data_version TRACE_DATA_VERSION
Trace data version input in form "0xYYZZZ" where YY is
the major and ZZZ is the minor version. A trace data
version found in the log will override this input
(default: None)
-t, --time_stamp_relative
Add TimeStamp to output in relative milliseconds(this
is approximation ONLY) (default: False)
-r RULES_FILE, --rules_file RULES_FILE
Alternate Rules file (default: /home/vishallocal/SYSFW
/system-firmware-tools/system-firmware-
test/scripts/sysfw_trace_rules.json)
-Pm, --print_match_only
Print just decoded data, (default: False)
This script can also be called as a python module with the same arguments as
the CLI. from sysfw_trace_parser import * sysfw_cli_job(args_arr=["-l",
"sysfw_v2019.03_fail.log","-o","/tmp/out.log","-Tv","0x00000"]);