3. Foundational ComponentsΒΆ
- 3.1. U-Boot
- 3.1.1. User’s Guide
- 3.1.1.1. General Information
- 3.1.1.2. USB Device Firmware Upgrade (DFU)
- 3.1.1.3. Booting over Ethernet (Ethernet RGMII)
- 3.1.1.4. NAND
- 3.1.1.5. SD, eMMC and USB
- 3.1.1.5.1. Partitioning eMMC from U-Boot
- 3.1.1.5.2. Updating an SD card from a host PC
- 3.1.1.5.3. Updating an SD card or eMMC using DFU
- 3.1.1.5.4. Booting Linux from SD card or eMMC
- 3.1.1.5.5. Booting tiboot3.bin, tispl.bin and u-boot.img from eMMC boot partition (For K3 class of SoCs)
- 3.1.1.5.6. Booting to U-Boot prompt from USB storage
- 3.1.1.5.7. Booting Linux from USB storage
- 3.1.1.6. SPI
- 3.1.1.7. OSPI/QSPI
- 3.1.1.8. UART
- 3.1.1.9. DDR3 ECC
- 3.1.2. Troubleshooting
- 3.1.1. User’s Guide
- 3.2. Kernel
- 3.2.1. Users Guide
- 3.2.2. Kernel Drivers
- 3.2.2.1. ADC
- 3.2.2.2. Crypto
- 3.2.2.3. MCAN
- 3.2.2.4. GPIO
- 3.2.2.5. I2C
- 3.2.2.6. HSR PRP
- 3.2.2.7. CPSW3g
- 3.2.2.7.1. Introduction
- 3.2.2.7.2. Driver Configuration
- 3.2.2.7.3. Device tree bindings
- 3.2.2.7.4. Multi MAC mode
- 3.2.2.7.4.1. Interrupt pacing
- 3.2.2.7.4.2. Common Platform Time Sync (CPTS) module
- 3.2.2.7.4.3. Enhancements for Scheduled Traffic (EST) Offload
- 3.2.2.7.4.4. Intersperse Express Traffic (IET) Frame Preemption offload
- 3.2.2.7.4.5. Forwarding and Queuing Enhancements for Time-Sensitive Streams (FQTSS, 802.1Qav)
- 3.2.2.7.5. Multi port Switch mode
- 3.2.2.7.5.1. Bridge setup
- 3.2.2.7.5.2. Turn On/Off Spanning Tree Protocol (STP)
- 3.2.2.7.5.3. VLAN configuration
- 3.2.2.7.5.4. Adding extra VLANs
- 3.2.2.7.5.5. Forwarding Data Bases (FDBs)
- 3.2.2.7.5.6. Multicast Data Bases (MDBs)
- 3.2.2.7.5.7. Multicast flooding
- 3.2.2.7.5.8. Enabling Cut Through forwarding
- 3.2.2.7.5.9. Transmit Traffic Control and Rate Limiting
- 3.2.2.8. PCIe End Point
- 3.2.2.9. PCIe Root Complex
- 3.2.2.10. PWM
- 3.2.2.11. OSPI/QSPI
- 3.2.2.12. SPI
- 3.2.2.13. NAND
- 3.2.2.14. MMC/SD
- 3.2.2.15. UART
- 3.2.2.16. USB
- 3.2.3. LTP-DDT Validation
- 3.2.4. FAQs
- 3.3. Filesystem
- 3.4. PRU-ICSS / PRU_ICSSG
- 3.4.1. Overview of PRU-ICSS and PRU_ICSSG
- 3.4.1.1. Getting Started Information
- 3.4.1.2. Hardware Information
- 3.4.1.3. Training Material
- 3.4.1.4. Development Tools
- 3.4.1.5. Software Information
- 3.4.1.6. Examples
- 3.4.1.7. Evaluation Hardware
- 3.4.1.8. TI Designs
- 3.4.1.9. Support
- 3.4.1.10. PRU FAQ
- 3.4.1.10.1. PRU Applications & Support questions
- 3.4.1.10.1.1. What is the difference between the PRU subsystem and ICSS?
- 3.4.1.10.1.2. Is TI providing libraries for the PRU?
- 3.4.1.10.1.3. Can I develop my own industrial protocols on the PRU-ICSS?
- 3.4.1.10.1.4. Can the PRU run a High Level Operating System?
- 3.4.1.10.1.5. My processor has a PRU. Is the PRU supported in the Linux Processor SDK?
- 3.4.1.10.2. PRU Memory Access questions
- 3.4.1.10.3. PRU GPI/O questions
- 3.4.1.10.3.1. What is the maximum speed for toggling PRU GPO pins via PRU software?
- 3.4.1.10.3.2. When does the PRU start capturing from the input pins?
- 3.4.1.10.3.3. Can the module be modified so that the GPI start bit is a zero instead of a one?
- 3.4.1.10.3.4. What happens after 28 bit GPI shifts?
- 3.4.1.10.3.5. Can data be pre-loaded into shadow registers prior to configuring the PRU GPO mode to shift out mode?
- 3.4.1.10.3.6. When does PRU<n>_CLOCKOUT start running?
- 3.4.1.10.3.7. When does the PRU start shifting data in the shadow registers?
- 3.4.1.10.3.8. The shadow registers are loaded by writing to PRU<n>_R30 [0:15]. Does this change the state of the corresponding device-level pins?
- 3.4.1.10.3.9. When the PRU<n>_ENABLE_SHIFT bit is cleared, does the PRU immediately stop shifting PRU<n>_DATAOUT?
- 3.4.1.10.3.10. Does the PRU shift data out LSB or MSB first?
- 3.4.1.10.3.11. What happens to the content stored in R30 when the PRU changes to a different GPO mode?
- 3.4.1.10.4. PRU INTC and System Event questions
- 3.4.1.10.5. PRU Debugger questions
- 3.4.1.10.1. PRU Applications & Support questions
- 3.4.2. Training
- 3.4.2.1. PRU Hands-on Labs
- 3.4.2.1.1. Lab Configuration
- 3.4.2.1.2. LAB 1: Toggle LED with PRU GPO
- 3.4.2.1.3. LAB 2: Read Push Button Switch on PRU0 GPI & Toggle LED with PRU1 GPO
- 3.4.2.1.4. LAB 3: Temperature Monitor
- 3.4.2.1.5. LAB 4: Introduction to Linux driver
- 3.4.2.1.6. LAB 5: RPMsg Communication between ARM and PRU
- 3.4.2.1.6.1. Build the PRU Firmware - Using CCSv6
- 3.4.2.1.6.2. Build the PRU Firmware - Using the Provided Makefile
- 3.4.2.1.6.3. Build the RPMsg Client Sample Driver
- 3.4.2.1.6.4. Copy files to the target file system
- 3.4.2.1.6.5. Part 1: Kernel space communication
- 3.4.2.1.6.6. What just happened?
- 3.4.2.1.6.7. Part 2: User Space Communication
- 3.4.2.1.6.8. Part 3: User Space Application
- 3.4.2.1.6.9. What just happened?
- 3.4.2.1.7. LAB 6: Blinking LEDs with RPMsg from Linux User Space
- 3.4.2.1.7.1. Build the PRU Firmware - Using CCSv6
- 3.4.2.1.7.2. Build the PRU Firmware - Using the Provided Makefile
- 3.4.2.1.7.3. Copy files to the target file system
- 3.4.2.1.7.4. Part 1: Linux Command Line LED Toggling
- 3.4.2.1.7.5. What just happened?
- 3.4.2.1.7.6. Part 2: Linux Shell Script LED Toggling
- 3.4.2.1.7.7. What just happened?
- 3.4.2.2. Getting Started with PRU Software Support Package
- 3.4.2.3. RPMsg Quick Start Guide
- 3.4.2.3.1. Introduction
- 3.4.2.3.2. Getting the Linux Processor SDK
- 3.4.2.3.3. Configuring and Building the Linux Kernel with RPMsg Support
- 3.4.2.3.4. Creating a Bootable SD Card with RPMsg Support
- 3.4.2.3.5. Booting the Board and Testing RPMsg
- 3.4.2.3.6. Getting Started with RPMsg Development
- 3.4.2.3.7. Common Issues
- 3.4.2.1. PRU Hands-on Labs
- 3.4.3. Linux Drivers
- 3.4.3.1. RemoteProc
- 3.4.3.2. RPMsg
- 3.4.3.3. PRU_ICSSG Ethernet
- 3.4.4. Firmware Development
- 3.4.5. Hardware
- 3.4.1. Overview of PRU-ICSS and PRU_ICSSG
- 3.5. Machine Learning
- 3.6. ARM Trusted Firmware-A
- 3.7. OP-TEE
- 3.8. System Firmware