3.2.2.6. HSR PRPΒΆ
Introduction
High-availability Seamless Redundancy (HSR) and Parellel Redundancy Protocol (PRP) are protocols supporting redundant network connections defined by IEC 62439-3. Both operate by using two ethernet ports together, and duplicating every frame to be sent over both ports, so if one connection fails, the transmission succeeds. Frames are tagged with a sequence number, so the receiving node can identify and discard duplicates. HSR/PRP provides an advantage over other protocols that handle link failure (e.g. STP/RSTP) because there is no downtime or packet loss on link failure. This is required in some industrial networking situations.
The major difference between HSR and PRP is that HSR networks are configured as a ring, then frames are sent both directions around the ring by all nodes. PRP networks can take any configuration, and all connections are simply physically duplicated. Additionally, PRP nodes can interoperate with standard ethernet networks, while HSR cannot. (See more details below and full details in IEC 62439-3)
Linux HSR PRP Support
Linux supports HSR/PRP protocol to be run over two EMAC ports where Linux takes care of duplicating the packets sent over the two ethernet ports and discarding the received duplicate packet. This is the non-offload HSR/PRP mechanism.
Getting Started
To try out HSR/PRP (assuming two supported platforms are set up already, and the ethernet ports are eth1/eth2):
1) Connect the Ethernet ports between devices, eth1 to eth1 and eth2 to eth2. (This acts as a 2 node ring for HSR, or a 2 node point-to-point for PRP)
- Bring down both the ethernet interfaces
ip link set eth1 down && ip link set eth2 down
- Configure both ports to have the same MAC address
ip link set dev eth1 address 70:FF:76:1C:0E:8C && ip link set dev eth2 address 70:FF:76:1C:0E:8C
- Bring up both the ethernet interfaces
ip link set eth1 up && ip link set eth2 up
- Create HSR or PRP feature
For HSR
ip link add name hsr0 type hsr slave1 eth1 slave2 eth2 supervision 45 version 1
For PRP
ip link add name prp0 type hsr slave1 eth1 slave2 eth2 supervision 45 proto 1
- Assign an IP address to the HSR/PRP interface
For HSR
ip addr add 192.168.2.20 dev hsr0
For PRP
ip addr add 192.168.2.20 dev prp0
With the above configuration, if a ping is run between the two platforms on the HSR/PRP interface, the ping will continue even if one of the connections is removed.