3.1.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layersetup.sh -f <config>
The following config files are located in the configs/coresdk directory of the oe-layersetup git repo.
Config File Description Supported machines/platforms coresdk-07.03.00.005-config.txt CoreSDK 07.03.00 Release am335x, am437x, am57xx, am654x, j7, j7200, am64xx
Note
AM64xx uses the internal OE layer to build the u-boot with the latest updates from the ti-u-boot repository. To build the u-boot with yocto for AM64xx, user has to follow the below step,
Update the meta-ti layer’s u-boot yocto recipe with the latest commit ID.
- For commit ID and other u-boot build information, refer to the AM64x Release notes.