3.1.3. Yocto Layer ConfigurationΒΆ
Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:
$ ./oe-layersetup.sh -f <config>
The following config files are located in the configs/coresdk directory of the oe-layersetup git repo.
Config File Description Supported machines/platforms coresdk-07.03.00.005-config.txt CoreSDK 07.03.00 Release am335x, am437x, am57xx, am654x, j7, j7200, am64xx