1.1.2. Build and Run the DemosΒΆ
Build Instructions
Processor SDK AM64x support GNU make based build system. Refer to /<INSTALL-DIR>/sitara-apps/makerules folder for all supported demos and build targets
Below is a list of build targets supported by processor SDK AM64x:
Build Target | Description |
benchmark_demo_build | Benchmarking demos |
Benchmark demos
How to build dependent components
Set-up Linux build environment to rebuild kernel, u-boot & DTB
$ cd /<INSTALL-DIR>/bin/scripts $ ./setup-ubuntu.sh
Refer the respective user guides to build Linux and other RTOS/NO-RTOS packages
- For Linux Kernel, u-boot & DTB [Use Link]
- For RTOS/NO-RTOS source (MCU+ SDK) [Use Link]
- For Industrial Protocols (ECAT) [Use Link]
- For Industrial Drives (EnDAT,HDSL) [Use Link]