4.1.17. How to Guide for working with Software Bill of Materials (SBOM)
4.1.17.1. Glossary
- SBOM
Software Bill of Materials - is a comprehensive list of all the software components, dependencies, and metadata associated with an application.
- SPDX
Software Package Data Exchange - is an open standard (or format) for communicating Software Bill of Materials (SBOM) information including components, licenses, copyrights, and security references.
- CycloneDX
CycloneDX is a full-stack Bill of Materials (BOM) standard that provides advanced supply chain capabilities for cyber risk reduction.
- VEX
Vulnerability Exploitability eXchange - is a standardized format for sharing information about vulnerabilities and their exploitability.
4.1.17.2. Generating SBOM
Processor SDK Linux AM62x Yocto build generates SBOMs in the following formats and versions:
Format |
Version |
|---|---|
SPDX |
3.0 |
CycloneDX |
1.6 |
Follow the steps below based on your required format.
4.1.17.2.1. Generating SBOM in SPDX 3.0 Format
SPDX 3.0 is generated by default when building Processor SDK Linux AM62x Yocto, no extra steps required. If you require additional vulnerability information, follow these steps:
Add the following line to your
local.conf:INHERIT += "vex"
Build Yocto according to the build instructions in Processor SDK - Building the SDK with Yocto.
The following artifacts will be generated in the Yocto deploy directory:
File |
Description |
|---|---|
|
The SPDX v3.0 SBOM file |
|
Vulnerability information file generated by |
4.1.17.2.2. Generating SBOM in CycloneDX Format
To generate SBOM in CycloneDX format, follow these steps:
Start with the build instructions in Processor SDK - Building the SDK with Yocto
After cloning
oe-layersetup, uncomment themeta-cyclonedxline in the layer configuration file, for example:meta-cyclonedx,https://github.com/iris-GmbH/meta-cyclonedx.git,main,0170751b487162f8e476fd32d441ddfcf24ca78a,layers=
Add the following line to your
local.conf:INHERIT += "cyclonedx-export"
Continue to build Yocto according to the build instructions in Processor SDK - Building the SDK with Yocto.
The following artifacts will be generated in the Yocto deploy directory:
File |
Description |
|---|---|
|
The CycloneDX SBOM file |
|
The CycloneDX VEX file |
4.1.17.3. Working with SBOM
It is recommended to use open-source tools for working with SBOMs. The following open-source tools are recommended for working with SBOMs:
Format |
Tool |
Description |
|---|---|---|
CycloneDX |
Visualize CycloneDX SBOMs in a human-readable format |
|
CycloneDX |
BOM analysis, modification, diffing, merging, format conversion, signing and verification. |
|
SPDX |
A collection of open-source tools for working with SPDX SBOMs |
Note
SPDX 3.0 is not yet widely supported by SPDX tools. Using such tools with SPDX 3.0 files may give varied or unexpected results.
4.1.17.4. CVE Analysis
The sbom-cve-check tool can be used to perform CVE analysis on the generated SPDX SBOM.
Install the tool:
pip install sbom-cve-checkNote
It is recommended to install this tool in a Python virtual environment.
Retrieve the following artifacts from the Yocto deploy directory:
File
Description
$IMAGE_NAME.rootfs.spdx.jsonThe SPDX v3.0 SBOM file
$IMAGE_NAME.rootfs.jsonVulnerability information file generated by
vex.bbclassRun the CVE analysis:
sbom-cve-check --sbom-path ${IMAGE_NAME}.rootfs.spdx.json \ --yocto-vex-manifest ${IMAGE_NAME}.rootfs.json \ --export-type yocto-cve-check-manifest \ --export-path cve-check.json
Note
sbom-cve-check only supports SPDX format and does not support CycloneDX.