3.6.3. Flash via Fastboot
This application note provides instructions on using Snagfactory tool for flashing.
The Snagfactory tool has two main operations:
Snagrecover: Boots the board (recovery) using USB DFU.
Snagflash: Flashes binaries to the on-board memory using the Fastboot protocol.
This tool supports flashing multiple boards simultaneously, enhancing efficiency in producion enviroment.
3.6.3.1. Installing Snagfactory
Snagfactory tool is hosted here Snagfactory.
More info about installation can be found in Snagfactory Readme.
Snagfactory also is available on pip.
$ python3 -m pip install --user snagboot
Note
At the time of 10.1 release, the corresponding Snagfactory version was v2.0.
3.6.3.2. Building bootloader binaries for Recovery
For Snagrecover, bootloader images must support DFU boot and fastboot download.
In addition to USB DFU fragment config (which enables DFU boot) for the u-boot
build, an additional fragment config am6x_a53_snagfactory.config needs to be
used, which enables fastboot support in U-Boot and other required configs for
snagfactory.
To build bootloader images for recovery using SDK, following change is needed
in Rules.make file present in the top level of Linux SDK Installer.
UBOOT_MACHINE_R5=am62x_evm_r5_defconfig am62x_r5_usbdfu.config
UBOOT_MACHINE_A53=am62x_evm_r5_defconfig am62x_a53_usbdfu.config am6x_a53_snagfactory.config
# For AM62X LP
UBOOT_MACHINE_R5=am62x_lpsk_r5_defconfig am62x_r5_usbdfu.config
UBOOT_MACHINE_A53=am62x_lpsk_a53_defconfig am62x_a53_usbdfu.config am6x_a53_snagfactory.config
# For AM62X SIP
UBOOT_MACHINE_R5=am62xsip_evm_r5_defconfig am62x_r5_usbdfu.config
UBOOT_MACHINE_A53=am62xsip_evm_a53_defconfig am62x_a53_usbdfu.config am6x_a53_snagfactory.config
Generate the bootloader images using top-level makefile by running following commands on the terminal from the top-level of the Linux SDK installer.
$ make u-boot_clean
$ make u-boot
$ make u-boot_stage
Save the bootloader binaries generated in a separate directory. These bootloader
images will be used for recovery and to start flashing the images. The bootloader
images after make can be found in board-support/built-images.
For more details regarding USB DFU refer USB Device Firmware Upgrade (DFU).
Note
CONFIG_FASTBOOT_BUF_SIZE is defined in am6x_a53_snagfactory.config
and specifies the maximum buffer size for flashing files. Its value must be equal
or greater than the largest file size being flashed. If smaller, non-sparse
images will not flash correctly due to issues with chunked processing.
3.6.3.3. Connections
Power off the EVM and set up the boot mode switches to boot from USB DFU.
SW2-11001100 SW3-00000000
Power on the board.
Optionally you can also connect host PC to board via UART to read the console logs.
3.6.3.3.1. How to use Snagfactory
Comprehensive instructions for using the Snagfactory tool can be found here.