4.1.8. How to enable Microtips LVDS Panel
Microtips Technology USA (13-101HIEB0HF0-S) 10.1” WUXGA (1920x1200) TFT LCD panel is supported on platforms:
Steps to enable OLDI Panel DT overlay:
Follow the How to enable DT overlays in linux guide for steps on building and adding the overlay to your SD card. Make sure the correct overlay file has been appended in the
name_overlaysvariable as suggested in the same page.
Board |
overlay file name |
|---|---|
AM62X SK |
k3-am625-sk-microtips-mf101hie-panel.dtbo |
AM62X LP SK |
k3-am62-lp-sk-microtips-mf101hie-panel.dtbo |
Steps to enable Touch on the Microtips Panel on AM625 SK EVM:
Note: The following steps are only applicable on AM625 SK EVM revision E3 board
Power off the LVDS board by disconnecting the 12V barrel jack (do not power off the SK EVM)
Run the following commands from the Linux prompt:
root@am62xx-evm:~# modprobe -r ili210x root@am62xx-evm:~# i2ctransfer -f -y 0 w3@0x3f 0x09 0x1 0x0e root@am62xx-evm:~# i2ctransfer -f -y 0 w6@0x3f 0x08 0x04 0x47 0x50 0x73 0x68 root@am62xx-evm:~# i2ctransfer -f -y 0 w1@0x3f 0x72 r9
Power on the LVDS board
Run the following command:
root@am62xx-evm:~# modprobe ili210x
After re-initializing the module, the touch IC should now be registered as an input and touch should be functional.