2.2. Yocto Layer Configuration

Processor SDK uses the following oe-layersetup configs to configure the meta layers. These are the <config> used in the command:

$ ./oe-layertool-setup.sh -f <config>

The following config files are located in the configs/processor-sdk directory of the oe-layersetup git repo.

Config File

Description

Supported machines/platforms

processor-sdk-scarthgap-chromium-10.00.07.04-config.txt

Processor SDK 10.00.07.04 Release

am62xx-evm, am62xx-lp-evm, beagleplay

processor-sdk-scarthgap-10.00.07.04-config.txt

Processor SDK 10.00.07.04 Release

am62xxsip-evm